这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-12 / 12

排序:
Dual Channel MIMO Measurements for WiMAX™ Wave 2
In WiMAX Wave 2 systems, a variety of dual-channel measurements can provide essential insight into their operation and performance. Article written by Ben Zarlingo and linked with permission from Wireless Design and Development.

文章 2009-06-26

New Solutions Put Wireless To The Test
Recent advances have made it possible for test vendors to provide off-the-shelf chipset-specific solutions for Wi-Fi, Bluetooth, and WiMAX RF test. Linked with permission from Mobile Dev & design.

文章 2009-06-11

MIMO and the Battle Between LTE and WiMAX™
Link to April 10, 2009 Microwave Journal executive interview with Andy Botka and Carla Feldman regarding the PXB MIMO Receiver Test and the broader issue of LTE and WiMAX development.

文章 2009-04-10

Test solutions soup up for 4G
Link to April 9, 2009 Microwave Journal editorial. Test equipment manufacturers are providing more capability by relying on the latest hardware and software for feature-rich and easy to use solutions with impressive raw performance.

文章 2009-04-09

A Day in the Life of a Mobile WiMAX™ Handset
April 2009 featured article in Microwave Products Digest

文章 2009-04-01

Using Base Station and MIMO Channel Emulators for Mobile WiMAX Devices
This article describes how a channel emulator can be used to characterize the performance of a MIMO receiver. The testing was done in stages of increasing complexity, namely testing under AWGN conditions, MIMO testing with known static channels, and finally testing with channels chosen to represent “real world” behavior.

文章 2009-01-11

PDF PDF 1.37 MB
What Every RF Engineer Should Know: OFDM & WiMax
Feature story by Janine Love.

案例分析 2008-12-27

Unraveling Modulation Quality in Mobile WiMAX™ Uplink and Downlink with Multiple Zones and Bursts
An article written for Microwave Journal addressing the difficulty in ensuring that the modulation quality of the WiMAX radio is sufficient for optimum RF performance and that it will perform according to industry standards.

文章 2007-11-01

PDF PDF 762 KB
First Pass Accuracy with Momentum GX for WiMAX Design
Archived article at Microwave Product Digest discussing the challenges for designers in meeting cost and power consumption goals, using 3D-Planar electromagnetic (EM) simulation technology.

文章 2007-11-01

WiMAX™: Plotting A New Path To Global Broadband Mobility
Archived article at Canadian Electronics identifying innovations in test and measurement to support the innovations in the industry.

文章 2007-09-01

Validating IEEE 802.16e Designs With The Mobile WiMAX MIMO Library
The IEEE 802.16e standard, often referred to as mobile WiMAX, specifies air interfaces for broadband wireless access (BWA) systems.

文章 2007-05-08

PDF PDF 524 Bytes
WiMAX™: The Next Generation of Broadband Wireless Access
Article reprint from Electronics in Canada. This article provides anoverview of the 802.16 standard, theWiMAX forum, and key applications.

文章 2004-09-01

PDF PDF 428 KB