Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discutez avec un expert

Support technique

Mesure Electronique

Support by Product Model Number:

1-25 sur 87

Tri:
Keysight wins Test and Measurement IoT Company of the Year Award for 2016
Frost & Sullivan Recognizes Keysight Technologies as Global Test & Measurement for IoT Company of the Year 2016.

Dossier de presse 2017-01-13

Keysight Announces 5G Massive MIMO Tutorial, Poster - Bulletin
The latest 5G resources from Keysight include the new 5G massive MIMO tutorial and 5G poster. The tutorial, titled "Massive MIMO Technology Insights and Challenges," begins with a review of different multi-antenna techniques and building up to the definition of massive MIMO and how engineers can deploy the technology in 5G communications systems.

Dossier de presse 2016-06-10

Keysight Technologies' New VXT PXIe Vector Transceiver Delivers Faster Solution Creation
Keysight announced the VXT PXIe vector transceiver, a fully calibrated instrument module that provides vector signal generation and analysis in four slots.

Dossier de presse 2015-10-01

Keysight Technologies Adds New Capabilities to EXM Wireless Test Set
Keysight announces new WLAN 802.11ah and 802.11af capabilities for the EXM wireless test set.

Dossier de presse 2015-06-26

Keysight Expands UXM Wireless Test Set LTE-A Capabilities with 4CC, 256 QAM, LTE-U, Cat 0 Support
Keysight announced verification of end-to-end IP data throughput for downlink rates of 587.5 Mbps with the E7515A UXM wireless test set. Using three component carriers (3CC) and 256 QAM in the downlink, Keysight achieved sustained bi-directional 3GPP UE category 11 data rates.

Dossier de presse 2015-05-21

Keysight Test System Achieves EMVCo Qualification in Mobile & Contactless Card Digital Protocol Test

Dossier de presse 2015-04-21

Keysight Announces FIME RF Test Bench for Mobile, Contactless Card Achieves EMVCo Qualification

Dossier de presse 2015-03-11

Keysight Technologies Introduces Solution to Test 802.11ah-Based Internet-Of-Things Devices
Keysight announces that its N7617B Signal Studio for 802.11 WLAN software is the industry's first flexible 802.11ah signal creation solution and supports a variety of Keysight vector signal generators.

Dossier de presse 2015-03-09

Keysight Technologies Introduces Next-Generation Phase Coherent PXIe Multi-Channel Vector Signal
Keysight introduced a multi-channel phase coherent M9391A PXIe vector signal analyzer (VSA) and M9381A PXIe vector signal generator (VSG) for characterization and test of the latest wireless designs requiring multiple time-synchronized or phase coherent channels.

Dossier de presse 2015-03-02

Keysight Technologies Enters into Manufacturing Test License (MTL) Agreement with Broadcom

Dossier de presse 2014-09-21

Agilent Technologies and FIME to Deliver Advanced Test Tools for Mobile Payments
Agilent Technologies Inc. (NYSE: A) and FIME, an advanced secure-chip testing provider, have announced an agreement to work together to deliver pioneering testing solutions to the payments and telecommunications markets.

Dossier de presse 2014-02-18

E6640A EXM Wireless Test Set Ready for Volume Production of LTE-A, 802.11ac WLAN Devices
Agilent Technologies today announced the E6640A EXM wireless test set, which offers breakthrough manufacturing-test scalability in technology coverage, performance and capacity to test up to 32 cellular and wireless-connectivity devices in parallel.

Dossier de presse 2014-02-13

Agilent PXT Wireless Communications Test Set Selected by Tri-L Solutions for LTE Over-the-Air Test
Agilent Technologies Inc. (NYSE: A) today announced that Tri-L Solutions Inc. has selected Agilent's PXT wireless communications test set and integrated it with Tri-L Solutions SmarTest measurement software for testing LTE over the air.

Dossier de presse 2013-04-08

Agilent Technologies Introduces Industry's First LTE-Advanced 8x8 MIMO Signal-Generation and Analysi
Agilent Technologies Introduces Industry's First LTE-Advanced 8x8 MIMO Signal-Generation and Analysis Solutions

Dossier de presse 2013-01-03

Agilent Technologies Releases New Software for X-Series Signal Analyzers
Agilent Technologies extended its leadership in 802.11ac WLAN test solutions with its latest measurement application release for X-Series signal analyzers. The software release offers expanded WLAN support to include the emerging 802.11ac standard.

Dossier de presse 2012-11-01

Agilent Technologies and CATR (TMC) to Collaborate on TD-LTE MIMO
Agilent Technologies Inc. (NYSE: A) announced a memorandum of understanding has been signed with the China Academy of Telecommunication Research (Telecommunication Metrology Center), or CATR (TMC). The two organizations have agreed to work together on TD-LTE MIMO over-the-air (OTA) test research.

Dossier de presse 2012-09-13

Agilent Technologies Announces Wireless Communications Test Set with Innovative Multiport Adapter
Agilent Technologies introduced the E6607B EXT wireless communications test set and companion E6617A multiport adapter. Optimized for non-signaling testing, the EXT/MPA combination increases test throughput and reduces the cost of test in the manufacturing of current- and next-generation smartphones and tablets that contain multiformat and multiband technologies.

Dossier de presse 2012-08-01

Agilent Technologies Accelerates Early Wireless Design Verification with New Release of SystemVue
Agilent will demonstrate SystemVue 2012.06 along with a range of solutions for everything from circuit-level modeling through system verification for general RF, microwave, 4G communications, and aerospace/defense applications at DAC2012 (Booth 313), June 3-7, in San Francisco. SystemVue 2012.06 will also be demonstrated at IMS 2012/IEEE MTT-S (Booth 1015), June 19-21, in Montr al, Canada. A range of premier partner solutions will be available on Agilent Avenue and throughout the event area.

Dossier de presse 2012-06-05

Agilent Technologies' Bluetooth® Low-Energy RF Test Solution Speeds Development of Devices Based on
Bluetooth low-energy technology enables long operational life with minimal power consumption for applications such as mobile communications, sports and fitness, health care, security and home entertainment.

Dossier de presse 2012-05-29

Agilent Introduces 6-GHz Signal Generators with Industry-Best Performance

Dossier de presse 2012-05-01

Agilent Technologies Introduces 6-GHz Signal Generators with Industry-Best Performance
Today's aerospace/defense environment requires enhanced radar performance to detect weak signals at long distances. To provide the pure and precise signals needed to test these designs, the MXG uses an innovative triple-loop synthesizer to deliver phase noise performance of -146 dBc/Hz at 1 GHz and 20 kHz offset. For developers of radar components such as mixers and analog-to-digital converters, the MXG also features industry-leading spurious performance of -96 dBc at 1 GHz.

Dossier de presse 2012-05-01

Agilent Technologies Named Oscilloscope Company of the Year
The award is based on Frost & Sullivan's recent analysis of the oscilloscope market. Frost & Sullivan ranked Agilent as the No. 2 company in 2009, but its rapid revenue growth since then has made it the leader in market penetration.

Dossier de presse 2012-04-25

Agilent Technologies Introduces Signal Processing Libraries for 802.11ac WLAN and 60-GHz 802.11ad
Agilent Technologies Inc. (NYSE: A) today released SystemVue 2011.10, the latest update to the leading design environment for wireless physical-layer architects.

Dossier de presse 2011-11-16

Agilent Technologies Introduces Innovative Multi-Measurement Signal Analyzer Capability for Wireless
Agilent Technologies Inc. (NYSE:A) today announced that an innovative, new multi-measurement capability is being added to its 89600 VSA software, enabling simultaneous signal analysis of multiple carriers and signal formats for more efficient testing and deeper signal insight in wireless test.

Dossier de presse 2011-11-15

Agilent Technologies' PXA Signal Analyzer Now Enables Wideband Measurement with up to 900
Agilent Technologies Inc. (NYSE:A) today announced that its high-performance PXA signal analyzer now supports up to 900 MHz of intermediate-frequency bandwidth, enabling it to act as a broadband down converter for analysis of wideband communications and radar signals in aerospace and defense applications.

Dossier de presse 2011-09-20

1 2 3 4 Page suivante