Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discutez avec un expert

Support technique

Mesure Electronique

Inscrire le numéro de modèle: Exemples : 34401A, E4440A

1-16 sur 16

Tri:
Solutions and Measurement Tools for Use in Average Power and Envelope Tracking Design - Application
This app note provides an outline of the techniques involved and the solutions Agilent provides for RF, baseband and system developers.

Notes d’application 2014-08-02

EXT Wireless Communications Test Set Non-signaling Test Overview
This application note explains how non-signaling test methods make it possible for manufacturers to reduce both test times and test equipment costs across a range of wireless technologies

Notes d’application 2012-08-01

PDF PDF 290 KB
Testing Handovers Between LTE and 3G cdma2000/1xEV-DO Cellular Networks - Application Note
This application note explains test handovers between LTE and third generation cdma2000/1xEV-DO cellular networks as well as network evolution.

Notes d’application 2011-06-15

Customizing the E656XC/N588XA Wireless Test Manager - Application Note
This document shows how to use the WTM program to perform extra test procedures and implement some of the program’s advanced capabilities.

Notes d’application 2007-07-30

Testing Push-to-Talk Over Cellular (R&D only) - Application Note
With nearly 200 GCF conformance and interoperability PoC test cases now in existence, testing the compliance of PoC to industry standards is essential and Keysight's made it easy.

Notes d’application 2006-07-27

Applications Testing with the Keysight 8960 Series 10 Wireless Test Set (R&D only) - Application Note
The 8960 (E5515C) and Keysight lab applications help you throroughly test to current technology standards.

Notes d’application 2006-03-27

How Digitally Generated Faded Signals Reduce Cost of Test (R&D only) - Application Note
Reduce cost of test, simplify testing and be assured of accuracy using digitally integrated, calibrated noise and fading patterns.

Notes d’application 2005-08-15

Designing and Testing cdma2000 Base Stations (AN 1357) - Application Note
This Application Note describes base station design and measurement issues at the physical...

Notes d’application 2003-02-25

Designing and Testing cdma2000 Mobile Stations - Application Note 1358
One of the proposals for the IMT-2000 requirements for a 3G global wireless communications system is cdma2000. This application note describes mobile station design and measurement issues at the physical layer (layer 1) that may be different between cdma2000 and cdmaOne.

Notes d’application 2003-01-13

Comparison of Keysight Technologies IS-95/IS-2000 Test Sets
The existing products cover the IS-95 CDMA standard with a wealth of features,while the E5515C/E1962B provides IS-2000 coverage with a more limited feature set combined with numerous performance enhancements.

Notes d’application 2001-07-18

Standards Comparison for Key Measurements on Mobile Stations for cdma2000 and IS-98-C
This product note outlines the key differences between the standards for IS-95 (IS-98C) mobile stations and IS-98-D (cdma2000) mobile stations.

Notes d’application 2001-03-02

Multi-Coded Waveform Quality and Code Domain Measurements for cdma2000
Waveform quality is the basic measure of the performance of a CDMA system transmitter. The success of a CDMA system lies in its efficient use of power, and the waveform quality measurement gives the percent of power that correlates to the ideal code.

Notes d’application 2001-02-14

HPSK Spreading for 3G (AN 1335)
The objective of this Application Note is to provide an overview of Hybrid Phase Shift Keying (HPSK) and explain how to start making modulation quality measurements on the reverse link (uplink) of 3G spread-spectrum systems.

Notes d’application 2000-11-01

Understanding CDMA Measurements for Base Stations and Their Components (AN 1311)
This Application Note presents the fundamental measurement principles for the RF parametric tests performed on Code Division Multiple Access (CDMA) base stations and their components.

Notes d’application 2000-06-01

Performing cdma2000 Measurements Today (AN 1325)
cdma2000 is the 3GPP2 standard for 3G technology derived from cdmaOne. Although the standard has not yet been defined, R&D component and system engineers need to test their cdma 2000 designs today. This Application Note is a guide to cdma2000 testing based on established cdmaOne measurements...

Notes d’application 2000-05-22

ESG Option 201 Real-time IS-2000 Measurements
This Product Note discusses features, setup, and applications for the Keysight ESG Option 201 Real-time cdma2000 personality. It is intended to provide R&D designers working on DSPs, ASICs, and other firmware components of IS-95 and IS-2000 mobile phones with techniques for testing and...

Notes d’application 2000-04-03