Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 64

Sort:
Keysight Expands UXM Wireless Test Set LTE-A Capabilities with 4CC, 256 QAM, LTE-U, Cat 0 Support
Keysight announced verification of end-to-end IP data throughput for downlink rates of 587.5 Mbps with the E7515A UXM wireless test set. Using three component carriers (3CC) and 256 QAM in the downlink, Keysight achieved sustained bi-directional 3GPP UE category 11 data rates.

Press Materials 2015-05-21

Keysight Demonstrates LTE-Advanced Category 11 IP Data Throughput with UXM Wireless Test Set
Keysight announced verification of end-to-end IP data throughput for downlink rates of 587.5 Mbps with the E7515A UXM wireless test set. Using three component carriers (3CC) and 256 QAM in the downlink, Keysight achieved sustained bi-directional 3GPP UE category 11 data rates.

Press Materials 2015-05-06

Keysight to Demonstrate New UXM Wireless Test Set Features at Mobile World Congress
The E7515A UXM wireless test set is the industry’s leading UE test platform ready for 3CC/4CC, 256 QAM, UE categories 11-14. Visit us at Hall 2, Booth 212.

Press Materials 2015-02-12

Keysight Extends UXM Wireless Test Set LTE-A Carrier Aggregation Support with 3CC, TDD, Uplink
The E7515A UXM wireless test set adds features to address the rapidly evolving 3GPP LTE-Advanced carrier aggregation advancements.

Press Materials 2015-01-21

Keysight Demonstrates LTE-A 450 Mbps End-to-End IP Data Throughput with UXM
The E7515A UXM wireless test set provides verification of three component carrier (3CC) end-to-end IP data throughput.

Press Materials 2014-11-18

Keysight Technologies announces expanded TRX module and EXM wireless test set enhancements
Keysight Technologies Announces Expanded TRX Module and EXM Wireless Test Set Enhancements

Press Materials 2014-10-01

Keysight Expands Functional Test Capabilities, Delivers Greater RF Design Confidence
The E7515A UXM wireless test set includes support for LTE-A category 7 data throughput, expanded functional test capabilities, and in-depth RF performance verification using the X-Series measurement applications.

Press Materials 2014-09-18

Agilent's UXM Wireless Test Set Accelerates Marvell's LTE-Advanced Category 7 Chipset Development
Agilent and Marvell worked in concert to achieve sustained bidirectional 300 Mbps downlink/100 Mbps uplink data throughput using 3GPP release 10 downlink and uplink carrier aggregation.

Press Materials 2014-05-06

Agilent’s UXM Wireless Test Set Enables New Insights into LTE-Advanced Category 6 Chipsets, Devices
Introducing the E7515A UXM wireless test set, the most highly integrated signaling test set created for functional and RF design validation in the 4G era and beyond.

Press Materials 2014-02-13

E6640A EXM Wireless Test Set Ready for Volume Production of LTE-A, 802.11ac WLAN Devices
Agilent Technologies today announced the E6640A EXM wireless test set, which offers breakthrough manufacturing-test scalability in technology coverage, performance and capacity to test up to 32 cellular and wireless-connectivity devices in parallel.

Press Materials 2014-02-13

Agilent Technologies announces industry-first capabilities for envelope tracking
Agilent Technologies announced two software releases that support the design and verification of envelope tracking, a technique that improves the efficiency and linearity of power amplifiers used in mobile handsets

Press Materials 2013-06-04

Agilent Technologies announces 160-MHz bandwidth and real-time capability for MXA signal analyzer
Agilent Technologies announced significant enhancements to its midrange N9020A MXA X-Series signal analyzer. New options for 160-MHz analysis bandwidth and real-time spectrum analyzer (RTSA) capability address the challenges of measuring interference in the next generation of heterogeneous wireless networks.

Press Materials 2013-06-04

Agilent PXT Wireless Communications Test Set Selected by Tri-L Solutions for LTE Over-the-Air Test
Agilent Technologies Inc. (NYSE: A) today announced that Tri-L Solutions Inc. has selected Agilent's PXT wireless communications test set and integrated it with Tri-L Solutions SmarTest measurement software for testing LTE over the air.

Press Materials 2013-04-08

Agilent Technologies Introduces Industry's First LTE-Advanced 8x8 MIMO Signal-Generation and Analysi
Agilent Technologies Introduces Industry's First LTE-Advanced 8x8 MIMO Signal-Generation and Analysis Solutions

Press Materials 2013-01-03

Agilent Technologies and CATR (TMC) to Collaborate on TD-LTE MIMO
Agilent Technologies Inc. (NYSE: A) announced a memorandum of understanding has been signed with the China Academy of Telecommunication Research (Telecommunication Metrology Center), or CATR (TMC). The two organizations have agreed to work together on TD-LTE MIMO over-the-air (OTA) test research.

Press Materials 2012-09-13

Agilent Technologies Announces Wireless Communications Test Set with Innovative Multiport Adapter
Agilent Technologies introduced the E6607B EXT wireless communications test set and companion E6617A multiport adapter. Optimized for non-signaling testing, the EXT/MPA combination increases test throughput and reduces the cost of test in the manufacturing of current- and next-generation smartphones and tablets that contain multiformat and multiband technologies.

Press Materials 2012-08-01

Agilent Technologies Accelerates Early Wireless Design Verification with New Release of SystemVue
Agilent will demonstrate SystemVue 2012.06 along with a range of solutions for everything from circuit-level modeling through system verification for general RF, microwave, 4G communications, and aerospace/defense applications at DAC2012 (Booth 313), June 3-7, in San Francisco. SystemVue 2012.06 will also be demonstrated at IMS 2012/IEEE MTT-S (Booth 1015), June 19-21, in Montr al, Canada. A range of premier partner solutions will be available on Agilent Avenue and throughout the event area.

Press Materials 2012-06-05

Agilent Technologies Announces Voice-over-LTE Test System Developed with Brüel & Kjær
Transporting voice over a packet-based LTE cellular infrastructure poses challenges that make voice-quality testing essential. The Agilent and Brüel & Kjær solution combines standards-based test methods with real-world base station emulation, RF test and functional test to ensure that VoLTE phones will meet user's expectations.

Press Materials 2012-05-10

Agilent Technologies Introduces 6-GHz Signal Generators with Industry-Best Performance
Today's aerospace/defense environment requires enhanced radar performance to detect weak signals at long distances. To provide the pure and precise signals needed to test these designs, the MXG uses an innovative triple-loop synthesizer to deliver phase noise performance of -146 dBc/Hz at 1 GHz and 20 kHz offset. For developers of radar components such as mixers and analog-to-digital converters, the MXG also features industry-leading spurious performance of -96 dBc at 1 GHz.

Press Materials 2012-05-01

Agilent Technologies Enhances FieldFox RF Analyzers with Options for Measuring Time Domains and Chan
Agilent will demonstrate its new FieldFox options, along with solutions that cover everything from circuit-level modeling through system verification for general RF, microwave, 4G communications, and aerospace/defense applications at IMS 2012/IEEE MTT-S (Booth 1015), June 19-21, in Montr�al, Canada. A range of premier partner solutions will also be available on Agilent Avenue and throughout the event area.

Press Materials 2012-05-01

Agilent Technologies Named Oscilloscope Company of the Year
The award is based on Frost & Sullivan's recent analysis of the oscilloscope market. Frost & Sullivan ranked Agilent as the No. 2 company in 2009, but its rapid revenue growth since then has made it the leader in market penetration.

Press Materials 2012-04-25

Agilent Technologies Announces Test Software for Equipment Based on Altair TDD/FDD LTE Chipset

Press Materials 2012-02-28

ETS-Lindgren Announces Support of Agilent PXT Wireless Test Set for LTE Over-the-Air Testing
Agilent PXT performs OTA tests to industry standards and allows user equipment (UE) developers to characterize and optimize the behaviour of their designs. The EMQuest/PXT solution is offered with all ETS-Lindgren AMS for the testing of wireless devices

Press Materials 2012-02-03

Agilent Technologies Announces Bluetest Support of Agilent PXT for LTE Over-the-Air Testin
Agilent Technologies Inc. (NYSE: A) today announced that Bluetest AB now supports Agilent's PXT wireless communications test set. The Bluetest RTS (Reverberation Test System) uses the Agilent PXT test set to evaluate LTE devices over the air.

Press Materials 2012-02-02

Agilent Technologies Announces Industry's First Eight-Channel RF Measurement Solution Addressing LTE
Agilent Technologies Inc. (NYSE: A) today introduced industry-leading enhancements to its N7109A multi-channel signal analyzer for emerging multichannel LTE, LTE-Advanced and MIMO RF measurement requirements, including LTE antenna beamforming and LTE-Advanced carrier aggregation.

Press Materials 2012-02-02

1 2 3 Next