이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-25 / 32

정렬방식:
History of 802.11 - White Paper
The 802.11ax standard holds great promise, especially for dense deployments in both indoor and outdoor environments. Like any emerging standard; however it adopts present unique challenges.

어플리케이션 노트 2016-05-19

PDF PDF 1.36 MB
WLAN 802.11ac 제조 테스트를 위한 솔루션 - 어플리케이션 노트 (영어)
이 “WLAN 802.11ac 제조 테스트를 위한 솔루션” 어플리케이션 노트는 빠르고 유연하며 경제적인 교정 및 비시그널링을 이용하는 802.11ac 클라이언트와 인프라 테스트에 대한 통찰력을 제공합니다.

어플리케이션 노트 2015-02-04

Speed Time to Market with Consistent Measurements from R&D Through Manufacturing - Application Note
This white paper describes the benefits of having a choice of bench top or modular instruments that are supported by common software applications.

어플리케이션 노트 2014-11-17

Enhancing Measurement Performance for the Testing of Wideband MIMO Signals - White Paper
This white paper describes a method for characterization and correction of channel frequency response for BBIQ measurements over large bandwidths when using the Keysight M9703A and 89600 VSA software.

어플리케이션 노트 2014-08-03

PDF PDF 1.47 MB
Measuring the Burst Time-Gated Power Signal of Wireless Technologies Using Keysight Power Sensors
Measuring pulse, burst, or modulated signals for wireless technologies such as TDMA, GSM, WLAN, WiMAX, and LTE is very important because it is part of functionality testing and power amplifier module verification during the manufacturing process.

어플리케이션 노트 2013-07-08

Make Custom OFDM Measurements with 89600 VSA Software Option BHF - Application Note
Read about how to configure 89600 VSA software with Option BHF custom OFDM modulation analysis to analyze and troubleshoot new, custom, proprietary, generic, or non-standard OFDM signals.

어플리케이션 노트 2012-11-21

PDF PDF 4.27 MB
802.11ac Power Measurement and Timing Analysis - Application Note
This technical article illustrates how Keysight 8990B peak power analyzer able to help technicians and engineers perform some of the test requirements when developing 802.11ac power amplifier module

어플리케이션 노트 2012-09-02

PDF PDF 3.46 MB
WiGig 테스트 어플리케이션 노트를 위해 완전하고 유연한 솔루션 창출 (영어)
새로운 WiGig 제품을 개발할 때는 각 디바이스의 송신기/수신기 부분과 관련된 테스트 문제를 해결해야 합니다. 삼중 대역 디바이스에서 신호에는 세 가지 핵심 속성이 있으며 이들은 모두 2.4GHz, 5.0GHz에서 작동합니다.

어플리케이션 노트 2011-06-13

Custom OFDM Signal Generation Using SystemVue - Application Note
This application note describes a new comms standard based on OFDM which is provided by SystemVue 2011 to create both simulation and measurement, with links to the new 89600B VSA software for further demodulation and analysis.

어플리케이션 노트 2010-12-09

How to migrate from the N4010A to N8300A for WLAN testing (Part 4)

어플리케이션 노트 2009-06-11

N8300A: Techniques for optimizing WLAN device testing (Part 3)

어플리케이션 노트 2009-05-12

PDF PDF 483 KB
N8300A: Implement a WLAN test plan using SCPI programming (Part 2)

어플리케이션 노트 2009-04-27

PDF PDF 687 KB
N8300A: Introduction to a WLAN manufacturing test plan and theory of implementation (Part 1)

어플리케이션 노트 2009-04-21

PDF PDF 507 KB
Simplify dc current drain measurements and analysis on WLAN Network cards
Minimizing current drain is critical to the success of new WLAN Network cards. High or excessive current drain can reduce the host device battery operating time considerably.

어플리케이션 노트 2008-06-04

MIMO Wireless LAN PHY Layer (RF) Operation & Measurement Application Note 1509
This application note is intended to provide an understanding of MIMO radio operation as it applies to WLAN, and the test configurations for multi-channel radios.

어플리케이션 노트 2008-04-30

MIMO Manufacturing Solution - Application Note
Compares two of the most popular MIMO manufacturing test methodologies, including examples to illustrate the relative merits.

어플리케이션 노트 2007-07-10

N4010A Programming Made Easy for WLAN Applications - Application Note
This application note shows WLAN test developers and application engineers how to create effective integration test plans and manufacturing test sequences for the N4010A test set.

어플리케이션 노트 2007-04-17

PDF PDF 954 KB
RF Testing of WLAN Products- Application Note
This Application note discusses the modulation technology behind several wireless LAN standards and the measurement techniques that can be used to trouble shoot and quantify their RF performance.

어플리케이션 노트 2007-01-10

전류 드레인 분석으로 WLAN 네트워크 카드 설계 및 테스트 향상 (AN 1468)
This application note explains how to simplify the complex task of accurately measuring and evaluating the current drain of a WLAN network card for its various operating modes.

어플리케이션 노트 2006-12-14

N4010A Wireless Connectivity Test Set Performance Guide, Application Note
This guide characterizes the performance of the N4010A wireless connectivity test set and the 89601A vector signal analysis (VSA) software combination

어플리케이션 노트 2004-06-29

PDF PDF 455 KB
Next-Generation WLAN Manufacturing Test Solutions
This application note begins with a brief introduction to IEEE 802.11 technologies, followed by a description of the golden radio-based test system and its main limitations for WLAN manufacturing.

어플리케이션 노트 2004-05-28

802.11 WLAN 수신기 테스트에 E4438C ESG 및 Signal Studio 사용
This 16 page application note describes how to properly construct the MAC header, user files, and frames for WLAN signal generation using Signal Studio software.

어플리케이션 노트 2003-10-01

Receiver Minimum Input Level Sensitivity
Receiver minimum input level sensitivity is the minimum specified rf level of a WLAN signal that a WLAN receiver will receive and demodulate.

어플리케이션 노트 2003-09-22

Improve the Circuit Evaluation Efficiency of Wireless LAN Chip Set Design (AN 1463-2)
This application note introduces circuit and component characteristics for the WLAN chipset design process using the ENA Series network analyzers. The topics highlighted are balanced measurements, fixture characterizations, and impedance matching.

어플리케이션 노트 2003-08-14

PDF PDF 133 KB
무선 LAN을 위한 등화 기법 및 OFDM 문제해결 - AN 1455
The discussions and measurements described here apply most specifically to the Keysight 89600 Series vector signal analyzers and their wireless networking measurement software.

어플리케이션 노트 2003-05-01

1 2 다음