이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

상세 분류

상세분류 제거

산업/기술

분야별 검색결과

1-25 / 39

정렬방식:
Using MATLAB to Create Keysight Signal and Spectrum Analyzer Applications - Application Note
Learn to use MATLAB software to configure, control, and acquire data from X-Series signal and spectrum analyzers, and then use scripts to create, modify and execute custom analyzer applications.

어플리케이션 노트 2016-11-16

PDF PDF 9.69 MB
Extending the Life of Test Systems that Support Long-term Programs - Application Note
As an original equipment manager (OEM), we offers efficient and effective alternatives that can extend the life of systems and ensure that the individual instruments are meeting their warranted spec.

어플리케이션 노트 2015-06-12

Effectively Maintaining and Troubleshooting Military Communication Systems - Application Note
This application note covers the “what” and “how” of effective testing for best performance in military communication systems. Two examples will highlight what’s possible: field test and verification of radar systems.

어플리케이션 노트 2014-09-11

Analyzing Frequency Stability in the Frequency and Time Domains - Application Note
Describes both methods with an emphasis on practical, cost-effective solutions. For those who are new to the time-domain perspective, two proven frequency-to-time conversion methods are also presented.

어플리케이션 노트 2014-08-11

Using RF Recording Techniques to Resolve Interference Problems - Application Note
This application note looks at functionality that is crucial to today’s commercial wireless and EW applications where interference-related issues are highly problematic.

어플리케이션 노트 2014-08-03

PDF PDF 1.96 MB
Using Flexible Digital Modulation Testing for Satellite Regenerative Payloads - Application Note
This application note focuses on solutions for the issues that create risks in the integration of mixed-signal systems with a mix of software and hardware tools. Examples focus on measurements of error vector magnitude (EVM), which is a key figure of merit for modulated signals implemented in either analog or digital form.

어플리케이션 노트 2014-08-01

Achieving High-Quality Microwave Measurements with the Right Test Accessories - Application Note
With high-performance instrumentation and accessories pushing the envelope of advanced high-frequency applications, it is now more crucial than ever for engineers to select the right test accessories.

어플리케이션 노트 2013-03-06

Understanding Phase Noise Needs and Choices in Signal Generation
This application note reviews the fundamentals of phase noise and takes a closer look at architectural choices and the effects of various functionality alternatives.

어플리케이션 노트 2013-01-14

6 Hints for Enhancing Measurement Integrity in RF/Microwave Test Systems - Application Note

어플리케이션 노트 2012-04-30

Generating and Applying High-Power Output Signals
This application note describes both the inner workings of the PSG with Option 521 and the applications of its high-power output signals.

어플리케이션 노트 2009-09-30

Building Hybrid Test Systems. Ensuring success in two common development scenarios - Application Not
Application Note 1465-33. When you migrate to a hybrid system that includes LXI along with GPIB, VXI, PXI, or any other architecture, two scenarios are most typical, minimum development time and maximum overall performance

어플리케이션 노트 2008-10-15

Multiport Solutions for E5071C ENA RF Network Analyzers Using External Switches
This app note describes how to expand the potential of multiport solutions for network analysis using the E5071C, with external electro-mechanical switches on handling high and low power signal measurements.

어플리케이션 노트 2008-03-10

Improving Throughput with Fast RF Signal Generator Switching
This note describes techniques for optimizing RF signal generators within ATE systems to reduce test times and improve throughput.

어플리케이션 노트 2007-09-19

AN1465-26 LAN/LXI를 포함하도록 GPIB 시스템 수정
이 어플리케이션 노트는 일반적인 GPIB 테스트 시스템에서 한 대의 계측기를 교체하는 프로세스를 안내하며 간단한 시스템 소프트웨어 변경을 통해 이러한 작업이 구현되는 방식을 보여줍니다.

어플리케이션 노트 2007-05-10

Using Linux in Your Test Systems: Linux Basics (AN 1465-27)
If you haven’t used Linux in test applications, this document will provide a detailed overview. Topics include: A brief Linux history, why use Linux, free tools available for application development and an instrument control overview.

어플리케이션 노트 2007-05-08

LXI-compliant oscilloscope boosts efficiency in ATE systems
The LXI (LAN eXtensions for Instrumentation) standard specifies the interaction of proven, widely used standards to enable fast, efficient, and cost-effective creation and reconfiguration of test systems.

어플리케이션 노트 2007-04-02

PDF PDF 286 KB
Migrating system software from GPIB to LAN/LXI (AN 1465-25) - Application Note
Migrating system software from GPIB to LAN/LXIis the sixth application note in a series designed to help you manage the shift to LXI from GPIB.

어플리케이션 노트 2007-02-02

Using Synthetic Instruments in Your Test System (AN 1465-24)
This note represents a brief history of SI, compares a rack-and-stack system to an SI-based system, descibes the initial applications of SIs, and illustrates the emulation of conventional instruments with SIs.

어플리케이션 노트 2006-08-28

How to Use VXI and PXI in Your New LXI Test System (AN 1465-23)

어플리케이션 노트 2006-06-06

Next-generation Test Systems: Advancing the Vision with LXI (AN 1465-16)

어플리케이션 노트 2006-05-01

PDF PDF 263 KB
LXI: GPIB, PXI 및 VXI 능가: 주요 테스트 과제 극복
이 어플리케이션 노트에서는 LXI 표준의 주요 속성, 시스템 개발 시 주요 과제 및 LXI가 핵심 도전과제를 해결하는 방법 및 LXI 디바이스틀 통해 구현된 새로운 테스트 가능성에 대해 중점적으로 다루고 있습니다.

어플리케이션 노트 2006-01-17

Calibrating Signal Paths in RF/Microwave Test Systems (AN 1465-19)

어플리케이션 노트 2005-10-31

Using LAN in Test Systems: Applications (1465-14) - Application Note and Example Programs
Topics include balancing cost, convenience and security in three common LAN scenarios: sharing instruments, remote monitoring and data acquisition, and functional test systems. Includes downloadable example programs.

어플리케이션 노트 2005-04-01

Using LAN in Test Systems: Setting up System I/O (AN 1465-15) - Application Note
This set of application notes shows you how to simplify test system integration by utilizing open connectivity standards such as local area networking (LAN). The collective goal of these notes is to help you produce reliable results, meet your throughput requirements and stay within your budget.

어플리케이션 노트 2005-03-29

PDF PDF 263 KB
Introduction to Test-System Design (AN 1465-1)

어플리케이션 노트 2005-01-20

1 2 다음