Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discutez avec un expert

Support technique

Mesure Electronique

Support by Product Model Number:

1-25 sur 62

Tri:
Surveying the Best Ways to Test Antennas and Antenna Arrays - Application Note
This application note provides insights into testing antenna and antenna arrays, and is part 6 in a series of radar application notes.

Notes d’application 2017-01-09

PDF PDF 2.17 MB
New Pulse Analysis Techniques for Radar and EW - Application Note
This app note discusses the best tools for different types of pulse analysis, along with display and analysis techniques for various signals and measurement goals.

Notes d’application 2016-05-26

Measuring Radar Signals with Vector Signal Analyzers and Wideband Instruments - Application Note
This application note provides insights into measuring radar signals with vector signal analyzers and wideband instruments and is part 4 in a series of radar application notes.

Notes d’application 2016-05-04

PDF PDF 3.62 MB
Defining the Pulsed Radar Signal and the Essential Measurements of Signal Power - Application Note
This application note defines that nature of actual radar signals and describes practical ways to measure power in those signals.

Notes d’application 2016-03-30

PDF PDF 2.49 MB
A Framework for Understanding: Deriving the Radar Range Equation - Application Note
Radar scans three-dimensional space to gather information about detected objects such as location, shape and speed. This entire process is described in this app note by the radar range equation.

Notes d’application 2016-03-03

PDF PDF 1.19 MB
Techniques for Precision Validation of Radar System Performance in the Field - Application Note
This application note provides an overview of field testing radar systems and Line Replaceable Units (LRU) using high-performance FieldFox combination analyzers.

Notes d’application 2015-07-28

Extending the Life of Test Systems that Support Long-term Programs - Application Note
As an original equipment manager (OEM), we offers efficient and effective alternatives that can extend the life of systems and ensure that the individual instruments are meeting their warranted spec.

Notes d’application 2015-06-12

Techniques for Precise Power Measurements in the Field - Application Note
This application note will discuss techniques for measuring average and peak power and the associated equipment options available for field testing.

Notes d’application 2015-05-22

Radar Development Using Model-Based Engineering
This application note describes how SystemVue is well suited for use in model-based engineering. It is for system engineers, directors of engineering and people involved in the development of Radar.

Notes d’application 2015-04-14

PDF PDF 1.59 MB
Addressing the Challenges of High-Speed Digital I/O for Aerospace Defense – Application Note
This application note will also discuss test challenges and commercial test solutions for fiber digital I/O technologies to help mitigate risk in upgrading to fiber-based technologies.

Notes d’application 2015-01-21

Generating Multi-Dimensional Signals to Test Radar/EW Systems
This application note describes how to use SystemVue to generate multi-dimensional signals for testing Radar and modern Electronic Warfare (EW) systems.

Notes d’application 2014-11-09

Effectively Maintaining and Troubleshooting Military Communication Systems - Application Note
This application note covers the “what” and “how” of effective testing for best performance in military communication systems. Two examples will highlight what’s possible: field test and verification of radar systems.

Notes d’application 2014-09-11

Radar Measurements - Application Note
This application note focuses on the fundamentals of measuring basic pulsed radars and measurements for more complex or modulated pulsed radar systems.

Notes d’application 2014-08-22

PDF PDF 6.84 MB
Analyzing Frequency Stability in the Frequency and Time Domains - Application Note
Describes both methods with an emphasis on practical, cost-effective solutions. For those who are new to the time-domain perspective, two proven frequency-to-time conversion methods are also presented.

Notes d’application 2014-08-11

Streaming, Analysis and Playback of RF Interference Signals in AD Applications - Application Note
Streaming, Analysis and Playback of RF Interference Signals in Aerospace and Defense Applications –looks at countering undesirable signals using a system based on COTS hardware and software when intentional interference is created to disrupt the operation of a victim receiver.

Notes d’application 2014-08-03

Simulation and Verification of Pulse Doppler Radar Systems - Application Note
Keysight SystemVue illustrates key algorithms in modern Pulsed Doppler radar system design, and also connects to Keysight sources and signal analyzers to verify hardware performance.

Notes d’application 2014-08-02

PDF PDF 10.44 MB
Simulating Power Supply Transients and Noise in the Satellite and Defense
5991-0655EN,satellite,defense,power supply transients and noise,aerospace/defense,defense,A/D

Notes d’application 2014-08-02

Creating a Complete and Flexible Solution for WiGig Testing Application Note
When developing new WiGig products, testing must address the transmitter and receiver portions of each device. In a tri-band device, signals have three key attributes: they operate at 2.4 GHz, 5.0 GHz

Notes d’application 2014-08-01

Using Flexible Digital Modulation Testing for Satellite Regenerative Payloads - Application Note
This application note focuses on solutions for the issues that create risks in the integration of mixed-signal systems with a mix of software and hardware tools. Examples focus on measurements of error vector magnitude (EVM), which is a key figure of merit for modulated signals implemented in either analog or digital form.

Notes d’application 2014-08-01

Time Sidelobe Measurements to see Performance of Compressed-Pulse Radars - Application Note
This application brief defines problems seen in measurements of compressed-pulse radars, describes the time sidelobe method, and outlines uses of this approach.

Notes d’application 2014-08-01

Improving Radar Performance by Optimizing Overall Signal-to-Noise Ratio
Better noise-figure measurements enhance characterization of excess noise in receivers.

Notes d’application 2014-08-01

OFDMA Introduction and Overview for Aerospace and Defense Applications - Application Note
Provides a brief introduction to the concepts of OFDM and OFDMA, with an eye toward the special considerations and environments for A/D applications.

Notes d’application 2014-05-15

PDF PDF 1.56 MB
Pulsed Carrier Phase Noise Measurements - Application Note
This application note discusses basic fundamentals for making pulsed carrier phase noise measurements.

Notes d’application 2014-03-13

Overcoming the Challenges of Simulating Phased-Array Radar Systems
This application note discusses a solution that reduces design cycles, significantly reduces cost and allows you to simulate a scenario before taking it to land, skies and seas.

Notes d’application 2014-02-26

A Flexible Testbed to Evaluate Potential Co-Existence Issues Between Radar and Wireless Systems
This application note offers suggestions that assert finding and addressing problems in a lab environment is typically much less costly than trying to correct issues after deployment to the field.

Notes d’application 2014-01-08

PDF PDF 1.18 MB

1 2 3 Page suivante