Hable con un experto

Technical Support

Electronic Measurement

Find by Product Model Number: Examples: 34401A, E4440A

Refine the List

remove all refinements

By Topic

By Type of Content

By Product Category

1-25 of 38

Sort:
What are the login and passwords that are used on the X-Series Signal Analyzers?
There are two different login accounts: User account and Administrator account

FAQ 2015-01-13

If I have N9051A Pulse Measurement Software, how do I upgrade to N9051B?
Order N9051B Option A2B to receive a user-installed software license, which causes any existing N9051A licenses to be recognized as N9051B licenses. The N9051B-2FP license is required, while all others are optional and independent of each other.

FAQ 2014-10-21

How do I upgrade to “Deep Capture” for the N9051B Pulse Measurement Software?
Deep Capture is a software license upgrade performed by the end-user. This is only available for the N9051B version, order N9051B Option 5FP.

FAQ 2014-10-21

Are trial licenses available for the N9051B Pulse Measurement Software?
Yes, a trial license is available to let you explore the N9051B free of charge for 30 days. The trial has all features enabled.

FAQ 2014-10-21

I ordered the N9051A, but it is no longer installed on the signal analyzer. The N9051B is installed, but my N9051A licenses don’t work. What shou
The N9051B is the recommended replacement for N9051A. The N9051A license can be upgraded by adding a low-cost N9051B-A2B license.

FAQ 2014-10-21

When I redeem a license certificate for a final license for the N9051B Pulse software, I need my HostID. Where do I find this?
On the X-Series signal analyzer, press System > Show > System. In the table, around the 10th row, you will find “HostID”, this is composed of the model and serial number.

FAQ 2014-10-21

How does the N9051B Pulse Measurement Software GUI work?
The GUI is standard MS Windows type: pull-down menus, dialogs, on-screen buttons, etc. A USB mouse and keyboard are required. The PC-ststandard keys of the X-SA front panel are recognized: numbers (digits 0-9, decimal point, minus, BkSp); plus Enter, Select, Escape, Ctrl, Alt, Del, and Tab; and the Mode key.

FAQ 2014-10-21

How is the N9051B Pulse Measurement Software delivered, installed and licensed?
Important: N9051B runs only on the CPU inside an X-Series signal analyzer, which must be Windows 7 and 64-bit. See the FAQ for further details.

FAQ 2014-10-21

What does the “Deep Capture” option give me in the N9051B Pulse Measurement Software?
The N9051B software operates in “batch” mode: digitizing the RF signal into IQ samples, captured a time-segment into memory, and then analyze it. Review the entire FAQ for full details.

FAQ 2014-10-21

Where can I find manuals for discontinued and obsolete Hewlett-Packard, Agilent and Keysight test equipment?
Most Keysight products have PDF manuals that can be found on product pages. Other vendors also supply old manuals.

FAQ 2014-08-01

What is 802.11af, and does Keysight have a solution for testing 802.11af devices?
Learn more about Keysight's 802.11af solutions…

FAQ 2014-02-28

How does the 89601BU "update and subscription service" work?
Option 200 is mandatory and you cannot use the 89600 VSA software without having Option 200 installed. Software version.....

FAQ 2014-01-27

How to add N9051A, Pulse Measurement Software, to the mode key selections.
X-Series signal analyzer with Windows 7 and Software versoin A.12.xx installed may not list N9051A as selection avilable under the Mode key.

FAQ 2013-05-16

Is the N9068A phase noise application supported by N9030A PXA Option EXM external mixing?
Yes, the N9068A phase noise application is supported when using N9030A PXA Option EXM external mixing. In addition, Option EXM supports normal spectrum analyzer applications, including PowerSuite one-button measurements.

FAQ 2012-10-25

Does the PXA (with Option EXM) support the 11970VE01 mixer (50 to 85 GHz)?
Yes.

FAQ 2012-10-25

Will the external mixer Option EXM support the 11974 Series preselected mixers?
There are no plans to support the 11974 Series preselected mixers with the N9030A PXA.

FAQ 2012-10-25

What external mixers will work with my PXA/mmW EXA and how do I order them?
Currently, the N9030A PXA/mmW EXA with Option EXM will work with either the 11970 Series (with the exception of the 11970K) or ) or external mixers from other vendors such a OML Inc. mixers.

FAQ 2012-10-17

What file formats does the 89601A VSA software support for signal waveforms?
Recorded data from the following files can be interpreted by the 89600: ASCII (.txt and .csv), Binary (89600 SDF .sdf, .dat), Binary (E3238 .cap), Binary (N5510A .bin), MATLAB 7 (or earlier, .mat)

FAQ 2012-05-28

Do the E4406A, PSA Series and 89600 VSA Software report Peak Code Domain Error for W-CDMA and cdma2000?
Yes. The screen capture below shows a W-CDMA Modulation Accuracy measurement on the E4406A and PSA Series, and Peak Code Domain Error is reported in the results table.

FAQ 2012-05-26

How do a take a sweep with both the Quasi-Peak and EMI Average detector at the same time with an MXE EMI Receiver?
Switch to EMI Receiver mode...

FAQ 2012-05-10

Why do I get a Meas Uncal message when I select either the Quasi-Peak or EMI Average detector for taking a full band sweep with the MXE EMI Receiver?
Sweeptime has reached its maximum. See complete FAQ for further details...

FAQ 2012-05-10

How do I make the signal list compare measurements made with the detectors used to different limit lines in my MXE EMI Receiver?
Meas Setup, Detectors (Measure)...

FAQ 2012-05-10

Can the PXA support external mixing for frequencies >325 GHz?
A third-party vendors, like Virginia Diodes, Inc. may be able to work with you on providing a custom external mixing solution to cover frequencies up to 1 THz.

FAQ 2012-02-24

What preamplifier options can be used with the N9030A PXA frequency range options?
Refer to the table included...

FAQ 2012-02-24

Will the PXA work with the N8975AZ-Kxx block down converters for noise figure to 110 GHz?
Yes, you will be able to use the N8975AZ-Kxx noise figure block converters with the PXA.

FAQ 2012-02-24

1 2 Next