1-2 of 2

Sort:
When I put a N6700 family DC Power Supply module into my mainframe, I get error 207 listed on the front panel when I turn the unit on. What does th...
Error 207 means “calibration file version error”. This means that the module was calibrated in a N6700B mainframe with a version of firmware that is newer than the version of firmware in the mainframe where it is generating the error.

FAQ 2012-07-30

What is the part number for the output connector for the N67XX?
This information is found on pg 24 of the N6700B user guide.

FAQ 2011-07-08