Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

51-75 of 133

Sort:
What is the settling time for the E364xA supplies?
For the E364xA series, Settling Time is defined as the maximum time required for the output voltage to change from 1% to 99% (or vice versa) following receipt of a VOLTage or APPLy command from the GPIB or RS-232 interface. The settling time is <...

FAQ 2010-09-08

How can I read the calibration date for an E363xA or an E364xA power supply?
The calibration message containing the factory calibration date can be retrieved by using the "CALibration:STRing" command. After the calibration is completed, the date can be changed with the " CALibration:STRing " command.

FAQ 2010-09-08

How can I eliminate the flashing single digit in the front-panel display?
The flashing digit indicates the digit of the output parameter displayed that can be changed by turning the front panel knob. Use the resolution key (<) or (>) to move the flashing digit to the left or right until the flashing stops.

FAQ 2010-09-08

E363xA and E364xA: Disabling the Control Knob
To disable the front-panel control knob, scroll the flashing digit on the front-panel display to the right or left using the selection keys (<) or (>) until the flashing digit disappears. Notice that the control knob and all front-panel keys are n...

FAQ 2010-09-08

How can you change or view the secondary address in the 6030A, 6031A, 6032A, 6033A, 6035A, or 6038A power supplies?
These products have been retrofitted with SCPI language capability, in addition to the original or compatibility mode. Secondary addressing of these products is only available in SCPI mode.

FAQ 2010-09-08

66xxA and E36xxA: Determining Power Supply Constant Current Mode
The power supply cannot be "put" into the constant current mode.

FAQ 2010-08-27

How can I prevent a loading delay when using the Measurement Manager with Microsoft® .NET 2.0 on a computer that is connected to a LAN…
To prevent a loading delay when using the Measurement Manager (AMM) with Microsoft® .NET 2.0, follow the instructions below:….

FAQ 2010-08-09

What are the differences between the Keysight N6705A DC Power Analyzer and the N6705B DC Power Analyzer?
The N6705B mainframe has new labeling that identifies which knobs have secondary functions when you press them...

FAQ 2010-08-09

For the E363xA and E364xA Bench Power Supply, the display update speed when the "Display Limit" function is on is different from …
For the E363xA and E364xA Bench Power Supply (BPS), the display update speed is different because....

FAQ 2010-08-09

When will Keysight USB modular instruments and USB Modular DAQs supports Windows 7?
For 32 bit Windows 7, the supportability of modular instruments and DAQs will happen...

FAQ 2010-07-18

66000A: Setting Dwell Time
The List mode can contain up to 20 Voltage, Current or Dwell steps if controlled over the GPIB, or up to 8 steps if controlled from the optional keyboard...

FAQ 2010-05-26

661xC and 663xB: Power Supply Output Transition Time

FAQ 2010-05-16

I sent a Keysight 663xx power supply in for service and I received a unit that has a different serial number. How do I transfer my 14565B software...
When receiving a unit back from a service request, write down the model number and the new serial number

FAQ 2010-05-16

How can I clear the content of power supply memory for programmable E36xxA power supplies?
There is no way to clear the contents of the store/recall states. They can be overwritten as many times as desired but there is not an explicit way to delete saved states.

FAQ 2010-05-16

Why USB modular instruments (U272XA, U2741A, U2751A and U2761A) is not detectable by E5813A?
PC is failed to enumerate the USB modular instrument.

FAQ 2010-04-09

Is U2722A compatible with E5813A?
No

FAQ 2010-03-22

Is U2723A compatible with E5813A?
No

FAQ 2010-03-22

How can I make U8001A or U8002A to be in Output On stage upon powered up?
Order option AUT.

FAQ 2010-02-01

What is the voltage and current limit setting for U8001A and U8002A upon powered up?
Same as the setting before power cycle.

FAQ 2010-02-01

What does the LGA option on the N6751A and N6752A modules offer?
The LGA option is strongly recommended on the N6751A/52A modules. The LGA option stands for Large Gate Array.

FAQ 2009-12-20

Is there any variations in up/down-programming times from channel to channel in E3646A, E3647A, E3648A and E3649A?
Channel to channel up/down-programming variations time is less than 30ms

FAQ 2009-08-06

How can noise be superimposed on the output of a dc power supply?
Keysight power supplies are designed to have the lowest noise that is practically possible. For some applications it is desirable to simulate the effect of noise on the output, for example to test system immunity to power line disturbances.

FAQ 2009-06-14

Does the Measurement Manager (AMM) run on Window Vista operating system?
Yes. The Measurement Manager (AMM) rev. 1.8.3.0 and above will able to run on Windows Vista ...

FAQ 2009-06-10

662xA: Replacing GPIB Printed Circuit Board Assembly

FAQ 2009-03-30

Does the Keysight Measurement Manager (AMM) support regional language settings other than English (US)?
Yes, the Keysight Measurement Manager (AMM) supports regional language settings other than English (US)….

FAQ 2009-01-12

Previous 1 2 3 4 5 6 Next