Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 133

Sort:
For an auto-ranging power supply, how do I determine the maximum output current for any operating voltage? | Keysight
You will always obtain rated output power of the unit along any point of the auto-ranging operating curve.

FAQ 2015-09-08

Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

Where can I find manuals for discontinued and obsolete Hewlett-Packard, Agilent and Keysight test equipment?
Most Keysight products have PDF manuals that can be found on product pages. Other vendors also supply old manuals.

FAQ 2014-08-01

Why are USB modular instruments (U2700 Series) and USB DAQ modules (U2300, U2500, U2600 Series) not detectable by the E5810B?
Establish the connection between the USB modular Instrument and the PC directly, and then disconnect the device from the PC (while it’s still powered-on), and connect to E5810B.

FAQ 2014-04-17

How can I source a sinusoid waveform on the B2961A/B2962A?
Click the above link for details.

FAQ 2013-12-24

How can I source an exponential waveform on the B2961A/B2962A?
Click the above link for details.

FAQ 2013-12-24

What is the difference among Trigger Types on Single View?
Click the above link for details.

FAQ 2013-09-16

How can I source a pulsed signal on the B2961A/B2962A?
Click the above link for details.

FAQ 2013-09-16

What is the equivalent command to "Output after Sweep" parameter on "Sweep" dialog?
It should be [:SOURce]:FUNCtion:TRIGgered:CONTinuous. Once you send it with the parameter "ON", the parameter is set to "END VALUE".

FAQ 2013-09-16

What is the difference among data query commands such as ":FETCh?", ":MEASure?", ":READ?", :SENSe:DATA?"?
They have the function to query data similarly but there is some difference among them. Click the above link for details.

FAQ 2013-09-16

How can I find the sensing type of the channels on the B2961A/B2962A?
If the low terminal state of the channel is set to FLOATING, you can see the status indicator on GUI.

FAQ 2013-03-11

Can I upgrade from B2961A to B2962A?
No, you cannot upgrade from B2961A to B2962A.

FAQ 2013-03-11

How can I update its firmware on the B2961A/B2962A?
Click the above link for details.

FAQ 2013-03-11

How can I find the power-on state setting of the B2961A/B2962A?
You can find the power-on state setting on the System Start-up dialog box. Click the above link for details.

FAQ 2013-03-11

How can I perform a self calibration on B2961AB2962A?
Click the above link for details.

FAQ 2013-03-11

How can I save or load the measurement setups on the B2961A/B2962A?
Click the above link for details.

FAQ 2013-03-11

How to configure the time constant of the output filter with the B2961A/B2962A?
The time constant of the output filter can be configured on the Output Filter dialog box. Click the above link for details.

FAQ 2013-03-11

Where can I get LabVIEW Plug and Play Instrument Driver for B2961A/B2962A?
You can get LabVIEW Plug and Play Instrument Driver for B2961A/B2962A from NI.com.

FAQ 2013-03-11

Can I set the different limit values for each of polarities on the B2961A/B2962A?
Yes, it's possible by enabling V/I Limit for Each Polarity. Click the above link for details.

FAQ 2013-03-11

I can't source as low noise signal as expected from the B2961A/B2962A with the Low Noise Filter.
Click the above link for details.

FAQ 2013-03-11

Can B2961A/B2962A connect its output to the ground when the output is switched off?
Yes, the B2961A/B2962A can connect its output to the ground by specifying the output-off state to "ZERO" when the output is switched off.

FAQ 2013-03-11

What kind of interface can I use to control the B2961A/62A?
The GPIB, USB and LAN are available to control the B2961A/62A.

FAQ 2013-03-11

The Keysight B2961A/B2962A shows the message "Interlock terminal is open" and don't accept to input voltage more than 42 V.
Click the above link for details.

FAQ 2013-03-11

How can I find the power-on program setting of the B2961A/B2962A?
You can find the power-on program setting on the System Start-up dialog box. Click the above link for details.

FAQ 2013-03-11

How can I enable Over Voltage/Current Protection function on the B2961A/B2962A?
Click the above link for details.

FAQ 2013-03-11

1 2 3 4 5 6 Next