Discutez avec un expert

Support technique

Mesure Electronique

Recherche par numéro de modèle du produit: Exemples : 34401A, E4440A

Affiner la liste

retirer tout le raffinement

Par industrie/technologie

Par type de contenu

1-25 sur 44

Tri:
LTE-Advanced: Technology and Test Challenges 3GPP Releases 10, 11, 12 and Beyond - Application Note
This application note summarizes the ITU requirements for 4G and the 3GPP requirements for LTE-Advanced, including the expected timeline. Key solution proposals for LTE-Advanced are also presented with a look at Release 10 and beyond. Lastly anticipated design and test challenges are addressed.

Notes d’application 2014-09-01

Performing Digital-IF/RF-Digital Bit Error Rate Measurement - Application Note
This Application Note describes how to use Keysight Instruments and ADS EDA software to verify RF performance measures such as BER and EVM for end-to-end digital-IF/RF-digital systems--from bits in to bits out.

Notes d’application 2014-07-31

PDF PDF 531 KB
Quickly Validate Designs for DOCSIS 3.1 Compliance - Application Brief
This “DOCSIS 3.1 Test Solution" app brief gives insight into Keysight solutions that can be used for testing DOCSIS 3.1 transmitters, receivers and components.

Notes d’application 2014-06-24

Envelope Tracking and Digital Pre-Distortion PA Testing for LTE User Terminal Components - App Note
This application note discusses measurement solutions for power amplifier testing using Envelope Tracking (ET) and lookup table (LUT)-based DPD.

Notes d’application 2014-03-07

PDF PDF 3.73 MB
Testing WLAN Devices According to the 802.11x Standards - Application Note
This application note provides a survey of transmitter/receiver test requirements for 802.11a, b, g, n, ac. It also presents an overview of Keysight’s solutions for WLAN testing.

Notes d’application 2013-10-21

Easily Create Custom Waveforms with Waveform Creator - Application Note
This application note provides instructions for how to create custom waveform plug-ins using the M9099 Waveform Creator application software

Notes d’application 2013-10-01

PDF PDF 593 KB
GNSS Technologies and Receiver Testing - Application Note
This application note provides information on GNSS technologies including GPS, Compass, Beidou, Galileo, and Glonass, along with the related receiver test challenges and solutions.

Notes d’application 2013-05-08

Multichannel Measurements in MIMO 802.11ac Baseband IQ Simulation, Design & Test - Application Note
This solution brief will show Keysight Technologies' complete, end-to-end solution for multichannel measurements of 802.11ac BBIQ simulation, design and test.

Notes d’application 2013-04-05

PDF PDF 748 KB
DVB-T and DVB-T2 Transmitter Test Challenges - Application Note
This application note presents a discussion of the DVB-T and DVB-T2 systems and the measurement challenges facing developers of transmitters for these systems.

Notes d’application 2013-02-27

PDF PDF 986 KB
Testing DVB-T and DVB-T2 Receivers - Application Note
This application note presents a discussion of the DVB-T and DVB-T2 systems and the measurement challenges facing developers of receivers such as set-top-boxes.

Notes d’application 2013-02-02

PDF PDF 716 KB
Addressing the Challenges of Deploying Single Frequency Networks DVB-T & DVB-T2 - Application Note
This application addresses the challenges of deploying SFN systems for digital video broadcasting and describe's Keysight's solutions for meeting these challenges.

Notes d’application 2013-01-17

PDF PDF 1.58 MB
Optimizing Transceiver Test with the Keysight M9381A Vector Signal Generator
Accelerate transceiver test throughput with the fast Keysight M9381A PXIe Vector Signal Generator. Achieve cost reductions in test while maintaining high test quality.

Notes d’application 2012-08-29

Creating and Optimizing 802.11ac Signals Application Note
This application note details how to create and optimize 802.11ac signals using the N7617B Signal Studio for WLAN 802.11a/b/g/n/ac software with Keysight's RF signal generators to get the highest quality signals from the instruments.

Notes d’application 2012-07-19

PDF PDF 2.10 MB
Testing New-generation Wireless LAN - Application Note
This application note introduces the new WLAN new-generation testing technology of 802.11ac. Keysight's 802.11ac software allows engineers to view and troubleshoot all 802.11ac modulation formats.

Notes d’application 2012-05-22

PDF PDF 881 KB
Transition from 2G/3G to 3.9G/4G Base Station Receiver Conformance Test - Application Note
This application note will help you migrate from 2G/3G to 3.9G/4G BTS test. Various test requirements are explained as well as how to perform those tests using the new X-Series signal generators.

Notes d’application 2012-04-16

PDF PDF 581 KB
LTE-Advanced Signal Generation and Measurement Using SystemVue - Application Note
This application note introduces changes in Release 10 of the 3GPP specification for LTE-Advanced, a new generation of the LTE standard that promises dramatic improvements in throughput.

Notes d’application 2010-12-23

Designing and Testing 3GPP W-CDMA Base Stations (Including Femtocells) - Application Note
W-CDMA is one of several wideband digital cellular technologies competing for the third-generation (3G) cellular market.

Notes d’application 2010-08-01

Stimulus-Response Testing for LTE Components - Application Note
This note focuses on the 3GPP LTE specifications that present some new challenges for manufacturers of components and equipment for LTE systems.

Notes d’application 2010-05-03

Conduct DVB-T/H Conformance Tests with Keysight's Real-time DVB-T/H Digital Video Solution
This application note provides an introduction to the performance test requirements for DVB-T/H receivers, as defined in EICTA MBRAI 2.0, and it describes test setup and configurations.

Notes d’application 2010-04-30

PDF PDF 904 KB
Typical GPS Receiver Verification Tests Using a GPS Signal Simulator - Application Note
This paper describes typical GPS receiver verification tests using a GPS signal simulator. The tests are used to verify functionality of embedded GPS receivers in mobile consumer products such as cell phones and other handheld receivers.

Notes d’application 2010-03-04

Measuring ACLR Performance in LTE Transmitters - Application Note
This note focuses on the adjacent channel leakage-power ratio (ACLR) test, a vital one for LTE.

Notes d’application 2010-01-07

GPS Receiver Testing - Application Note
This paper describes GPS receiver tests used for GPS verification. It also introduces an application capable of generating the required GPS signals for a repeatable and flexible test environment.

Notes d’application 2010-01-04

CMMB Conformance Testing using the PXB with N7623B Signal Studio for Digital Video
This application note introduces CMMB technologies and conformance test requirements and explains the test setup and configurations for the N5106A PXB and N7623B Signal Studio for Digital Video

Notes d’application 2010-01-04

PDF PDF 936 KB
MIMO in LTE Operation and Measurement-Excerpts on LTE Test - Application Note
Focuses on MIMO radio operation and implementation as it applies to Long Term Evolution (LTE). MIMO (spatial multiplexing) is one of several multiple antenna techniques being implemented in LTE.

Notes d’application 2009-10-06

MIMO Performance and Condition Number in LTE Test - Application Note
Topics include basic concepts of MIMO, how antenna and channel correlation affects system performance, recommendations for the best measurement tools to use when developing LTE products and systems.

Notes d’application 2009-10-06

1 2 Page suivante