Contact an Expert

Technical Support

Electronic Measurement

Find by Product Model Number: Examples: 34401A, E4440A

201-225 of 392

Sort:
The modulation (AM, FM, phase, and pulse modulation) on my E8663B does not turn on. What can I do to use this signal generator's modulation?

FAQ 2010-09-08

For waveform 5-pack licenses, can a customer generate a waveform in Signal Studio software not connected to a MXG/ESG, export to a location on thei...
Yes, this method can be used when customers only want to tweak waveform parameters and not evaluate RF performance beforehand.

FAQ 2010-09-08

What is the difference between the USB port on the front and rear panels of the MXG?
The MXG front panel USB port is for a USB Type A connector; USB rear connector is for a USB 5-pin Mini-B connector.

FAQ 2010-09-08

What happens to the RF output signal when Output Blanking is set to Off, On, or Auto?

FAQ 2010-09-08

For waveform 5-pack licenses, is there a way to have password protection against licensing a 5-pack waveform to prevent someone from inadvertently ...
No, this will be considered as an enhancement request for future releases.

FAQ 2010-09-08

For waveform 5-pack licenses, once a waveform is licensed, can it be copied and stored for archival purposes?
Yes, a licensed waveform can be copied and renamed for archival purposes. Be aware that the waveform can still only played on the ESG or MXG to which it has been licensed.

FAQ 2010-09-08

For waveform 5-pack licenses, is there a grace-period where I can still revoke/replace a waveform once it has been licensed?
Once the waveform is licensed, that license is permanent and cannot be revoked or replaced.

FAQ 2010-09-08

What is signal creation software?
Keysight's broad set of Signal Studio and Embedded signal creation software products enable the generation of a wide range of application specific test signals using the MXG, ESG, and PSG vector signal generators.

FAQ 2010-09-08

Where can I find LabView examples for the ESG, PSG, MXG, and E8663B signal generators?

FAQ 2010-09-08

Will the E8257D/67D PSG work with both AC and DC detection on the 8757D scalar network analyzer?
Yes. The E8257D/E8267D PSG with ramp sweep (Option 007) will work with both AC and DC detection on the 8757D scalar analyzer.

FAQ 2010-09-08

Will a PCI-X slot work for the N5101A Baseband Studio PCI Card?
Yes, PCI-X should be backward compatible with conventional PCI 2.2.

FAQ 2010-09-08

Will the MXG support Baseband Studio?

FAQ 2010-09-08

What are the file formats used for the MXG?

FAQ 2010-09-08

Can I upgrade my analog MXG to a vector MXG?
No, there is no upgrade from an analog MXG to a vector MXG.

FAQ 2010-09-08

For waveform 5-pack licenses, can the 30-day license attached to each waveform 5-pack license be activated whenever the customer wants –or– do the ...
The 30-day license for the evaluation of waveforms (Option D01) may be activated at anytime, although they must be used one at a time.

FAQ 2010-09-08

For waveform 5-pack licenses, since a waveform can be copied and renamed, is there protection from a user inadvertently licensing the same signal?
Yes, there is protection against using a license slot on a redundant signal. A unique identifier is associated and stored with each signal created by Signal Studio applications. It is this identifier that is licensed on the MXG or ESG signal gen...

FAQ 2010-09-08

How is a Signal Studio application license installed?
A Signal Studio license is installed using the License Manager software utility available for download and on the CD shipped with the Signal Studio software.

FAQ 2010-09-08

Where can I find information on MXG error messages?
A complete list of error messages is provided on the CD-ROM supplied with the MXG.

FAQ 2010-09-08

How do I erase or sanitize the memory on my MXG?
When moving the signal generator from a secure development environment, there are several security functions you can use to remove classified proprietary information from the instrument.

FAQ 2010-09-08

What is Option ALB on the MXG signal generator?
Option ALB on the MXG enables LAN LXI class B compliance. This option is included standard on all new MXG’s shipped since June 2009. MXG’s shipped before June 2009 can be upgraded by ordering option N51xxAK-ALB. Contact Keysight for more details.

FAQ 2010-09-03

Does the N9310A have a SCPI command similar to a LEARN string to query a complete description of its current setup?
The N9310A does not have a specific command which will provide all the data on one request.

FAQ 2010-08-15

The N9310A display is not updated when in remote control. Is this normal?
Running your N9310A in remote mode brings forward the following two symbols...:

FAQ 2010-08-13

How do I connect the MXG signal generator to a PC using LAN?
There are several methods for connecting the signal generator to the PC...

FAQ 2010-05-16

Why after using the binblockread() function in MATLAB, all subsequent data transfers return bad data/info?
The binblockread() function doesn't read the terminating character.

FAQ 2010-05-07

What is the meaning of this statement from the data sheet: "The acoustic noise is louder than typical Keysight equipment."
The instrument has a set of fans to remove internally generated heat. These fans generate ...

FAQ 2010-05-07

Previous 1 2 3 4 5 6 7 8 9 10 ... Next