Contact an Expert

Technical Support

Electronic Measurement

Find by Product Model Number: Examples: 34401A, E4440A

151-175 of 392

Sort:
How can I generate TETRA and DECT signal for basic interference testing in many compliance test houses, which are bursted, just like the real standard
You can use PRAM to simulate spectrally correct signals for TETRA and DECT for bursted signals. See the X-Series User’s Guide for further information.

FAQ 2012-04-30

Are the function generators all inside the MXG and EXG X-Series signal generators?
Yes, with Option 303, multifunction generator. See the data sheets for full capabilities.

FAQ 2012-04-30

Can we support atmospheric conditions with N7609B GPS on the N5182B MXG or N5172B EXG X-Series signal generators?
Yes.

FAQ 2012-04-30

Can you bypass the internal reference chain with clean rubidium source on the X-Series signal generators?
The 10 MHz path is very clean and works with an external reference. The 1-50 MHz tunable path is noisier, see the data sheets for more details.

FAQ 2012-04-30

Can you master/slave MXG and EXG or must they all be the same model number?
You can master/slave first generation MXG N5182A with the N5182B MXG and N5172B EXG X-Series signal generators. The N5172B or N5182B must be the master.

FAQ 2012-04-30

What are the plans to upgrade the N5102A DSIM, if I want it to go to 160 MHz BW on the N5182B MXG or N5172B EXG X-Series signal generators?
DSIM will be able to run up to 200MSa/sec.

FAQ 2012-04-30

Can you change the attenuation on external I and Q individually on the N5182B MXG or N5172B EXG X-Series signal generators?
Yes, improved over the first-generation MXG.

FAQ 2012-04-30

Is the phase coherency supported on the X-Series signal generators?
Yes, with Option 012, LO in/out for phase coherency.

FAQ 2012-04-30

Is the tuning speed the same as switching speed on the X-Series signal generators?
Yes, switching speed is the same as tuning speed.

FAQ 2012-04-30

Is the output power improved on the X-Series signal generators?
Yes, specified output power changed from +23 dBm to +24 dBm for MXG. For both MXG and EXG X-Series signal generators, standard output power has improved significantly. See the data sheet for more details.

FAQ 2012-04-30

Will the N5171B and N5172B EXG X-Series signal generator have an OCXO option for improved drift rate?
No

FAQ 2012-04-30

Is BER available on the N5182B MXG or N5172B EXG X-Series signal generators?
No, Option UN7, Internal Bit Error Rate Analyzer, is not available at introduction.

FAQ 2012-04-30

Do the new sources de-crypt waveforms in the same way as the legacy sources? Can we just use pre-existing waveforms?
Yes. First-generation MXG N5182A Signal Studio N76xxB waveforms will play in new sources. Exception will be N7613A Signal Studio for Fixed WiMAX which has the legacy N76xxA structure.

FAQ 2012-04-30

What is the size and format of the removable memory (SD card) on the X-Series signal generators?
8 GB SD card, RAW storage. This is available with Option 006 instrument security and removable memory card.

FAQ 2012-04-30

Will the MXG and EXG X-Series signal generator work with the analyzers for ESC (external source control)?
They will not work at the time of introduction. The next version of the X-Series signal analyzer firmware (late 2012) should support the analog versions. The vector versions are to be added in the future, but the timing is undetermined.

FAQ 2012-04-30

Can we add a SCPI logger/history for past few commands on the X-Series signal generators?
Yes, we have this capability.

FAQ 2012-04-30

Using the E8267D PSG Vector Signal Generator in a System
Browse through this index of resources generated to ease your test system design challenge

FAQ 2012-03-30

What is the polynomial to generate the PN9 sequence in the ESG-D Series RF signal generator?
We follow the ITU standards for PN sequences.

FAQ 2012-03-13

ESG and ESG-D Series: Selectivity Measurements
The ESG-D Series provides the appropriate adjacent channel power (ACP)

FAQ 2012-03-13

I downloaded the Service Support Software for the E44xxB ESG-A/D from our website. The software is asking for a username and password. What is the...
The E44xxB ESG-A/D Service Support Software username and password are provided.

FAQ 2012-03-13

I downloaded the Service Support Software for the E44xxB ESG-AP/DP from our website. The software is asking for a username and password. What is t...
The E44xxB ESG-AP/DP Service Support Software username and password are provided.

FAQ 2012-03-13

I downloaded the Service Support Software for the 8648X from our website. The software is asking for a username and password. What is the username...
The 8648 Service Support Software username and password are provided.

FAQ 2012-03-13

Why doesn't the Keysight License Manager connect to my ESG?
Your ESG needs firmware revision C.04.84 or above...

FAQ 2012-03-02

How do I upgrade the PSA Series Memory Upgrade Option ANE?
The memory can be upgraded to 64 Megabytes by ordering E4440AU Option ANE. Click here for additional information.

FAQ 2012-02-26

My PSA Series Spectrum Analyzer Shows error +605 Data Corrupt or Stale, NRAM copy of !....
The non-volatile RAM battery has expired. The replacement battery P/N is 1420-0314C. Click here for additional information.

FAQ 2012-02-26

Previous 1 2 3 4 5 6 7 8 9 10 ... Next