Contact an Expert

Technical Support

Electronic Measurement

Find by Product Model Number: Examples: 34401A, E4440A

101-125 of 392

Sort:
What is the data content in the single satellite waveform files? Is it real navigation data?
The waveform files contain alternating 0s and 1s for the data. Real navigation data is not included since it is impossible for a receiver to calculate a location fix using only a single satellite signal.

FAQ 2012-11-21

How much baseband memory do I need in the ESG/PSG for opt. 422 scenario generator?
The scenario files reside on the hard drive until one is selected for playback, and then it is loaded into the baseband memory.

FAQ 2012-11-21

Is there a way to transfer sets of waveforms to each signal generator without having to connect the N7609B software to each instrument?
Yes. All of the waveform files are available on your PC when you install the N7609B application; they are in the application SW folder

FAQ 2012-11-21

Where can I find additional scenario files?
There is a link for additional scenario files on the product Web page for the E4438C-409 that takes you to this page...

FAQ 2012-11-21

Do I have to upgrade my N7620A licenses?
You may want to upgrade your N7620A licenses to N7620B licenses so that they can be managed using the Keysight License Manager.

FAQ 2012-10-28

What do the N7620B upgrade licenses cost?
All N7620B license upgrades are free.

FAQ 2012-10-28

Will the N7620B software recognize my N7620A licenses?
The N7620B software recognizes all N7620A licenses except for the N8241A, N6030A, and N9330A external Arbs.

FAQ 2012-10-28

How do I manage my N7620A licenses?
The N7620A software allows you to view your original N7620A licenses.

FAQ 2012-10-28

How do I install my N7620B licenses?
All N7620B licenses are managed with the Keysight License Manager.

FAQ 2012-10-28

I have the basic functionality license for N7620A and I want to get the advanced capability license. What should I do?
Install the N7620B software and get the N7620B-QFP, or N7620B-QTP advanced capability license

FAQ 2012-10-28

How do I upgrade my N7620A licenses?
Contact the customer contact center at Keysight Technologies.

FAQ 2012-10-28

Can MXG or EXG support more than 2 USB power sensors?
EXG/MXG are only able to display the measurements from 2 USB sensors at the same time. Up to ...

FAQ 2012-10-19

How do I upgrade my E8663B PSG Analog Signal Generator?
Find Information on Hardware Upgrades, Instrument Software, etc....

FAQ 2012-10-11

What types of files are installed on my machine when I download the Download Assistant for MATLAB?
During installation, the Download Assistant software installs a series of MATLAB functions as MATLAB files, including two MATLAB file examples, into your directory of choice. To learn how to use these functions,see ...

FAQ 2012-08-09

What type of connection is required in order to transfer data from PC to signal generator for MATLAB?
Data transfer from the PC to the signal generator requires a GPIB or Ethernet (TCP/IP) connection.

FAQ 2012-08-09

Do I need Instrument Control Toolbox if I already have MATLAB installed?
If you already have MATLAB installed, type “ver” at the MATLAB command line to see if you already have Instrument Control Toolbox installed.

FAQ 2012-08-09

Which signal generators are compatible with the Download Assistant for MATLAB?
Download Assistant V2.0 requires you to have MATLAB’s Instrument Control Toolbox installed. MATLAB supports instrument control, instrument configuration, and data transfer with its Instrument Control Toolbox, which allows a wide variety of Keysight instruments to be programmed from within the MATLAB environment.

FAQ 2012-08-09

Is the Instrument Control Toolbox required for all versions of Download Assistant?
Download Assistant V2.0 requires you to have MATLAB’s Instrument Control Toolbox installed.

FAQ 2012-08-09

Why is the Upgrade Assistant not able to detect my instrument?
If the Upgrade Assistant not able to detect you instrument, but the instrument is able to be ping on the IO libraries and works fine on the web interface, ensure that the socket SCPI is turn on.

FAQ 2012-07-17

Using the E8257D PSG Analog Signal Generator in a System
Browse through this index of resources generated to ease your test system design challenge

FAQ 2012-06-26

How do I upgrade my signal generator firmware?
Click here for information on how to upgrade your firmware.

FAQ 2012-06-12

How do I find internal instrument information, such as the firmware revision?
Click here to learn how to access internal instrument information.

FAQ 2012-06-08

Can the 8657x Signal Generator be turned on with the RF output off?
No, it can't. When a DUT could be destroyed by high RF output.

FAQ 2012-06-08

What should I do in order not to set the ARB Sample Clock each time I recall a stored ARB file?
Provided are the settings for Header Information of an ARB waveform file and the Procedure.

FAQ 2012-06-07

How can I transfer a "state" from one PSG to another?
Using ftp, the transferred states are not visible in the Recall list.

FAQ 2012-06-07

Previous 1 2 3 4 5 6 7 8 9 10 ... Next