Parla con un Esperto

Technical Support

Electronic Measurement

Find by Product Model Number: Examples: 34401A, E4440A

201-225 of 599

Sort:
Where can I find additional scenario files?
There is a link for additional scenario files on the product Web page for the E4438C-409 that takes you to this page...

FAQ 2012-11-21

Are scenario files compatible between the E4438C-409 and the N7609B?
Yes, the N7609B can use any of the scenario files created for the E4438C-409...

FAQ 2012-11-21

When simulating a signal that includes GLONASS and Galileo my receiver is reporting different satellite IDs than shown in the Signal Studio, why?
While GPS satellites are commonly identified by the pseudorandom codes (PRN) that they use, there is no industry standard yet for how to refer to the GLONASS or Galileo satellites.

FAQ 2012-11-21

How does the N7609B calculate the total output power in relation to the number of visible satellites during a scenario?
When you initially turn on the simulation, the Satellite Settings page will update the “Power” column to show the power of each satellite in dBm.

FAQ 2012-11-21

How do you calculate the individual output power of each satellite?
The ESG/PSG power level is distributed equally among the satellites.

FAQ 2012-11-21

I’m using the N7609B with an X-series signal generator. Can I generate a real-time GNSS signal without being connected to Signal Studio?
Yes, if you are using a stored scenario file, but not if you are using continuous scenario generation mode.

FAQ 2012-11-21

How do I obtain the NMEA GGA message file of trajectory information in order to create a dynamic scenario for a moving GNSS receiver?
There are several ways to do this...

FAQ 2012-11-21

What is the maximum sampling rate for the GNSS waveforms?
The sampling rates vary depending on which constellation is being simulated, and they range from 2.044 MSa/s for GLONASS up to 24.552 MSa/s for Galileo.

FAQ 2012-11-21

What is the data content in the single satellite waveform files? Is it real navigation data?
The waveform files contain alternating 0s and 1s for the data. Real navigation data is not included since it is impossible for a receiver to calculate a location fix using only a single satellite signal.

FAQ 2012-11-21

How much baseband generator memory is needed in the signal generator to use basic mode waveforms?
The amount of memory that is needed depends on how many waveform files you need to have in the instrument memory at one time.

FAQ 2012-11-21

Is there a way to transfer sets of waveforms to each signal generator without having to connect the N7609B software to each instrument?
Yes. All of the waveform files are available on your PC when you install the N7609B application; they are in the application SW folder

FAQ 2012-11-21

Playback of M9392A Recorded Files on the M9381A PXI Vector Signal Generator
Example program for the M9391A PXI Vector Signal Generator. This program will load waveforms captured by the M9392A PXI Vector Signal Analyzer into the M9381A PXI Vector Signal Generator for playback. A document will describe the procedure and the programming instructions for loading and playing back of these waveform files.

Programming Example 2012-11-06

ZIP ZIP 319.72 KB
What do the N7620B upgrade licenses cost?
All N7620B license upgrades are free.

FAQ 2012-10-28

Do I have to upgrade my N7620A licenses?
You may want to upgrade your N7620A licenses to N7620B licenses so that they can be managed using the Keysight License Manager.

FAQ 2012-10-28

How do I manage my N7620A licenses?
The N7620A software allows you to view your original N7620A licenses.

FAQ 2012-10-28

Will the N7620B software recognize my N7620A licenses?
The N7620B software recognizes all N7620A licenses except for the N8241A, N6030A, and N9330A external Arbs.

FAQ 2012-10-28

How do I install my N7620B licenses?
All N7620B licenses are managed with the Keysight License Manager.

FAQ 2012-10-28

I have the basic functionality license for N7620A and I want to get the advanced capability license. What should I do?
Install the N7620B software and get the N7620B-QFP, or N7620B-QTP advanced capability license

FAQ 2012-10-28

How do I upgrade my N7620A licenses?
Contact the customer contact center at Keysight Technologies.

FAQ 2012-10-28

Can MXG or EXG support more than 2 USB power sensors?
EXG/MXG are only able to display the measurements from 2 USB sensors at the same time. Up to ...

FAQ 2012-10-19

How do I upgrade my E8663B PSG Analog Signal Generator?
Find Information on Hardware Upgrades, Instrument Software, etc....

FAQ 2012-10-11

Do I need Instrument Control Toolbox if I already have MATLAB installed?
If you already have MATLAB installed, type “ver” at the MATLAB command line to see if you already have Instrument Control Toolbox installed.

FAQ 2012-08-09

Is the Instrument Control Toolbox required for all versions of Download Assistant?
Download Assistant V2.0 requires you to have MATLAB’s Instrument Control Toolbox installed.

FAQ 2012-08-09

Which signal generators are compatible with the Download Assistant for MATLAB?
Download Assistant V2.0 requires you to have MATLAB’s Instrument Control Toolbox installed. MATLAB supports instrument control, instrument configuration, and data transfer with its Instrument Control Toolbox, which allows a wide variety of Keysight instruments to be programmed from within the MATLAB environment.

FAQ 2012-08-09

What types of files are installed on my machine when I download the Download Assistant for MATLAB?
During installation, the Download Assistant software installs a series of MATLAB functions as MATLAB files, including two MATLAB file examples, into your directory of choice. To learn how to use these functions,see ...

FAQ 2012-08-09

Previous 1 2 3 4 5 6 7 8 9 10 ... Next