Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

76-100 of 757

Sort:
How can I find the low terminal state of the channels on the B2961A/B2962A?
If the low terminal state of the channel is set to FLOATING, you can see the status indicator on GUI.

FAQ 2013-03-11

How can I set up Power-on State of the B2961A/B2962A?
It is possible to store the desired instrument condition as Power-on State. Click the above link for details.

FAQ 2013-03-11

I can't source as low noise signal as expected from the B2961A/B2962A with the Low Noise Filter.
Click the above link for details.

FAQ 2013-03-11

What kind of interface can I use to control the B2961A/62A?
The GPIB, USB and LAN are available to control the B2961A/62A.

FAQ 2013-03-11

The Keysight B2961A/B2962A shows the message "Interlock terminal is open" and don't accept to input voltage more than 42 V.
Click the above link for details.

FAQ 2013-03-11

How can I enable Over Voltage/Current Protection function on the B2961A/B2962A?
Click the above link for details.

FAQ 2013-03-11

How can I configure Trigger Output Signals with the B2961A/B2962A?
Click the above link for details.

FAQ 2013-03-11

Can I upgrade from B2961A to B2962A?
No, you cannot upgrade from B2961A to B2962A.

FAQ 2013-03-11

How can I update its firmware on the B2961A/B2962A?
Click the above link for details.

FAQ 2013-03-11

How to configure the time constant of the output filter with the B2961A/B2962A?
The time constant of the output filter can be configured on the Output Filter dialog box. Click the above link for details.

FAQ 2013-03-11

Can the B2961A/B2962A step the source value immediately after the value is changed by its rotary knob?
Yes, it's possible by enabiling Immediate V/I Update function. Click the above link for details.

FAQ 2013-03-11

How can I find the sensing type of the channels on the B2961A/B2962A?
If the low terminal state of the channel is set to FLOATING, you can see the status indicator on GUI.

FAQ 2013-03-11

How can I find the power-on state setting of the B2961A/B2962A?
You can find the power-on state setting on the System Start-up dialog box. Click the above link for details.

FAQ 2013-03-11

Can I set the different limit values for each of polarities on the B2961A/B2962A?
Yes, it's possible by enabling V/I Limit for Each Polarity. Click the above link for details.

FAQ 2013-03-11

How can I find the power-on program setting of the B2961A/B2962A?
You can find the power-on program setting on the System Start-up dialog box. Click the above link for details.

FAQ 2013-03-11

Do temperature changes affect the factory channel correction calibration?
temperature changes, channel correction calibration, factory correction calibration,x-series signal generators

FAQ 2013-02-26

For User channel correction calibration, is it better to do a spot user cal or over an overlapping range?
Overlapping is good idea, but not required.

FAQ 2013-02-26

How long is the factory channel correction calibration good?
The factory channel correction lasts the life of the source.

FAQ 2013-02-26

Can running user correction calibration over a narrower range improve calibration?
No, the number of points is always fixed at a 5 MHz interval

FAQ 2013-02-26

When you perform the User channel correction routine, do you need to compensate for the cable between spectrum analyzer or power meter and source?
No, the cable error has been calibrated.

FAQ 2013-02-26

How does DC calibration affect channel corrections?
If a DC calibration is run with channel corrections applied, this may or may not degrade performance slightly.

FAQ 2013-02-26

What is the difference between the User channel correction and the factory channel correction?
See the EXG data sheet or MXG data sheet

FAQ 2013-02-26

Do User channel corrections cover multiple attenuator steps?
Yes. Bypass step, 0 dB step, and 5 dB step.

FAQ 2013-02-26

For User channel correction calibration, when frequency is tuned out of “user” correction frequency range, is factory correction applied?
Yes, we apply smoothing between cal arrays to ensure no discontinuity.

FAQ 2013-02-26

For User channel correction, how many unique calibration files are supported?
We can support thousands on internal solid state drive.

FAQ 2013-02-26

Previous 1 2 3 4 5 6 7 8 9 10 ... Next