Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

51-75 of 757

Sort:
What is the equivalent command to "Output after Sweep" parameter on "Sweep" dialog?
It should be [:SOURce]:FUNCtion:TRIGgered:CONTinuous. Once you send it with the parameter "ON", the parameter is set to "END VALUE".

FAQ 2013-09-16

Can the B2900A Series of SMU sweep voltage source by the know on the front panel?
Yes, it's possible by enabiling Immediate V/I Update function. Click the above link for details.

FAQ 2013-09-16

Does the B2900A Series of SMUs have Source Memory Sweep Function?
No, the B2900A Series of SMUs doesn't have Source Memory Sweep Function as Keithley 2400 has.

FAQ 2013-09-16

Can I use N1294A-021/022 low noise filters with B2901A/02A/11A/12A SMU?
No, they aren't recommended to be used with the Keysight B2901/02/11/12A SMUs.

FAQ 2013-09-16

How to use the interlock to output more than ±42V?
B2900A has interlock detection with the digital I/O on the rear pannel. Click the link for details.

FAQ 2013-09-16

How can I source a pulsed signal on the B2961A/B2962A?
Click the above link for details.

FAQ 2013-09-16

What is the difference among data query commands such as ":FETCh?", ":MEASure?", ":READ?", :SENSe:DATA?"?
They have the function to query data similarly but there is some difference among them. Click the above link for details.

FAQ 2013-09-16

What is the difference among Trigger Types on Single View?
Click the above link for details.

FAQ 2013-09-16

How can the B2900A Series of SMU source pulses whenever it receives an external trigger signal?
It can do it by configuring a digital I/O pin to be used for an external trigger signal. Click the above link for details.

FAQ 2013-09-16

How do I upgrade my E8267D PSG Vector Signal Generator?
Find Information on Hardware Upgrades, Instrument Software, etc....

FAQ 2013-08-23

How do I upgrade my E8257D PSG Analog Signal Generator?
Find Information on Hardware Upgrades, Instrument Software, etc....

FAQ 2013-08-20

How do I get the N5162A, N5182A, N5172B, N5182B default waveform files from Keysight and download them into the instrument memory?
The arbitrary waveform files are stored in the non-volatile memory of the N5182A/N5162A MXG when they ship out of the factory. In case these waveform files are accidentally deleted, a user can retrieve them through either of the following methods...

FAQ 2013-08-14

When should I use Real-time Custom Modulation vs. Arb Custom Moduation vs. Creating my own IQ waveform?
It is always easier to use the real-time custom modulation mode inside the instrument until you run out of the flexibility.

FAQ 2013-08-14

How do you clear the M9381A PXIe Vector Signal Generator and M9380A PXIe CW Source modules memories?
Please refer to the documents for a comprehensive listing of memory installed into these products.

FAQ 2013-08-06

How do I change the 10 MHz reference source if Signal Studio for pulse building doesn’t detect the reference?
Most of the time, Signal Studio will recognize the reference; however, it can be changed in the download -> customize menu.

FAQ 2013-05-16

Is there a way to put insert a missing pulse into the signal?
Yes, you can add a “Off time” object to the pulse pattern and change the duration to meet your pulse requirements.

FAQ 2013-05-16

Are there any options to adjust the pulse definitions within Signal Studio for pulse building?
No, at the moment the rise and fall times are defined by their 0-100 percent points and the pulse width is defined to be the 100-100 percent point.

FAQ 2013-05-16

Where can I find information or example programs using the API for Signal Studio?
The Signal Studio for pulse building help file has information and example programs under the API control chapter.

FAQ 2013-05-16

How do I find the HOST ID of my instrument or PC?
Keysight software options are licensed to many different types of hardware, using a unique hardware identifier called the Host ID. The Host ID is composed of 1, 2, or 3 elements, depending upon the software model and the target hardware platform.

FAQ 2013-05-07

How much programming compatibility does exist between 81101A, 81104A, 81110A and 81150A, 81160A?
The implemented 81150A, 81160A SCPI command set is based on Keysight’s 81101A, 81104A, 81110A Pulse Pattern Generator product family. Therefore, most of the commands available for that instrument family are also available in the 81150A, 81160A models.

FAQ 2013-03-21

What USB storage devices are compatible with the MXG?
The MXG is now compatible with most USB storage devices.

FAQ 2013-03-13

I can't source as low noise signal as expected from the B2961A/B2962A with the Low Noise Filter.
Click the above link for details.

FAQ 2013-03-11

Can I set the different limit values for each of polarities on the B2961A/B2962A?
Yes, it's possible by enabling V/I Limit for Each Polarity. Click the above link for details.

FAQ 2013-03-11

How can I perform a self calibration on B2961AB2962A?
Click the above link for details.

FAQ 2013-03-11

Can the B2961A/B2962A step the source value immediately after the value is changed by its rotary knob?
Yes, it's possible by enabiling Immediate V/I Update function. Click the above link for details.

FAQ 2013-03-11

Previous 1 2 3 4 5 6 7 8 9 10 ... Next