Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

151-175 of 755

Sort:
When simulating a signal that includes GLONASS and Galileo my receiver is reporting different satellite IDs than shown in the Signal Studio, why?
While GPS satellites are commonly identified by the pseudorandom codes (PRN) that they use, there is no industry standard yet for how to refer to the GLONASS or Galileo satellites.

FAQ 2012-11-21

How can I set up Power-on State of the B2901/02/11/12A?
It is possible to store the desired instrument condition as Power-on State. Click the above link for details.

FAQ 2012-11-21

Are scenario files compatible between the E4438C-409 and the N7609B?
Yes, the N7609B can use any of the scenario files created for the E4438C-409...

FAQ 2012-11-21

How do you calculate the individual output power of each satellite?
The ESG/PSG power level is distributed equally among the satellites.

FAQ 2012-11-21

How does the N7609B calculate the total output power in relation to the number of visible satellites during a scenario?
When you initially turn on the simulation, the Satellite Settings page will update the “Power” column to show the power of each satellite in dBm.

FAQ 2012-11-21

I’m using the N7609B with an X-series signal generator. Can I generate a real-time GNSS signal without being connected to Signal Studio?
Yes, if you are using a stored scenario file, but not if you are using continuous scenario generation mode.

FAQ 2012-11-21

How do I obtain the NMEA GGA message file of trajectory information in order to create a dynamic scenario for a moving GNSS receiver?
There are several ways to do this...

FAQ 2012-11-21

How much baseband memory do I need in the ESG/PSG for opt. 422 scenario generator?
The scenario files reside on the hard drive until one is selected for playback, and then it is loaded into the baseband memory.

FAQ 2012-11-21

Where can I find additional scenario files?
There is a link for additional scenario files on the product Web page for the E4438C-409 that takes you to this page...

FAQ 2012-11-21

Can Keysight provide a location accuracy specification for the Option 409?
Unfortunately, Keysight cannot provide a location accuracy specification because this is dependent on the GPS receiver.

FAQ 2012-11-21

Can I use the triaxial cable with B2900A?
Yes. You can use the triaxial cable by using the N1294A adaptor.

FAQ 2012-11-20

Can I use N1294A-001/002 banana-triaxial adapter with B2961A/62A?
Yes, it is recommended that the banana-triaxial adapter should be used with B2961A/62A in the case of < 1nA sourcing.

FAQ 2012-11-11

Can ULNF and LNF be used with the B2901/02/11/12A?
No. Using these optional filters with the Keysight B2901/02/11/12A SMUs is not recommended.

FAQ 2012-11-01

How do I manage my N7620A licenses?
The N7620A software allows you to view your original N7620A licenses.

FAQ 2012-10-28

How do I upgrade my N7620A licenses?
Contact the customer contact center at Keysight Technologies.

FAQ 2012-10-28

Will the N7620B software recognize my N7620A licenses?
The N7620B software recognizes all N7620A licenses except for the N8241A, N6030A, and N9330A external Arbs.

FAQ 2012-10-28

Do I have to upgrade my N7620A licenses?
You may want to upgrade your N7620A licenses to N7620B licenses so that they can be managed using the Keysight License Manager.

FAQ 2012-10-28

Can MXG or EXG support more than 2 USB power sensors?
EXG/MXG are only able to display the measurements from 2 USB sensors at the same time. Up to ...

FAQ 2012-10-19

How do I upgrade my E8663B PSG Analog Signal Generator?
Find Information on Hardware Upgrades, Instrument Software, etc....

FAQ 2012-10-11

Does the B2901/02/11/12A have any search function?
No, the B2901/02/11/12A doesn't have any search function which the analyzers such as the B1500A have.

FAQ 2012-10-09

I cannot store the channel 2 measurement condition to USB memory stick, why not?
The instrument may be configured to use the conventional command set. Click the above link for details.

FAQ 2012-10-09

The password is required to access the instrument.
The password is required to access the instrument compliant with the LXI specification. Click the above link for details.

FAQ 2012-10-09

The channel 2 in the B2902A or B2912A doesn't receive any SCPI commands.
The instrument may be configured to use the conventional command set. Click the above link for details.

FAQ 2012-10-09

How to determine the frequency for Sin function of Quick IV List Sweep?
Frequency = 1 / ( (360 [degree] / X Step [degree]) * Trigger Period )

FAQ 2012-10-09

Where is the cfunc.h header file called for in the 33120A Users Guide example program?
Some older versions of the IB Libraries provided this header file during installation. This file was required to access commands from the IB command library.

FAQ 2012-09-05

Previous 1 2 3 4 5 6 7 8 9 10 ... Next