Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

176-200 of 756

Sort:
Where is the cfunc.h header file called for in the 33120A Users Guide example program?
Some older versions of the IB Libraries provided this header file during installation. This file was required to access commands from the IB command library.

FAQ 2012-09-05

When I put a N6700 family DC Power Supply module into my mainframe, I get error 207 listed on the front panel when I turn the unit on. What does th...
Error 207 means “calibration file version error”. This means that the module was calibrated in a N6700B mainframe with a version of firmware that is newer than the version of firmware in the mainframe where it is generating the error.

FAQ 2012-07-30

Why is the Upgrade Assistant not able to detect my instrument?
If the Upgrade Assistant not able to detect you instrument, but the instrument is able to be ping on the IO libraries and works fine on the web interface, ensure that the socket SCPI is turn on.

FAQ 2012-07-17

Using the E8257D PSG Analog Signal Generator in a System
Browse through this index of resources generated to ease your test system design challenge

FAQ 2012-06-26

How Do I Find My Host Information?
The Host ID is the model and/or serial number of the product, both of which can be found on the serial number label on the back of the instrument.

FAQ 2012-06-14

How do I upgrade my signal generator firmware?
Click here for information on how to upgrade your firmware.

FAQ 2012-06-12

How do I find internal instrument information, such as the firmware revision?
Click here to learn how to access internal instrument information.

FAQ 2012-06-08

Can the 8657x Signal Generator be turned on with the RF output off?
No, it can't. When a DUT could be destroyed by high RF output.

FAQ 2012-06-08

How can I transfer a "state" from one PSG to another?
Using ftp, the transferred states are not visible in the Recall list.

FAQ 2012-06-07

Does the E4438C ESG support MediaFLO?
Qualcomm has prepared MediaFLO IQ sample files to work with the 64-megasample arbitrary waveform generator.

FAQ 2012-06-07

How many capacitance measurement units (MFCMUs) can be installed in the B1500A?
Only one MFCMU can be installed in a B1500A mainframe.

FAQ 2012-06-07

Why is the FSK modulation index of the ESG limited to about 4 or less on the E4438C and 1 or less on the E443XB?
The interpolation in the DSP algorithms for the baseband generator limits the modulation index.

FAQ 2012-06-07

When I want to use reconstruction filters other than 250 kHz, 2.5 MHz, and 8 MHz, what should I do?
Use external filters instead of those preset filters to prevent the unwanted image spurious.

FAQ 2012-06-07

I just received my signal generator which had the signal studio pre-installed in the instrument by the factory. I also received a binder containin...
Since the license(s) is pre-installed, the certificate entitlement(s) is not attached.

FAQ 2012-06-07

What should I do in order not to set the ARB Sample Clock each time I recall a stored ARB file?
Provided are the settings for Header Information of an ARB waveform file and the Procedure.

FAQ 2012-06-07

What is the difference between E4438C options 001, 002, 601 and 602?
ARB memory depth, waveform segment and availaiblity of digital I/O port vary.

FAQ 2012-06-07

When attempting to make a Modulation Accuracy (Rho) measurement in the cdmaOne personality I get the error message, "Cannot correlate to input sign...
The Modulation Accuracy (Rho) measurement in the cdmaOne personality requires that you only have the pilot carrier turned on for your base station. If other code channels are turned on, you will get this error message.

FAQ 2012-05-26

Does Option UNU, pulse modulation, exist on the X-Series signal generators?
No, Option UNW, narrow pulse, is the only pulse option.

FAQ 2012-04-30

What is the maximum size user file that can be played real-time on the N5182B MXG or N5172B EXG X-Series signal generator?
For real-time custom modulation, it is 1024 MSa for the MXG and 512 MSa for the EXG. For real-time signal studio applications, it is up to 4 GB. Refer to specific Signal Studio Application for detailed specifications.

FAQ 2012-04-30

Can we get user defined data in ARB mode?
No, it is the same random pattern as in first-generation N5181A MXG. Real-time custom modulation has user defined data.

FAQ 2012-04-30

Are the function generators all inside the MXG and EXG X-Series signal generators?
Yes, with Option 303, multifunction generator. See the data sheets for full capabilities.

FAQ 2012-04-30

Is BER available on the N5182B MXG or N5172B EXG X-Series signal generators?
No, Option UN7, Internal Bit Error Rate Analyzer, is not available at introduction.

FAQ 2012-04-30

Does Option UNY, enhanced low phase noise, require Option UNX, low phase noise,on the X-Series signal generators?
No, they are independent options with different levels of phase noise performance above 3 GHz.

FAQ 2012-04-30

Is the tuning speed the same as switching speed on the X-Series signal generators?
Yes, switching speed is the same as tuning speed.

FAQ 2012-04-30

Do the new sources de-crypt waveforms in the same way as the legacy sources? Can we just use pre-existing waveforms?
Yes. First-generation MXG N5182A Signal Studio N76xxB waveforms will play in new sources. Exception will be N7613A Signal Studio for Fixed WiMAX which has the legacy N76xxA structure.

FAQ 2012-04-30

Previous 1 2 3 4 5 6 7 8 9 10 ... Next