Here’s the page we think you wanted. See search results instead:

 

Hable con un experto

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 756

Sort:
Signal Analyzer IVI and MATLAB Instrument Drivers
Supported models: N9000A, N9010A, N9020A, N9030A, N9038A, E4406A, E4440A, E4443A, E4445A, E4446A, E4448A, N8201A, E4447A, E4401B, E4402B, E4403B, E4404B, E4405B, E4407B, E4408B, E4411B, E7401A, E7402A, E7403A, E7404A, E7405A, M9290A, N9040B, N9038A, M9420A, N9000B, N9010B, N9020B, N9030B, N9040B, M9290A, M9420A, M9421A, SPN9026A, SPN9003A, N9041B, M90XA

FAQ 2017-09-21

What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2017-08-30

30 Day Free Trial Licenses for the M8000 Series
Overview of & links to all trial licenses within the M8000 product family.

FAQ 2017-08-09

What are the Keysight equivalent model numbers for Centellax BERT products and test accessories?
Click on the question for full details of the equivalent model numbers.

FAQ 2017-07-13

How do I create a Mono FM Signal using N5182B MXG ARB?
You can configure N7611B Signal Studio Broadcast Radio to play a mono/FM signal.

FAQ 2017-06-28

How many carriers can the MXG support in Carrier Aggregation mode?
One MXG can support one instance of the Carrier Aggregation mode. One instance of the Carrier Aggregation mode supports 5 component carriers.

FAQ 2017-06-28

Can I determine if a Keysight Signal Generator needs to be operated in terms of a status value or the temperature that it was last performed?
Keysight signal generators do not have any circuitry to monitor temperature values, or even log temperatures, inside any of our signal generators.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

What is the time out limit of response time (2.4) in M8020A Interactive link training?
The LTSSM (Link Training and Status State Machine) implements the timeouts as specified in the PCIe specification. Click on the question for additional information.

FAQ 2017-06-28

Save Time with a Modern Bench Power Supply
The new low cost DC Bench Power Supply from Keysight has three independent outputs & built in data logger. See how a modern Bench Power Supply can help you.

FAQ 2017-06-20

What are the new Wave 2 features for Mobile WiMAX™ 802.16 system profiles?
Read about IO-MIMO and IO-BF (beamforming) profiles...

FAQ 2016-12-02

Firmware update error with "Cannot Open another Window"
I cannot update the firmware with the error message; "Cannot Open another Window"

FAQ 2016-08-04

How do I clear the External Reference Warning on the display?
Step by step procedure can be found here...

FAQ 2016-01-08

How do I set the reference to external, have notification of any external reference problems, and have it remain external with a Preset?
Process steps included here...

FAQ 2016-01-08

Signal Analyzer LabVIEW Instrument Drivers
Supported models: M9290A, M9420A, N9000A, N9010A, N9020A, N9030A, N9038A, N9040B

FAQ 2015-12-11

How do I upgrade my N5191A UXG X-Series Agile Signal Generator, Modified Version, 10 MHz to 40 GHz?
Find Information on Hardware Upgrades, Instrument Software, etc.

FAQ 2015-10-01

For an auto-ranging power supply, how do I determine the maximum output current for any operating voltage? | Keysight
You will always obtain rated output power of the unit along any point of the auto-ranging operating curve.

FAQ 2015-09-08

Signal Generator Firmware Update Center
Download signal generator firmware, release notes, upgrade guide and FAQs.

FAQ 2015-08-27

How do I upgrade my N5182B MXG X-Series RF Vector Signal Generator?
Find Information on hardware upgrades, instrument firmware and more.

FAQ 2015-04-22

Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

How do I upgrade my N5172B EXG X-Series RF Vector Signal Generator?
Find Information on hardware upgrades, instrument firmware and more.

FAQ 2014-10-14

How do I upgrade my N5193A UXG Agile Signal Generator?
Find Information on Hardware Upgrades, Instrument Software, etc.

FAQ 2014-10-01

Beginning with PXB firmware version 2.2.0.14, application software updates are not provided as part of the PXB firmware.
Applications will no longer be embedded in PXB firmware, read this to learn how to get the most current version of Signal Studio.

FAQ 2014-08-13

All N603x Arbitrary Waveform Generators IVI and MATLAB Instrument Drivers
Supported models: N6030A, N6031A, N6032A, N6033A

FAQ 2014-08-12

1 2 3 4 5 6 7 8 9 10 ... Next