Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

101-125 of 526

Sort:
Windows login process appears on my ENA every time after power up. Can I skip this?
Yes.

FAQ 2011-10-07

What is the difference between "sweep speed", "cycle time" and "time per data point" as related to a vector network analyzer?

FAQ 2011-10-07

On the ENA and ENA-L, is there a SCPI command to query the active channel?
Yes.

FAQ 2011-10-07

Is there an outline for configuring my HP Basic to communicate with the Keysight ENA analyzer via SCPI-LAN?

FAQ 2011-10-07

For Cable Testing should I use a TDR, a network analyzer, or both?
The cable specifications will determine the test equipment requirements...

FAQ 2011-10-07

Using the VBA program, can the ENA / ENA-L control the handler interface to control other peripherals?
Yes.

FAQ 2011-10-07

Anti-Virus FAQ for ENA

FAQ 2011-10-07

ENA & PNA Series Network Analyzer Frequently-Asked Questions (FAQs)

FAQ 2011-10-07

On the ENA and ENA-L, is there a SCPI command to query the active trace?
Yes.

FAQ 2011-10-07

On the ENA / ENA-L, what occurs if I select "order-based display" in sweep mode?
Measurement points of different segments are plotted in constant intervals.

FAQ 2011-10-07

Is it possible to control external instruments by the ENA/ENA-L?
Yes. It is possible to control external instruments by the ENA/ENA-L with built-in VBA programs.

FAQ 2011-10-07

My simulation software is failing to import Touchstone files with extensions *.s1, *.s2, etc. Is there a way to rectify this issue?

FAQ 2011-10-07

While programming the ENA I am receiving the error, "-128, Numeric data not allowed". Why?
For many analyzers the data transfer format is adjustable when outputting data...

FAQ 2011-10-07

What are the benefits of the built-in VBA?

FAQ 2011-10-07

Is it possible to change the font size of softkey menu on ENA?
Yes. The font size of softkey menu can be changed with following procedure...

FAQ 2011-10-07

How can I find accessories for a Keysight product?
For instrument-specific accessories (such as probes for an oscilloscope), first go to the product page and then see the related accessories. For general-purpose accessories (such as rf & microwave test accessories, carts, and racks), go to the ...

FAQ 2011-10-07

The ENA / ENA-L was infected with the virus. What should I do?
Remove the LAN cable and perform system recovery.

FAQ 2011-10-07

Does the touchstone file generated by the ENA / ENA-L include the electrical delay?
The touchstone files do not include electrical delay. Please use port extension.

FAQ 2011-10-07

Can I disable the front keys, keyboard, mouse and/or touch screen on the ENA / ENA-L?
Yes.

FAQ 2011-10-07

Is it possible to measure the velocity of propagation utilizing a Keysight Vector Network Analyzer (VNA)?
Keysight VNAs do not directly provide the velocity of propagation measurement. As an alternative the steps below outline a method to calculate the velocity of propagation based upon the physical length of the cable under test.

FAQ 2011-10-07

Where can I find upgrade information of ENA?
Please refer to the ENA series service and support home page.

FAQ 2011-10-07

On the ENA, how can I make CW sweep (Fixed frequency) without turning off the ENA's output signal each time a sweep finishes?
Turn off the "Init Src Ctrl" feature, then hold trigger.

FAQ 2011-10-07

Are the adapters in the 85033E 30kHz to 9GHz calibration kit phase matched?
Yes.

FAQ 2011-10-07

Is the ENA code-compatible with the 8753?
No, but the Code Conversion Assistant Editor is available to assist with code conversion.

FAQ 2011-10-07

What is the difference between Smoothing and Averaging on a Keysight network analyzer?

FAQ 2011-10-07

Previous 1 2 3 4 5 6 7 8 9 10 ... Next