Here’s the page we think you wanted. See search results instead:

 

Discutez avec un expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

retirer tout le raffinement

Par sujet

By Type of Content

Par catégorie de produit

101-125 of 163

Sort:
What is the length of the thermocouple cable for the U1186A Thermocouple (K-type) and Temperature Adapter?
The length of the K-type thermocouple bead is approximately 1m....

FAQ 2009-01-12

Does the Keysight Measurement Manager (AMM) support regional language settings other than English (US)?
Yes, the Keysight Measurement Manager (AMM) supports regional language settings other than English (US)….

FAQ 2009-01-12

Why is the battery life of the U1253A Handheld Digital Multimeter (DMM) typically shorter than the battery life of the U1251A/U1252A?
The battery life of the U1253A Handheld Digital Multimeter (DMM) is typically shorter because its display brightness is set to the highest….

FAQ 2008-10-09

What is the maximum frequency for the U1252A Digital Multimeter's square wave output?
The maximum frequency for the U1252A Digital Multimeter's square wave output is 4800Hz….

FAQ 2008-10-07

How long would the battery of the U1252A Handheld Digital Multimeter last if I perform continuous datalogging?
If you perform continuous datalogging, the fully-charged NiMH battery of the U1252A Handheld Digital Multimeter will last for 36 hours....

FAQ 2008-09-25

Can I perform measurement with the U1252A Digital Multimeter and charge the battery at the same time?
No, you cannot perform measurement with the U1252A Digital Multimeter and charge the battery at the same time…..

FAQ 2008-09-24

Can I save measurements with the U1241A or U1242A Handheld Digital Multimeter?
You can save measurements with the U1242A Handheld Digital Multimeter but not with the U1241A….

FAQ 2008-09-24

What is the maximum frequency that can be measured with the U1252A Digital Multimeter?
The U1252A Digital Multimeter has a frequency counter function that can measure frequency up to 20MHz.

FAQ 2008-09-24

What is the peak-to-peak voltage of the square wave that is generated by the U1252A Digital Multimeter?
The peak-to-peak value of the square wave that is generated by the U1252A Digital Multimeter is 2.8V.

FAQ 2008-09-24

How long can the batteries of the U1241A or U1242A Handheld Digital Multimeter last?
The batteries that are supplied with the U1241A or U1242A Handheld Digital Multimeter can last for more than 200 hours under normal use.

FAQ 2008-09-24

Can I connect the U1241A/U1242A Handheld Digital Multimeter to a PC?
No, the U1241A/U1242A Handheld Digital Multimeter cannot be connected to a PC because it does not come with any PC interface.

FAQ 2008-09-24

Can I measure temperature with the U1241A/U1242A Handheld Digital Multimeter?
Yes, you can measure temperature with the U1241A/U1242A Handheld Digital Multimeter using a thermocouple adaptor and thermocouple tip….

FAQ 2008-09-24

Can I use regular AAA batteries in the U1241A and U1242A Handheld Digital Multimeters?
Yes, you may use regular AAA batteries for the U1241A and U1242A Handheld Digital Multimeters….

FAQ 2008-09-24

Why are 4339B measurement values unstable when measuring resistance above 100 GΩ with the 16117B or 16118A test fixture?
Resistance above 100 GΩ is beyond the measurable range of the 16117B/16118A.

FAQ 2008-06-11

Can I use non-Keysight resistivity test fixtures with the 4339B?
Yes, as long as the resistivity test fixture has connectivity to the 4339B, it can be used with the 4339B. It is recommended that the 16117C test leads be used to connect a non-Keysight test fixture.

FAQ 2008-06-10

Is there any test fixture for the 4339B to measure SMD components at test voltages above 100 V dc?
The 16339A Component Test Fixture is available.

FAQ 2008-06-10

Why cannot I measure well DUTs above 100 G ohm with the 16117B?
Since the 16117B has non-shielded clips, the maximum measurable range is limited to 100 G ohm.

FAQ 2008-05-19

Why is the 16008B furnished with an acrylic plate?
The 16008B is furnished with an acrylic plate to prevent the guard electrodes from being scratched when the 16008B is not in use.

FAQ 2008-05-16

Can I replace the 16008B's conductive elastomer when it is deteriorated?
No, since the conductive elastomer cannot be removed from the main electrode assembly of the 16008B, replace whole main electrode assembly with new one.

FAQ 2008-05-16

Does the 16008B comply with a certified method of national standard?
The 16008B is compatible with ASTM D257 Standard Test Methods for DC Resistance or Conductance of Insulating Materials.

FAQ 2008-05-15

How can I order supplemental parts for component test fixtures/accessories?
You can order the necessary parts by the part numbers shown in the Accessories Selection Guide for Impedance Measurements.

FAQ 2008-04-22

What type of internal memory is installed into the 34420A NanoVolt, Micro-Ohm Meter?
Please refer to the document linked to this page for a comprehensive listing of memory installed into the Keysight 34420A.

FAQ 2008-04-09

Can I measure temperature with the Keysight 34401A?
Most temperature sensors convert temperature to a corresponding resistance (thermistors and RTDs) or low-level dc voltag (thermocouples).

FAQ 2008-04-03

What is the Temperature Measurement Range of the Keysight 34307A Thermocouples?
Use the specifications of the Omega Engineering Inc thermocouple wire with part number TT-J-24.

FAQ 2007-01-09

What types of memory are installed into the Keysight 34401A Digital Multimeter?
Please refer to the document linked to this page for a comprehensive listing of internal memory for the 34401A digital multimeter.

FAQ 2006-11-03

Previous 1 2 3 4 5 6 7 Next