Contact an Expert

Technical Support

Network Analyzers

Find by Product Model Number: Examples: 34401A, E4440A

1-25 of 91

Sort:
[Method of Implementation] DisplayPort 1.3 Cable-Connector Assembly Compliance Test

Programming Example 2015-02-27

[Method of Implementation] USB Type-C Cable-Connector Assembly Compliance Test

Programming Example 2015-02-06

[Method of Implementation] USB 3.1 Cable-Connector Assembly Compliance Test

Programming Example 2015-02-06

[VBA Sample Program] ENA Amplifier Measurement Wizard VBA

Programming Example 2014-11-05

[VBA Sample Program] ENA Mixer Measurement Wizard VBA

Programming Example 2014-11-05

[VBA Sample Program] USB Power sensor measurement wizard

Programming Example 2014-11-05

[VBA Sample Program] ENA IMD Measurement Wizard VBA
This sample program assists intermodulation distortion (IMD) measurements using the ENA and SG.

Programming Example 2014-11-05

[VBA Sample Program] Recommended VBA package for E5071C
This is the package of popular VBA programs for the E5071C.

Programming Example 2014-11-05

[Method of Implementation] HDMI Cable Assembly Compliance Test

Programming Example 2014-10-20

[Method of Implementation] MIPI D-PHY TxRx Interface S-parameter and Impedance Test

Programming Example 2014-10-10

[Method of Implementation] BroadR-Reach Link Segment Compliance Test

Programming Example 2014-08-28

[Method of Implementation] USB 2.0 Cable-Connector Assembly Compliance Test

Programming Example 2014-06-26

[E5063A Sample Program] Save Trace Data Macro
This macro enables the ENA user to save the multiple channel/trace data with various formats.

Programming Example 2014-05-19

[Method of Implementation] SATA RXTX Impedance Compliance Test

Programming Example 2014-04-28

[Method of Implementation] SATA SI Compliance Test

Programming Example 2014-04-28

[Method of Implementation] Ethernet Tx/Rx Return Loss Test

Programming Example 2014-04-27

[Method of Implementation] Ethernet Cable Test

Programming Example 2014-04-22

[Method of Implementation] MIPI M-PHY TxRx Interface S-parameter and Impedance Test

Programming Example 2014-04-08

HDMI Source/Sink Impedance Test

Programming Example 2014-03-31

E5063A Sample Programs in Help
This is sample program files which are shown in the E5063A Help. See the E5063A Help for more detail.

Programming Example 2014-02-01

ENA Sample Programs in Help
This file provides the sample programs using Excel VBA with VISA-COM/VISA. This shows examples of Setup, Calibration, Ecal, Limit Test, File Transfer, Data Transfer (Read/Write) and Error Detection using SRQ. The ENA help explains more details.

Programming Example 2013-06-04

ZIP ZIP 591 KB
[Method of Implementation] DisplayPort 1.2b Cable-Connector Assembly Compliance Test

Programming Example 2013-04-18

[VBA Sample Program] ENA Data Transfer Program
This Microsoft Excel sample VBA program enables the ENA user to transfer the data to an external PC.

Programming Example 2013-04-01

[Method of Implementation] PCI Express 3.0 PCB Differential Trace Impedance Test

Programming Example 2013-03-25

[Method of Implementation] MHL Cable-Connector Assembly Compliance Test

Programming Example 2013-03-14

1 2 3 4 Next