Contact an Expert

Technical Support

Electronic Measurement

Find by Product Model Number: Examples: 34401A, E4440A

1-25 of 64

Sort:
Signal Analyzer IVI and MATLAB Instrument Drivers
Supported models: N9000A, N9010A, N9020A, N9030A, N9038A, E4406A, E4440A, E4443A, E4445A, E4446A, E4448A, N8201A, E4447A, E4401B, E4402B, E4403B, E4404B, E4405B, E4407B, E4408B, E4411B, E7401A, E7402A, E7403A, E7404A, E7405A, M9290A, N9040B, N9038A

FAQ 2015-05-27

Signal & Spectrum Analyzer Benchtop/Handheld Firmware Update Center
To access the most recent version of firmware or software for signal and spectrum analyzer - benchtop and handheld models.

FAQ 2015-04-08

Where can I find manuals for discontinued and obsolete Hewlett-Packard, Agilent and Keysight test equipment?
Most Keysight products have PDF manuals that can be found on product pages. Other vendors also supply old manuals.

FAQ 2014-08-01

How can I get correct Log Frequency Scale Trace Data Using IntuiLink or BenchVue with my ESA Series Spectrum Analyzer?
Save the trace as a .csv file

FAQ 2014-03-13

What is included with Option UK6?
Beginning December 19, 2013, the list below describes what will be included with Option UK6:

FAQ 2014-02-27

What Printers can be used for my Network and Spectrum Analyzer products?
Printer Compatibility Information for your specific model of Network and/or Spectrum Analyzer can be found here.

FAQ 2014-01-31

What is the RF Test Blog?
RF engineers know that making good measurements is a challenge. The RF Test Blog was created as a resource for RF engineers to find ways to make better RF measurements.

FAQ 2013-12-17

What calibrations are available on X-Series, PSA, ESA analyzers and X-Series, ESG-C, PSG Signal Generators at time of initial sale from the factory?
Details regarding time of sale calibrations can be found here...

FAQ 2013-10-15

How do I use the Service Request method (SRQ) to determine if the X-Series, ESA and PSA Signal Analyzers measurement is complete or has an error me...
Click here for information on the Service Request query to determine when a measurement is complete.

FAQ 2013-06-25

How do I remotely program my spectrum or vector signal analyzer?
Instructions, examples, and references for remotely programming your spectrum analyzer

FAQ 2013-05-16

What is a Spectrum Analyzer?
"What is a spectrum analyzer?” You asked and we answered.

FAQ 2013-03-28

How do I upgrade my ESA-E Series Spectrum Analyzer?
Find information on Hardware Options, Measurement Personalities, Connectivity Methods, Firmware Upgrades, etc....

FAQ 2013-03-28

What Configuration issues are there with option AYQ, Quasi Peak Detector in the ESA-E Series of Spectrum Analyzers?
View the compatibility issues here....

FAQ 2012-12-05

What is the Noise Figure accuracy specification for measuring “my device”?
Keysight supplies a web-based noise figure measurement uncertainty calculator. More details about how to use this tool can be found here...

FAQ 2012-07-31

For my Spectrum Analyzer, where can I find a conversion guide between IVI-COM and SCPI?
The linked spreadsheet provides a mapping between IVI-COM and SCPI

FAQ 2012-05-26

What type of cabinets can the ESA Rackmount Kit (Option 1CP) be installed into?
The ESA Rackmount Kit (Option 1CP) was designed to mount into an System II Rack.

FAQ 2012-03-16

How do I transfer the screen image on my PSA, ESA, or EMC analyzer to a PC using Keysight VEE?
See content for complete details and an example program...

FAQ 2012-03-16

How do I erase/clear the user data in an ESA or EMC series spectrum analyzer for security reasons?
Follow this link for further information....

FAQ 2012-03-16

What is the fastest pulse risetime that I can measure with my spectrum analyzer in zero span?
The measurement risetime may not be faster that the best risetime of the spectrum analyzer

FAQ 2012-03-02

Why do spurious signals appear in my spectrum analyzer span when I apply a clean signal to the RF input?
Overdriving the input mixer of the analyzer may cause the spurs.

FAQ 2012-02-26

Can I make Noise Figure Measurements below 10 MHz with the ESA-E Series Spectrum Analyzer?
Yes, you can make useful noise figure measurements with the ESA-E Series Spectrum Analyzer down to 200 kHZ, however, no instrument specifications are provided.

FAQ 2012-02-25

Why didn't my new ESA-E arrive with all the personalities that I ordered installed?
If more than two or three personalities have been ordered, memory limitations may not permit all of them to be installed at the same time...

FAQ 2012-02-25

How do I configure my ESA-E Series Spectrum Analyzer for Noise Figure measurements?
Configure your ESA-E Series Spectrum Analyzer with Option 219, Noise Figure Measurement Personality and Hardware and Option 1DS, Internal Preamplifier at time of purchase.

FAQ 2012-02-25

What are the Noise Figure specifications above 3 GHz for the ESA Series Spectrum Analyzer?
The specifications for instrument noise figure uncertainty is nominally the same as from 10 MHz to 26.5 GHz, especially for high gain devices under test.

FAQ 2012-02-25

Can I use the internal microwave preamp, Option H26, with the ESA-E Series Spectrum Analyzer Noise Figure solution?
We do not recommend using the Option H26 internal microwave preamp at this time. Option H26 has not been tested for compatability with the Noise Figure Measurement Personality.

FAQ 2012-02-25

1 2 3 Next