与专家交流

技术支持

电子测量

按产品型号查找: 示例:34401A,E4440A

1-25 / 854

排序:
如何升级我的 PSA系列频谱分析仪
Find information on Hardware Options, Measurement Personalities, Connectivity Methods, Firmware Upgrades, etc…

FAQ 2015-04-06

我能用手持式频谱分析仪测量 VSWR、回波损耗和 DTF 吗?
可以,配有选件 CA7 和 TG7 的 HSA N9342C 手持式频谱分析仪支持测量 VSWR。

FAQ 2015-03-26

Can I use a Windows 7 PC to upgrade my PSA Series Spectrum Analyzer?
In Windows 7 you can use the Windows XP mode to run the PSA Firmware Update Program.

FAQ 2015-03-12

Signal Analyzer IVI and MATLAB Instrument Drivers
Supported models: N9000A, N9010A, N9020A, N9030A, N9038A, E4406A, E4440A, E4443A, E4445A, E4446A, E4448A, N8201A, E4447A, E4401B, E4402B, E4403B, E4404B, E4405B, E4407B, E4408B, E4411B, E7401A, E7402A, E7403A, E7404A, E7405A, M9290A, N9040B

FAQ 2015-02-06

X 系列测量应用软件免费试用许可证
30 day trial license available for the X-Series measurement applications.

FAQ 2014-12-19

89600 VSA software and X-Series signal analyzer software compatibility matrix
Supported versions listed here

FAQ 2014-12-16

What hardware platforms are no longer supported by the 89600 VSA software?
A list of discontinued hardware by version number

FAQ 2014-12-16

What hardware platforms are supported by the 89600 VSA and 89600 WLA Software?
The measurement hardware front ends include supported by the current version of software are listed here.

FAQ 2014-12-16

信号和频谱分析仪固化软件/软件升级中心
最近更新产品的一站式购物...

FAQ 2014-12-08

How do I upgrade my M9290A CXA-m PXIe Signal Analyzer?
Find Information on Hardware Options, Measurement Applications, etc....

FAQ 2014-11-17

How do I find my Host ID when I run software on a PC?
For the PSA model, when requesting an N9051A trial

FAQ 2014-10-31

我能否升级 M9290A CXA-m PXIe 信号分析仪的频率范围?
不能,M9290A 不支持频率范围升级。

FAQ 2014-10-27

M9290A CXA-m PXIe 信号分析仪是否支持扫描模式以进行频谱分析?
是的,M9290A 同时支持扫描模式和 FFT 模式,以进行信号的频谱分析。

FAQ 2014-10-27

能否将 M9290A CXA-m PXIe 信号分析仪拆分为独立的模块化组件?
不能,这是因为 M9290A 采用单个模块,无法拆分为独立的组件。

FAQ 2014-10-27

M9290A CXA-m PXIe 信号分析仪是否与其他的台式 X 系列信号分析仪代码兼容?
是的,M9290A 能够与台式 X 系列信号分析仪代码兼容。

FAQ 2014-10-27

M9290A CXA-m PXIe 信号分析仪是否配置跟踪发生器?
M9020A 目前不提供跟踪发生器功能。

FAQ 2014-10-27

M9290A CXA-m PXIe 信号分析仪有几个插槽?
M9290A 是一款 4 插槽 PXIe 模块。

FAQ 2014-10-27

I ordered the N9051A, but it is no longer installed on the signal analyzer. The N9051B is installed, but my N9051A licenses don’t work. What shou
The N9051B is the recommended replacement for N9051A. The N9051A license can be upgraded by adding a low-cost N9051B-A2B license.

FAQ 2014-10-21

If I have N9051A Pulse Measurement Software, how do I upgrade to N9051B?
Order N9051B Option A2B to receive a user-installed software license, which causes any existing N9051A licenses to be recognized as N9051B licenses. The N9051B-2FP license is required, while all others are optional and independent of each other.

FAQ 2014-10-21

What are key differences between N9051A and N9051B Pulse Software?
See the table in this FAQ for details.

FAQ 2014-10-21

How is the N9051B Pulse Measurement Software delivered, installed and licensed?
Important: N9051B runs only on the CPU inside an X-Series signal analyzer, which must be Windows 7 and 64-bit. See the FAQ for further details.

FAQ 2014-10-21

When I redeem a license certificate for a final license for the N9051B Pulse software, I need my HostID. Where do I find this?
On the X-Series signal analyzer, press System > Show > System. In the table, around the 10th row, you will find “HostID”, this is composed of the model and serial number.

FAQ 2014-10-21

Are trial licenses available for the N9051B Pulse Measurement Software?
Yes, a trial license is available to let you explore the N9051B free of charge for 30 days. The trial has all features enabled.

FAQ 2014-10-21

How do I upgrade to “Deep Capture” for the N9051B Pulse Measurement Software?
Deep Capture is a software license upgrade performed by the end-user. This is only available for the N9051B version, order N9051B Option 5FP.

FAQ 2014-10-21

What does the “Deep Capture” option give me in the N9051B Pulse Measurement Software?
The N9051B software operates in “batch” mode: digitizing the RF signal into IQ samples, captured a time-segment into memory, and then analyze it. Review the entire FAQ for full details.

FAQ 2014-10-21

1 2 3 4 5 6 7 8 9 10 ... 下一页