聯絡是德專家

技術支援

電子量測

依產品型號搜尋: 例如: 34401A, E4440A

76-100 / 853

排序:
為何分段式記憶體擷取模式這麼有用?哪種 Keysight Infiniium 示波器才可支援此模式?
分段式記憶體模式可提供更有效的擷取記憶體使用率,能儲存由長時段所隔離的感興趣事件之波形。所有目前出貨的 Keysight Infiniium 和許多舊型裝置皆可支援分段式記憶體。

FAQ 2013-09-18

Can I use the MXA or PXA real-time Frequency Mask Trigger (FMT) to provide a trigger output that can be used to trigger another device?
Yes, you can configure the MXA or PXA to provide a trigger output when using FMT.

FAQ 2013-08-07

Can I get the real-time I/Q samples out via LAN on my MXA or PXA signal analyzer with option RT1 or RT2?
No, however you can save the real-time trace (Frequency & Amplitude) data into a .csv file from the spectrogram trace (10,000) traces.

FAQ 2013-08-07

How can I tell if my instrument is licensed for options B1X, B1Y, and MPB?
You can check to see what options are installed in your instrument by pressing the [System] hard key, then the {Show} soft key, then the {System} soft key.

FAQ 2013-08-07

What are the specifications for real-time analysis bandwidths on N9030A PXA signal analyzers with option RT1 or RT2?
See details...

FAQ 2013-08-07

What upgrade kit option provides real-time functionality for my N9030A PXA signal analyzer?
If you already have option B1X, B1Y, and MPB in your instrument, order N9030AK-RT2 or N9030AK-RT1...

FAQ 2013-08-07

I am looking at a 160 MHz OFDM signal at 5 GHz on my MXA or PXA signal analyzer. Why can’t I see the whole signal?
The instrument preselector is limiting the bandwidth of the MXA or PXA input.

FAQ 2013-08-07

Why is option B85 or B1X required for real-time spectrum analyzer on an MXA or PXA signal analyzer?
All the real-time processing takes place in the option B85 or B1X hardware.

FAQ 2013-08-07

What features will my MXA or PXA signal analyzer have after I install option RT2 or RT1 real-time spectrum analyzer?
Frequency mask trigger, power vs. time measurements, real-time spectrogram, trace zoom peak, average, sample, and negative peak detectors...

FAQ 2013-08-07

Why is option MPB required at frequencies above 3.6 GHz for real-time spectrum analysis in an X-Series signal analyzer?
At frequencies above 3.6 GHz, a YIG Preselector (a tracking band-pass filter) is used to reject out-of-band signals. This filter’s bandwidth is significantly less than 85 or 160 MHz so it must be bypassed if the user wishes to utilize the full 85 or 160 MHz of real-time bandwidth in their PXA.

FAQ 2013-08-07

My FieldFox will not boot up. Is there a way to reset it?
FAQ for FieldFox failure to boot

FAQ 2013-07-29

How do I figure out the analysis bandwidth upgrade option(s) I should order to achieve the analysis bandwidth I need to have in my X-Series analyzer?
Use the X-Series analysis bandwidth wizard to determine the upgrade option(s) that are needed for the analysis bandwidth you need.

FAQ 2013-07-19

How do I upgrade my N1996A CSA Spectrum Analyzer?
Find information on Hardware Options, Measurement Personalities, Firmware Updates, etc...

FAQ 2013-07-16

How do I use the Service Request method (SRQ) to determine if the X-Series, ESA and PSA Signal Analyzers measurement is complete or has an error me...
Click here for information on the Service Request query to determine when a measurement is complete.

FAQ 2013-06-25

What are the deep signal capture capabilities for the N9030A Signal Analyzer?
Details found here...

FAQ 2013-06-25

Can the N9000A CXA signal analyzer install both additional 75 ohm RF input and the built-in tracking generator?
No, the tracking generator is not compatible with 75 ohm input connector.

FAQ 2013-06-25

How do I upgrade my N9030A PXA Signal Analyzer?
Find Information on Hardware Upgrades, Instrument Software and Measurement Applications, etc....

FAQ 2013-06-04

我在哪裡可以找到過時的HP測試儀器的使用手冊?
有一些公司可能還會提供這些使用手冊…

FAQ 2013-05-29

How do I remotely program my spectrum or vector signal analyzer?
Instructions, examples, and references for remotely programming your spectrum analyzer

FAQ 2013-05-16

How to add N9051A, Pulse Measurement Software, to the mode key selections.
X-Series signal analyzer with Windows 7 and Software versoin A.12.xx installed may not list N9051A as selection avilable under the Mode key.

FAQ 2013-05-16

How do I upgrade my N9320B Spectrum Analyzer?
Find Information on Hardware Upgrades, Instrument Software, etc...

FAQ 2013-05-09

N6171A MATLAB Software - Keysight Compatible Instruments
N6171A MATLAB software can be purchased along with a new Keysight instrument or purchased as software to add to an existing instrument.

FAQ 2013-04-29

Will Keysight continue to sell existing functionality/upgrades for my instruments?
We have no plans to end upgrade offerings for existing Windows XP functionality

FAQ 2013-04-25

Is the firmware revision A.12.xx installer the same for both Windows XP and Windows 7?
Firmware revision A.12.xx installer for Windows XP is a separate file than the firmware revision A.12.xx installer for Windows 7. Both are available on the Download button for the instrument software.

FAQ 2013-04-25

How do I know what operating system my instrument will have?
Your quote and order will indicate the operating system.

FAQ 2013-04-25

上一個 1 2 3 4 5 6 7 8 9 10 ... 下一頁