Contact an Expert

Technical Support

Electronic Measurement

Find by Product Model Number: Examples: 34401A, E4440A

Refine the List

remove all refinements

By Topic

By Type of Content

By Product Category

1-25 of 415

Sort:
Infiniium Oscilloscope Software
Infiniium oscilloscope software.

FAQ 2015-02-26

Is there a 3D model of the InfiniiVision 2000/3000/3000T X-Series oscilloscopes?
Yes, see the IGES, SAP, and Step format file downloads.

FAQ 2015-02-18

Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

Does the 86100D DCA-X Support Windows 7?
Yes. Existing mainframes my be upgraded by ordering 86100DU-WN7 from your local contact center. All the new 86100Ds ship with Windows 7 installed.

FAQ 2014-09-25

Where Can I Find Free Trials?
Find the available free trials by product family.

FAQ 2014-08-14

Where can I find manuals for discontinued and obsolete Hewlett-Packard, Agilent and Keysight test equipment?
Most Keysight products have PDF manuals that can be found on product pages. Other vendors also supply old manuals.

FAQ 2014-08-01

Is there a 3D model of the InfiniiVision 6000 X-Series oscilloscopes?
Yes, see the IGES, SAP, and Step format file downloads.

FAQ 2014-04-29

Will the 86100C DCA-J be updated to support Windows 7?
No, the 86100C platform and software will not support Windows 7.

FAQ 2014-04-18

Why are USB modular instruments (U2700 Series) and USB DAQ modules (U2300, U2500, U2600 Series) not detectable by the E5810B?
Establish the connection between the USB modular Instrument and the PC directly, and then disconnect the device from the PC (while it’s still powered-on), and connect to E5810B.

FAQ 2014-04-17

Does PC link 2.51 support Windows 7, 64 bits?
No

FAQ 2014-04-17

Can I operate 86107A over continuous frequency bands?
The 86107A can operate over the following continuous frequency range if the 86100A/B/C mainframe has firmware revision A04.10 or above.

FAQ 2013-12-12

What are the remote control commands to switch between FlexDCA and the legacy user interface?
The :SYSTem:FCONfig command can be used to switch between the possible user interfaces.

FAQ 2013-12-12

Can I upgrade my 86100A, 86100B or 86100C mainframe to obtain an 86100D?
The 86100D has major hardware differences that make an upgrade uneconomical. Keysight regularly offers trade-in and other incentive programs for DCA mainframes. Contact your local representative for details about the current trade-in program available for your unit.

FAQ 2013-11-27

Why does handheld scope’s date/time display disappears or shows hexa characters?
This condition indicates that the internal memory battery level is low.

FAQ 2013-11-22

Can I switch off the U1602A/U1604A Handheld Oscilloscope's audible key sound?
Yes, you have the option to switch on or off the audible key sound of the U1602A/U1604A Handheld Oscilloscope….

FAQ 2013-11-17

Can I export the data saved in the U1602A/U1604A Handheld Oscilloscope's internal memory to my PC?
No, you cannot export the data saved in the U1602A/U1604A Handheld Oscilloscope's internal memory to your PC....

FAQ 2013-11-17

Can I upgrade to option 001(Host USB interface) for the U1600A Series Handheld Oscilloscopes after purchase?
No, you cannot upgrade to option 001 for the U1600A Series Handheld Oscilloscopes after purchase….

FAQ 2013-11-17

Can I save the image of Meter or Logger mode to the internal memory of my U1602A/U1604A Handheld Oscilloscope?
No, you cannot save your Meter or Logger data to the internal memory nor the USB Flash Memory (for option-001) of your U1602A/U1604A....

FAQ 2013-11-17

Are the input channels on the U1602A and U1604A Handheld Oscilloscopes isolated?
No, the scope channels 1 and 2 on the U1602A and U1604A Handheld Oscilloscopes are not isolated. They share the same ground.

FAQ 2013-11-17

What parts and accessories are available for my 10400A-series probe?

FAQ 2013-11-15

Why is the segmented memory acquisition mode useful and which Infiniium oscilloscopes support it?
Segmented memory mode offers more efficient acquisition memory usage for storing waveforms with events of interest that are separated by long periods of time. All currently shipping Infiniiums and many older units support segmented memory.

FAQ 2013-09-18

Can I use the U2701A/U2702A IVI driver on Windows 8?
Yes, but you need to run a special command after installation...

FAQ 2013-07-20

Infiniium Oscilloscopes: Waveform Labeling
Is it possible to label waveforms?

FAQ 2013-05-31

Infiniium Oscilloscopes: Mouse and Trackball Usage
What type of mouse can be used with the Infiniium oscilloscope? Can a trackball device be used?

FAQ 2013-05-31

Infiniium Oscillscopes: Trigger Setup for Violation Mode
When triggering on a setup time violation, what would cause a trigger to occur on a setup time value that is larger than specified?

FAQ 2013-05-31

1 2 3 4 5 6 7 8 9 10 ... Next