전문가 상담

기술 지원

전자 측정

모델번호로 검색: 예제: 34401A, E4440A

상세 분류

상세분류 제거

주제별

분야별 검색결과

제품 카테고리별

26-50 / 414

정렬방식:
Infiniium Oscilloscopes: Waveform Labeling
Is it possible to label waveforms?

FAQ 2013-05-31

Infiniium Oscillscopes: Trigger Setup for Violation Mode
When triggering on a setup time violation, what would cause a trigger to occur on a setup time value that is larger than specified?

FAQ 2013-05-31

Infiniium Oscilloscopes: Mouse and Trackball Usage
What type of mouse can be used with the Infiniium oscilloscope? Can a trackball device be used?

FAQ 2013-05-31

How can I bundle N1045A remote heads together in a tight space?
For simple differential setups, two heads can simply be clipped together using the supplied clip. To mount more heads see the full body of this FAQ for mounting dimensions and thermal considerations.

FAQ 2013-04-24

What are the rack mount kit part numbers for the 86100 DCA?
Rack mount kits for 86100 DCA are available to purchase as stand-alone parts.

FAQ 2012-12-20

Can I remotely query the 86100D DCA-X to determine which user interface is running?
Yes. Issue the query :SYSTem:FCONfig? If the response is "Legacy" then the legacy UI is in use. If the response is "Compatible" or "Standard" then the FlexDCA interface is in use.

FAQ 2012-12-12

How do I order the Infiniium oscilloscope hard drive replacement kit?
For Infiniium oscilloscopes with the Windows® XP operating system, the part number depends on the oscilloscope model number ...

FAQ 2012-11-13

What is the difference between the Auto and Normal trigger modes on InfiniiVision oscilloscopes?
In auto trigger mode, the trigger will be forced if the specified conditions are not met. In normal trigger mode, the trigger will never be forced and a trigger will only occur if the specified conditions are met.

FAQ 2012-10-17

All IntuiLink Tools for Keysight Oscilloscopes
Supported Models: Infiniium Series, 1000 Series, 2000 X-Series, 3000 X-Series, 5000 Series, 6000 Series, 7000 Series, and 54600 Series Oscilloscopes

FAQ 2012-09-26

What is the typical power consumption of the 86100C and 86100D Digital Communications Analyzer?
Typical measurements of 86100C and 86100D power consumption

FAQ 2012-09-25

How can I de-embed a test fixture using the 86100C/D Digital Communications Analyzer?
N1010A software with InfiniiSIM-DCA option provides the capability to de-embed and embed fixtures, cables, probes, and other circuit elements.

FAQ 2012-09-25

Is there a 3D model of the InfiniiVision 4000 X-Series oscilloscopes?
Yes, see the IGES, SAP, and Step format file downloads.

FAQ 2012-09-12

How do I get >8 bit vertical resolution on my Keysight real-time oscilloscope?
Most Keysight oscilloscopes give 8-bit vertical resolution at normal acquisition mode.

FAQ 2012-08-31

What application software is available for 16900, 1680x, 1682x and 1680/1690 Series logic analyzers?
See the table for quickly seeing the application support available for Keysight U4000, 16900, 16800 and 1680/90 logic and protocol analyzers.

FAQ 2012-08-14

인피니비젼 5000/6000/7000 시리즈의 사용자 캘리브레이션을 위해 필요한 악세사리와 절차를 알고 싶습니다.
필요한 악세사리는 아래와 같습니다.

FAQ 2012-07-31

세그멘티드 메모리 옵션, N5454A를 구매했습니다. 메뉴에서 찾을 수가 없습니다. 어떻게 해야 하나요?
세그멘티드 메모리는 firmware 5.10 이상에서 동작합니다.

FAQ 2012-07-31

What can I do if the Keysight USB Modular Instrument driver installations failed to complete installation on a Windows 7 environment?
If you encountered the event mentioned above, follow the installation best practices steps below.

FAQ 2012-07-25

What can I do if I fail to establish hardware connection after successfully installing Keysight USB modular instrument driver on a Win7 environment?
If you encountered the event mentioned above, follow the installation best practices steps below.

FAQ 2012-07-25

Which probe positioners are available to hold the N1021B?
The adapter provided with the N1021B is generic enough to work with robot arms or common industry positioners ...

FAQ 2012-07-06

54800 시리즈 Infiniium 오실로스코프의 암호해제 또는 데이터삭제는 어떻게 할 수 있습니까?

FAQ 2012-05-09

고 대역폭 54850 시리즈 Infiniium 스코프에서 BNC 커넥터를 사용하는 이유
고 대역폭 54850 시리즈 Infiniium 스코프에서 BNC 커넥터를 사용하는 이유

FAQ 2012-05-08

ENA는 액티브 프로브에 대해 프로브 전원 연결을 제공합니까?

FAQ 2012-04-17

How do I establish a peer-to-peer connection between my PC and an InfiniiVision 5000/6000/7000 Series oscilloscope?
There are two methods ...

FAQ 2012-03-27

MSO6000, MSO7000 시리즈의 디지털 채널이 동작하지 않습니다.
디지털 채널 오류에 몇 가지 알려진 원인이 있습니다.

FAQ 2011-11-01

Y1, Y2 커서를 자동으로 X1, X2 위치에 따라 움직이게 설정할 수 있나요ㅏ?
가능합니다.

FAQ 2011-11-01

이전 1 2 3 4 5 6 7 8 9 10 ... 다음