전문가 상담

기술 지원

전자 측정

모델번호로 검색: 예제: 34401A, E4440A

상세 분류

상세분류 제거

주제별

분야별 검색결과

제품 카테고리별

151-175 / 414

정렬방식:
키사이트 인피니엄 스코프는 HDTV trigger mode를 지원합니까?
.

FAQ 2008-04-17

Where are the NI instrument drivers for 6000 Series scopes?
National Instruments has developed two software drivers for our 6000 Series scopes (A and L Series). They both are downloadable from NI web sites below.

FAQ 2008-03-27

Do I need a J8130A in order to use the MSO6000 with option FRS?
Yes, the J8130A (VPT1000) is required in addition to order the option FRS on the MSO6000 in order to do FlexRay Measurements on the MSO6000. Without the VPT1000, there is no FlexRay functionality on the MSO6000. Keysight does provide an additional ...

FAQ 2008-02-19

If the J8130A must be purchased separately what are the required options to use it with the scope?
No extra options are required on the J8130A to run with the MSO6000. The plain J8130A product is sufficient. However, the J8130A has a few potential options that could be ordered if needed: -The option 001 allows the VPT1000 to be used as a Flex...

FAQ 2008-02-12

Does the option FRS or the N5432A for the MSO6000 include the J8130A VPT1000 or must it be purchased separately?
The J8130 (VPT1000) must be ordered separately.

FAQ 2008-01-31

인피니엄스코프(5483x, 5485x, MSO8000, 및 DSO80000 시리즈)의 CPU 보드에 사용되는 리튬배터리 CR2032 3V 의 파트번호는 무엇입니까?
.

FAQ 2008-01-08

How would I download the scope setup/trace files or screen images off to an USB drive on the 6000L series scope?
With an external PC connected to the scope via LAN interface, you can use the web browser control on the LAN and download scope data to an USB drive plugged into the scope’s front panel USB interface.

FAQ 2007-11-02

Is the battery option retrofitable to previously purchased oscilloscope?
No. The battery option for the 6000 Series is a factory-installed option which is not retrofitable to previously purchased oscilloscopes.

FAQ 2007-11-02

What are the applications for battery-powered oscilloscope?
Battery-powered oscilloscopes are targeted for engineers and technicians in automotive testing, quality testing, industrial applications, power control circuit testing, In-vehicle, marine, and aerospace applications.

FAQ 2007-11-02

How long does the charge last?
~2 hrs initially

FAQ 2007-11-02

Is there a way to access online help for 6000L?
Yes. Press right mouse click on the specific softkey image.

FAQ 2007-11-02

How many months/years is it expected to last?
Occasional battery users can use the battery ~10 years before replacement, while heavy users may need to replace within 2-3 years.

FAQ 2007-11-02

Can I use the oscilloscope while the battery is being charged?
Yes, the battery automatically recharges when the scope is connected to AC line power.

FAQ 2007-11-02

What is the technology used in the battery powered 6000 Series?
Rechargeable lithium ion battery

FAQ 2007-11-02

How do I maximize the battery life?
Avoid charging and discharging the battery repeatedly.

FAQ 2007-11-02

How much will it add to the weight of the scope?
12.35 Lbs without power adapter and 14 Lbs with power adapter

FAQ 2007-11-02

What comes with the 6000L Series oscilloscope?
The 6000L Series oscilloscope comes with the following items

FAQ 2007-11-02

Does 6000L Series oscilloscope require extra rack mount kit?
No. There are front-panel brackets and rack rails included as part of the product to attach it to the rack securely.

FAQ 2007-11-02

Is Keysight’s battery-powered scope safe to use?
Keysight’s battery powered 6000 Series scopes were designed and manufactured to meet strict safety measures and comply with international safety standards.

FAQ 2007-11-02

Is it necessary to connect the ground post on the rear panel to earth ground?
If the circuit under test has voltages that exceed 30Vrms (or >42Vpk), the scope chassis needs to be connected to earth ground.

FAQ 2007-11-02

What is unique about Keysight’s battery powered oscilloscope?
Keysight’s 6000 Series with the battery option is the only battery powered mixed signal oscilloscope (MSO), highest performance 100MHz -500MHz battery powered oscilloscopes and only 1GHz battery powered oscilloscope available in the market.

FAQ 2007-11-02

How many charges will the battery last through?
The battery should deliver >80% of initial capacity after 300+ charge/discharge cycles.

FAQ 2007-11-02

If the battery dies and will not recharge, is it return to factory or service center for repair?
The oscilloscope battery is not user replaceable. You must return the oscilloscope to Keysight for battery replacement.

FAQ 2007-11-02

What digital probe cables and accessories are available for Keysight mixed-signal oscilloscopes (MSOs)?
The digital probe kit for all Keysight 6000-series and 54620/40-series MSOs is P/N 54620-61801. The digital probe kit for all 8000-series and 54830-series MSOs is P/N 54826-68701.

FAQ 2007-08-10

로직 분석기에서 이용할 수 있는 프로브에는 어떤 것들이 있습니까?
키사이트는 다음과 같이 4가지 로직 분석기 프로브를 공급하고 있습니다.

FAQ 2007-06-26

이전 1 2 3 4 5 6 7 8 9 10 ... 다음