Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

101-125 of 204

Sort:
ESA Series L1500A: IF Relay Lifetime

FAQ 2008-10-08

ESA Series L1500A: Spectrum Analyzer Model and Product Numbers

FAQ 2008-10-08

ESA-L1500A: Spectrum Analyzer 12 Vdc Operation

FAQ 2008-10-08

How long would the battery of the U1252A Handheld Digital Multimeter last if I perform continuous datalogging?
If you perform continuous datalogging, the fully-charged NiMH battery of the U1252A Handheld Digital Multimeter will last for 36 hours....

FAQ 2008-09-25

Can I use D-type linearity to calibrate the V8486A Power Sensor?
Yes, you can use D-type linearity to calibrate the V8486A Power Sensor....

FAQ 2008-09-25

Why is the 50 MHz reference calibration not required for the U2000 Series USB Power Sensors?
The U2000 USB Power Sensors do not require a 50MHz reference calibration because their cable lengths and sensor/meter pairings are fixed….

FAQ 2008-09-25

Why does "National Instruments" appear as the manufacturer of the U2000 Series USB Power Sensors in the Device Properties?
"National Instruments" will appear as the manufacturer of the U2000 Series USB Power Sensors if the Keysight IO Libraries is not installed. …

FAQ 2008-09-25

Can I use regular AAA batteries in the U1241A and U1242A Handheld Digital Multimeters?
Yes, you may use regular AAA batteries for the U1241A and U1242A Handheld Digital Multimeters….

FAQ 2008-09-24

How long can the batteries of the U1241A or U1242A Handheld Digital Multimeter last?
The batteries that are supplied with the U1241A or U1242A Handheld Digital Multimeter can last for more than 200 hours under normal use.

FAQ 2008-09-24

Can the 4339B be used for HIPOT (High-potential) tests?
No, the requirements of HIPOT tests are different from the insulation resistance tests and measurements.

FAQ 2008-09-11

Does the 4338B carry CE mark?
Yes, the 4338B carries the CE mark.

FAQ 2008-06-11

Is it possible to parallel more than 2 units of the 42841A to expand bias current output range?
No. Instrument does not have firmware to control more than 2 units of the 42841A. In addition, connecting more than 2 units of the 42841A may cause an "OVLD" status due to possible imbalance of DC bias source and sink currents.

FAQ 2008-05-26

What are the criteria to be applied when choosing the instrument for C-V measurements from the 4294A and E4980A?
It depends on the size and the thickness of the gate oxide film of the device.

FAQ 2008-05-26

What are the size, cable length and weight of the 42941A probe?
The 42941A has 15 cm long probe body, 1.5 m long cable and approximately 2.4 kg in weight.

FAQ 2008-05-20

Why is the 16008B furnished with an acrylic plate?
The 16008B is furnished with an acrylic plate to prevent the guard electrodes from being scratched when the 16008B is not in use.

FAQ 2008-05-16

How do I change Daylight Saving Time Settings on the ENA?
Keysight confirmed that Daylight Saving Time Setting can be changed with following procedure...

FAQ 2007-10-05

What hard copy manuals are included with option ABA for the ENA 6 series?

FAQ 2007-07-12

How long will the 8546A/2E instruments be supported?
Support life will end in March 2006

FAQ 2007-06-29

How do I calculate the accuracy of 4284A when the desired stimulus is RMS current rather than RMS voltage?
The Keysight 4284A data sheet provides measurement accuracy as a function of stimulus level in RMS volts.

FAQ 2007-05-09

What is the Temperature Measurement Range of the Keysight 34307A Thermocouples?
Use the specifications of the Omega Engineering Inc thermocouple wire with part number TT-J-24.

FAQ 2007-01-09

I received my 35670A, but I found that a floppy disk to do performance test was not included in the shipment. I bought several 35670A in the past y...

FAQ 2006-10-02

HP 8753B Network Analyzer CRT Display Replacement

FAQ 2005-04-12

What Is Quasi-peak Detection?
An annoyance meter....

FAQ 2004-06-22

How many correction points can be entered into an 8590EM Series EMC Analyzer?
80 discrete points....

FAQ 2004-06-22

What is the ETS part number for the 11955A?
ETS # 93110B

FAQ 2004-06-22

Previous 1 2 3 4 5 6 7 8 9 Next