By Topic

By Industry/Technology

By Type of Content

By Product Category

51-75 of 3453

Sort:
How do I install the cables and adapter for the M9485A?
The installation procedure is shown in the M9485A Start Up Guide.

FAQ 2017-05-25

What is the service (repair/calibration) support strategy?
The service (repair/calibration) support strategy of the M9485A is the module level. Only defective module can be returned, if it needs repair.

FAQ 2017-05-25

Is there any system level specification for the M9485A?
No, there is no system level specification.

FAQ 2017-05-25

Signal Analyzer IVI and MATLAB Instrument Drivers
Supported models: N9000A, N9010A, N9020A, N9030A, N9038A, E4406A, E4440A, E4443A, E4445A, E4446A, E4448A, N8201A, E4447A, E4401B, E4402B, E4403B, E4404B, E4405B, E4407B, E4408B, E4411B, E7401A, E7402A, E7403A, E7404A, E7405A, M9290A, N9040B, N9038A, M9420A, N9000B, N9010B, N9020B, N9030B, N9040B, M9290A, M9420A, M9421A, SPN9026A, SPN9003A, N9041B

FAQ 2017-05-24

How can I order custom configuration for M9485A?
You can order each module/accessory separately as you like. Please refer to below item list and startup guide for detail.

FAQ 2017-05-24

What is the part number of connector saver for the M9376A, M9378A/B?
The connector saver is an adapter of coaxial straight male-SMA female-SMA on the test port of the M9376A, M9378A/B. This adapter can be replaced easily if the connecter is broken or is worn down.

FAQ 2017-05-24

How should I stack 2 PXI chassis for M9485A 2-chassis configuration?
It is recommended to use M9485-60003 1U spacer kit which is included in cable kit for two chassis configurations.

FAQ 2017-05-24

What is the dimension and connector location of each modules of the M9485A?

FAQ 2017-05-19

Why is sensor with internal calibration capability not measuring 0dBm after performing zero & calibration process?
Power sensors with internal calibration capability( eg. N192XA, U848x, U2020XA, U2040XA) use its built in reference when performing a zero and calibration.

FAQ 2017-05-05

Is there a 3D model of the InfiniiVision 4000 X-Series oscilloscopes?
Yes, see the IGES, SAP, Step, PKG, X_T, EASM, and PDF format file downloads.

FAQ 2017-05-05

How to perform cal factor correction when using 8480 series power sensor ( with cal factor below 85% or above 100%) with old power meters (HP435B/HP43
If you are using an HP435B or HP436A, the minimum cal factor setting is 85% and the maximum is 100%.

FAQ 2017-03-30

Why is the linearity of E441x, E930x and E932x Power Sensors not tested per sensor’s dynamic range?
In actuality, there is little necessity to test linearity of the E4412A and E4413A Power Sensors below -20dBm….

FAQ 2017-03-29

Why is the accuracy of U200x Power Sensors not tested per sensor’s dynamic range?
The accuracy of those sensors is essentially a combination of linearity, instrumentation accuracy and traceability to absolute accuracy at 50MHz, 0dBm.

FAQ 2017-03-29

Is there a 3D model of the M924xA PXIe modular oscilloscopes?
Yes, see the IGES, SAP, Step, EASM, PKG, and PDF format file downloads.

FAQ 2017-03-23

How to maintain 16195B?
The 16195B which consists of Open, Short, 50 Ω Load and Low-loss Capacitor terminations is calibration kit for LCR Meter/Impedance Analyzer and Network Analyzer (NA). The 16195B itself does not have warranted specification as independent product. Maintenance of the 16195B depends on what instrument you calibrate with 16195B.

FAQ 2017-03-15

How do I get replacement parts for individual items in the training kit?
Here are the parts that need to be purchased from Keysight at www.keysight.com/find/parts

FAQ 2017-02-26

XY Display Mode Example
The XY time mode converts the oscilloscope from a volts-versus-time display to a volts-versus-volts display using two input channels.

FAQ 2017-02-24

How do I create an amplitude correction file in Excel and load it into my X-Series Analyzer?
Details using Excel can be found here...

FAQ 2017-02-08

Looking for the best cheap oscilloscope?
Professional quality, low cost oscilloscope. Keysight 1000 X-Series oscilloscope proves a cheap oscilloscope doesn't have to be low quality.

FAQ 2017-02-07

FieldFox Manuals, Firmware, Software and Product Support
Manuals, firmware upgrade, software trials & upgrade and support page for FieldFox analyzers

FAQ 2017-02-02

Why does the FPGA Configuration Window appear upon boot up?
Information on why the FPGA Configuration Window appears...

FAQ 2017-02-02

Is there a 3D model of the Infiniium V-Series oscilloscopes?
Yes, see the Step format file downloads.

FAQ 2017-01-25

Is There a GPS Receiver for FieldFox?
GPS capability has been added to FieldFox starting from firmware revision A.05.33.

FAQ 2017-01-23

What is the maximum USB flash drive storage limit with FieldFox?
FF USB storage

FAQ 2016-11-28

Where do I download the mechanical drawings for the M9502A?
Files can be imported into your modeling application.

FAQ 2016-11-16

Previous 1 2 3 4 5 6 7 8 9 10 ... Next