Here’s the page we think you wanted. See search results instead:

 

Hable con un experto

Soporte Técnico

Medición Electrónica

Support by Product Model Number:

76-100 de 289

Ordenar:
What is the calibration cycle for the 8156A optical attenuator?
The recommended calibration cycle for the 8156A is 24 months.

FAQ 2011-07-06

Can I connect angled to flat or straight or visa versa?
No, generally neither connection of different connector types (straight vs. angled) can be done.

FAQ 2011-07-06

How is a computer's fingerprint ID obtained?
To rely on the CPU- ID remove the network-card before installing the PFL.

FAQ 2011-07-06

Do the 8165XA FP Laser Sources have optical isolators on the output?
Each 8165xA FP Laser Source has an optical isolator on the output.

FAQ 2011-07-06

What is the difference between the 8163xA and the 8163xB power sensors?
The 8163xA optical power sensors did not have an analog output available.

FAQ 2011-07-06

Do the 81611/12/13/14A Optical Return Loss Modules have an external source input?
Yes, the 81611/12/13/14A Optical Return Loss Modules each have an input for an external source.

FAQ 2011-07-06

What accessories should I order with the 8166XA DFB Laser?
An 816x mainframe is required to operate a DFB Laser Source Module. Additionally, a connector adapter ...

FAQ 2011-07-06

Can I control the large slot tunable laser wavelength using an external analog voltage?
There are several techniques which can be applied to scan the tunable laser wavelength.

FAQ 2011-07-06

Can the output power on the 8166xA DFB source be adjusted?
The maximum output power on the sources can be attenuated up to 6.0 dB, in 0.1 dB steps.

FAQ 2011-07-06

Can the 81003FD be used with the 81002FF integrating sphere?
No, the 81003FD will not work with the 81002FF integrating sphere.

FAQ 2011-07-06

Does the 81689A operate with the Lambda Scan in the PNP Drivers?
No, Lambda Scan requires one of the large slot tunable lasers.

FAQ 2011-07-06

What accessories should I order with the 8165XA FP Laser?
An 816x mainframe is required to operate a FP Laser. Additionally, a connector adapter ...

FAQ 2011-07-06

What accessories should I order with a 8163X power sensor module?
The power sensors will not be able to operate as standalone instruments.

FAQ 2011-07-06

What are the differences between the 81610A and the 81611/12/13/14A Optical Return Loss Modules?
The 81610A does NOT have an internal source, while the 81611/12/13/14A all do.

FAQ 2011-07-06

How can I reset the password to the factory setting '1234'?
The password, as well as all other user settings, can be reset to the factory default settings by ...

FAQ 2011-07-06

What accessories should I order with the 816XX Tunable Laser Sources?
See long answer.

FAQ 2011-07-06

How can I mount an optical head in an instrumentation rack?
To mount two (2) 8162x optical heads side by side next to an 8163A optical multimeter, please order ...

FAQ 2011-07-06

How do I calibrate the 81534A Return Loss Module with the 81610CC Reference Cable?
A patchcord between the output of Return Loss Module and 81610CC reference cable has to be used..

FAQ 2011-07-06

What is the monitor output option for the 8156A optical attenuator?
When the attenuator is ordered with the monitor output, a 13 dB coupler is placed after the attenuator ...

FAQ 2011-07-06

What is the rack mount kit for the 8156A optical attenuator?
Below is a list of possible rack mount part numbers for the 8156A.

FAQ 2011-07-06

How do I upgrade the firmware for large slot tunable lasers in the 8164 mainframe?
You can upgrade the 816xx full size tunable lasers firmware via GPIB, via floppy disks or ...

FAQ 2011-07-06

How can I read the responsivity data of my 8163x optical power sensor module, optical head, and ...
To read out the responsivity data of your optical power sensor module, optical head or attenuator ...

FAQ 2011-07-06

Can I use the 815xxA Series optical heads with the 81618A / 81619A interface modules?
The 815xxA Optical Heads can NOT be used with the 81618A/81619A interface modules.

FAQ 2011-07-06

Is the 8156xA suitable for Cable TV applications?
The angled connector versions 81561A and 81567A avoid irritating interference effects.

FAQ 2011-07-05

What accessories should I order with the 8162x optical heads?
The heads will not be able to operate as standalone instruments. The following accessories are needed ...

FAQ 2011-07-05

Anterior 1 2 3 4 5 6 7 8 9 10 ... Siguiente