Here’s the page we think you wanted. See search results instead:

 

Hable con un experto

Soporte Técnico

Medición Electrónica

Support by Product Model Number:

101-125 de 285

Ordenar:
Is the power control loop of the 81566A/67A also working for signal packets?
Yes, the averaging time of the 81566A/67A has to be adjusted to a time significantly longer than ...

FAQ 2011-07-05

Can I use the newer 816xx modules in the older 8153A mainframe?
The new 816xx modules will NOT operate in the older 8153A mainframe.

FAQ 2011-07-05

Why can't I install the license key from my PFL CD-ROM?
If you have PFL version 1.0.3 the installation process is described on the CD-ROM (PFL README.pdf).

FAQ 2011-07-05

What happens if the power unit is changed from dBm to Watt or vice versa?
All dependent parameters are automatically converted accordingly so all features remain fully functional.

FAQ 2011-07-05

Does Keysight Technologies offer analog outputs for the optical heads?
Keysight Technologies offers several different optical heads:

FAQ 2011-07-05

I am going through several patch cables before I connect to my device. Where do I establish my reference?
If you are measuring return loss through several patch cables there are three calibrations which are ...

FAQ 2011-07-05

Is the 8156xA suitable for Cable TV applications?
The angled connector versions 81561A and 81567A avoid irritating interference effects.

FAQ 2011-07-05

What is the calibration cycle for the 816x mainframes?
The 816x mainframes do not require calibration.

FAQ 2011-07-05

Should I use a Germanium (Ge) or a Indium Gallium Arsenide (InGaAs) optical head?
An important difference between Ge and InGaAs is the shape of the spectral responsivity curves.

FAQ 2011-07-05

Why can't I acquire the license key?
To rely on the CPU- ID remove the network-card before installing the PFL.

FAQ 2011-07-05

I need to perform return loss measurements on multimode cable. Will 8161x RTL modules allow me to do so?
Specifications are not valid if using a multimode cable.

FAQ 2011-07-05

Will the 8164A mainframe print in color?
The 8164A will not print in color to an external printer.

FAQ 2011-07-05

Does the parameters 'averaging time' and 'speed' influence the power control loop of the 81566A/67A?
The user selected averaging time is effective for all internal power measurements...

FAQ 2011-07-05

Can I use the 816xx series modules in any of the 816x mainframes?
The compact modules will operate in any of the 816X mainframes. However, the large slot tunable ...

FAQ 2011-07-05

What is the difference between the FETCH and the READ command to get the data from the power modules?
The FETCH and READ command will both acquire a power reading from the mainframe.

FAQ 2011-07-05

How small is CD and PMD of the 8156xA?
The value of CD and PMD of the 8156xA is equivalent to the value of about 1 m optical fiber SMF28.

FAQ 2011-07-05

Why would I want to use the analog output on the front of the optical head?
The analog output provides a voltage (0-2V) proportional to the optical power in a given range ...

FAQ 2011-07-05

Is there an electrical extender cable available for the 8162xA/B optical heads?
The model number of this cable, with a length of 4 meters, is 81624CE.

FAQ 2011-07-05

What is the difference between the 8162xA and the 8162xB optical heads?
The main difference is the 8162xB models (except the 81625B) offer an analog output, the 8162xA's do not.

FAQ 2011-07-05

Can I use both PC and APC connectors with the optical heads?
Yes, you can use both straight (PC) and angled (APC) fiber with the Keysight Technologies optical heads.

FAQ 2011-07-05

How can I link the 8164A with the 8166A?
The mainframes can be linked together with a GPIB cable, where a remote PC takes the control ...

FAQ 2011-07-05

Why should I use an optical head for optical power measurements?
Use heads for bare fiber, open beam, highly accurate absolute power or high power measurements.

FAQ 2011-07-05

Can I use the 815xx Modules with the newer 816x mainframes? What are the trade-offs?
The 815xx modules will operate in the 8163 and 8164 mainframe, but NOT in the 8166 mainframe.

FAQ 2011-07-05

What is the calibration cycle for the interface modules?
The 81618A/81619A interface modules do not require calibration.

FAQ 2011-07-05

How much hysteresis does the power control loop of the 81566A/67A show?
There are two threshold levels (if power control is active).

FAQ 2011-07-05

Anterior 1 2 3 4 5 6 7 8 9 10 ... Siguiente