이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

201-225 / 1735

정렬방식:
Keysight Driver Migration Tool

FAQ 2012-01-20

The Keysight 8761B SPDT Coaxial Switches are not listed in the "Keysight 34945A, L4445A and L4490A/L4491A Configuration Guide". Why?
Due to the 8761B’s internal design the RF path selection is achieved via DC polarity reversal across the coil control terminals. The Keysight 34945A, L4445A and L4490A/L4491A Control Units do not provide a polarity reversal mode. Thus the 8761B cannot be controlled by the 34945A, L4445A and L4490A/L4491A Control Units.

FAQ 2012-01-16

ValiFrame MHL
Download ValiFrame software from BitifEye support page...

FAQ 2012-01-11

Does the ENA support 87050E / 87075C series multiport test sets?
Unlike the E5061A and E5062A, the E5061B, E5071C and E5072A (ENA) does NOT support full functions of 87050E / 87075C. But it is possible to change switch state of 87050E-Hxx / 87075C-Hxx via GPIB.

FAQ 2012-01-11

N9081A Bluetooth® 측정 어플리케이션에서 키사이트 X-시리즈 분석기는Bluetooth 호핑 신호를 측정할 수 있습니까?
단정해서 대답하자면 "측정할 수 없습니다". 블루투스 장치의 기능 작동을 테스트하려면 주파수 호핑이 근본적으로 필요합니다.

FAQ 2012-01-10

Bluetooth® ACP 특정을 완료하는 데 어떻게 해서 15분이 소요됩니까?
ACP 측정에 필요한 시간은 블루투스 테스트 사양 요구사항때문입니다.

FAQ 2012-01-10

송신 분석(Transmit Analysis)의 피크 전력은 3.78dBm인데, 제로 스팬에서는 왜 3.66dBm입니까?
그것은 전력 도메인에서 측정하는 것이 아니라 IQ 도메인에서 측정하므로 VBW 펑션이 없습니다. 가장 중요한 계수는 버켓 폭입니다.

FAQ 2012-01-10

BER 테스트는 N9081A Bluetooth® 측정 어플리케이션에서 언제 적용합니까?
BER 테스트는 PRBS9 신호 패턴과 관련하여 EDR에만 적용됩니다.

FAQ 2012-01-10

N9081A와 W9081A는 Bluetooth® 4.0을 지원할 수 있습니까, 아니면 향후 지원할 예정입니까?
예. N9081A와 W9081A는 Bluetooth 4가 실현하는 저전력 측정을 지원합니다.

FAQ 2012-01-10

What are the differences between Keysight M918xA DMMs and Signametrics SMX2060 Series DMMs?

FAQ 2012-01-01

PDF PDF 387 KB
What is a BSDL logical port?
The Boundary Scan Description Language (BSDL) logical port description is used to assign names and connections on the device pin.

FAQ 2012-01-01

What is a linkage bit in a BSDL?
The linkage bit in a Boundary Scan Description Language (BSDL) is use to describe a nondigital pins such as power, ground, no-connects, or analog signals in a boundary scan device.

FAQ 2012-01-01

How do I repair the E6621A measurement application if it fails to launch?
A utility is available that will fix the E6621A measurement application. Click on the question above for a fuller description.

FAQ 2011-12-23

Can I recover the E6621A operating system if it fails to start correctly?
Yes, E6621A has a System Software Recovery mode. Click on the question above for a fuller description.

FAQ 2011-12-21

Can the 816x mainframes be controlled via GPIB?
Yes, the 816x mainframes offer complete GPIB control using either SCPI commands or the VXI PNP drivers.

FAQ 2011-12-09

What is a boundary scan linker mux?
A boundary scan linker mux (multiplexer) device, also known as JTAG scan bridge or scan path linker.

FAQ 2011-12-01

Is it possible to test non-boundary scan digital devices connected to boundary scan devices?
This test strategy is commonly known as Silicon Nail test where the boundary scan cell (driver/receiver) of the boundary scan device connected to the non boundary scan device pins will be able to simulate the operation of the non-boundary scan device.

FAQ 2011-12-01

Can I purchase external cables for my N4011A?
Yes. Click on the question above for a fuller description.

FAQ 2011-11-30

How can I set up File Security and board directories with NFS share?
Once you have enabled “Client for NFS”, you can mount any NFS share on your network. There are a few ways to set up NFS share file security.

FAQ 2011-11-01

How to access board directories resided on the Linux/Unix server using SAMBA/Common Internet File System (CIFS), if ICT controller is on Windows® 7?
SAMBA is a utility which allows you to share your files between Linux/UNIX and Windows®. By mounting the SAMBA share on your Linux/UNIX server, you can access the board files across the operating systems.

FAQ 2011-11-01

How can I turn on the Services for NFS on Windows® 7 ICT controller?
Both the Windows 7 Ultimate and Windows Enterprise Edition contain the client for the Network File System (NFS) and Subsystem for UNIX-based Applications (SUA).

FAQ 2011-11-01

How can I access my i3070/3070 ICT board directories residing on Linux/UNIX controller, if I am running my ICT controller on Windows® 7?
Services for Network File System (NFS) and Subsystem for UNIX-based Applications (SUA) are the software packages provided by Microsoft® to enable the UNIX subsystem and other parts of the UNIX environment to be integrated onto the Windows environment.

FAQ 2011-11-01

What are the known conflicts between MKS NutCracker and Interix and the recommended workaround solutions?
There are three known key issues which you need to look out for:

FAQ 2011-11-01

What is a USERCODE instruction?
The USERCODE is an optional instruction in the boundary scan description language) (BSDL) that allows a 32-bit user programmable identification code to be loaded and shifted out for examination.

FAQ 2011-11-01

How can I turn on the SUA and its UNIX utility package on Windows® 7 ICT controller?
It is recommended that you DO NOT enable or install SUA. This is an optional feature and utility that is not needed for mapping NFS share.

FAQ 2011-11-01

이전 1 2 3 4 5 6 7 8 9 10 ... 다음