이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

176-200 / 1735

정렬방식:
Which Connector Types Can Be Safely Connected, and Which Types May Cause Damage to the Interface?

FAQ 2012-04-05

What TAP signals are sampled during the rising edge of a TCK signal?
The test mode state (TMS) and test data in (TDI) signals are sampled into the test logic on the rising edge of a test clock (TCK) signal.

FAQ 2012-04-01

What TAP signals are sampled during the falling edge of a TCK signal?
The test data out (TDO) signals of the test access port (TAP) are sampled into the test logic on the falling edge of a test clock (TCK) signal.

FAQ 2012-04-01

How can I clear the memory on an 8566B, 8567A, or 8568B Spectrum Analyzer for security reasons?
See content for details on this subject....

FAQ 2012-03-29

How do I establish a peer-to-peer connection between my PC and an InfiniiVision 5000/6000/7000 Series oscilloscope?
There are two methods ...

FAQ 2012-03-27

키사이트 89600B VSA 소프트웨어(89601B)는 Bluetooth® Difference Error Vector Magnitude (DEVM) 테스트를 지원합니까?
89601B 옵션 AYA는 블루투스 기본 측정에 대한 DEVM 결과를 제공하지 않습니다. 키사이트는 N9081A Bluetooth 측정 어플리케이션을 사용할 것을 권장하고 있습니다.

FAQ 2012-03-22

PSA 시리즈 스펙트럼 분석기를 N5530S 측정 수신기 시스템에서 작동시키려면 어떤 옵션이 필요합니까?
옵션 B7J, 옵션 123, 옵션 1DS 및 E4440AU 옵션 233

FAQ 2012-03-15

What field of view (FOV) magnifications are available?
The x6000 does not use the field of view (FOV) concept, it uses an autofocus technique that sizes the inspection image to the joint type being inspected. Several slices are evaluated for the sharpest region to determine the slice location.

FAQ 2012-03-12

What 8960 settings might I need to change from the default power-on state to get my W-CDMA mobile to connect on a call?
W-CDMA is a very flexible technology that requires the UE firmware, 8960 settings, and uSIM values to be consistent. If you are experiencing difficulty with Location Update, Authentication, or Call Connection, try some of these settings, one at a ...

FAQ 2012-03-02

How does the 8960 & E1961A AMPS/136 Mobile Test Application compare to the 8920B?
This comparison table indicates the ....

FAQ 2012-03-02

IO Libraries Suite: What has changed in IO Libraries Suite 16.2?
IPv6 support, increased support for AXIe, support for Command Expert, bug fixes...

FAQ 2012-03-01

How much the default RF port power of N4375B? And can I change it?
It is 0 dBm, and you can change it.

FAQ 2012-03-01

PDF PDF 46 KB
How do I determine the maximum test clock (TCK) frequency of the boundary scan device?
The boundary scan device test clock (TCK) information is described in the boundary scan description language (BSDL) at the TAP port identification which assigns a special meaning to these signals.

FAQ 2012-03-01

What is a Compliance Enable pin?
Compliance enable pins are device pins that must be held at a static logic state (0 or 1) before the device enters into any 1149.1 activities.

FAQ 2012-03-01

Is there an advantage when purchasing the E6569 WTM Suite over purchasing the individual products separately?
The price of the suite is much lower than purchasing all the WTM separately. The other difference is that the Suite is licensed for a single PC and ships with one security key. More...

FAQ 2012-03-01

How do I make spectrum analysis measurements on signals above 110 GHz using a PSA Series Spectrum Analyzer (E4440A, E4446A, E4448A)?
With the addition of option AYZ on the PSA a user can connect external harmonic mixers to measure signals up to 325 GHz. Mixers in the frequency range of 110 to 325 GHz are available from third party venders such as Olssen Microwave.

FAQ 2012-02-28

How do I make spectrum analysis measurements on signals above 50 GHz using a PSA Series Spectrum Analyzer (E4440A, E4446A, E4448A)?
The PSA offers an option (AYZ) enabling the use of external millimeter harmonic mixers.

FAQ 2012-02-28

Do I need a bias tee or a diplexer for the 11970 or 11974 series harmonic mixers?
Neither the 11970 or 11974 Series requires a bias tee or diplexer.

FAQ 2012-02-28

How do I recover my PSA Spectrum Analyzer after a secure erase memory sanitization?
A secure erase memory sanitization clears all of the user writable instrument memory. Firmware and measurement personalities must be reinstalled.

FAQ 2012-02-26

Can I use 11970 or 11974 Series external mixers with my 859x Series Spectrum Analyzer?
No, while the 859X products did offer an L.O. output on the rear panel with option 010 Tracking Generator, there was never a provision for an I.F. Input, which is required for external mixing.

FAQ 2012-02-25

In Help, why are some features not documented? There are also some screenshots of the User Interface in Help that do not match my WTM.
Do you have more than one WTM loaded on your PC? Did you install an older WTM after the newer version? This can overwrite Help and Language Table files. More...

FAQ 2012-02-24

Why must my N4010A instrument firmware be A.05.04.01 (or newer)?
This is the minimum firmware revision for a hardware change that was introduced during December 2011.

FAQ 2012-02-24

8167 시리즈와 8168 시리즈 튜너블 레이저 소스(8167A/B, 8168A/B/C/D/E/F)에서 커넥터 옵션 021, 022와 023의 차이는 무엇입니까?

FAQ 2012-02-17

What is a Bypass Instruction?
The Bypass Instruction is an IEEE 1149.1 mandatory instruction which select the single bit Bypass register between the TDI and TDO.

FAQ 2012-02-01

What is a Bypass Register?
A Bypass Register is an IEEE 1149.1 mandatory register which consist of a single boundary scan cell.

FAQ 2012-02-01

이전 1 2 3 4 5 6 7 8 9 10 ... 다음