이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

126-150 / 1734

정렬방식:
How long does it take to measure a BER of 1 x 10(-12) at a data rate of 9.953Gb/s? What about at 2.488Gb/s?
It is not possible to predict with certainty when errors will occur. Therefore, you must use a confidence level to know when you have tested error-free for long enough to say that you have a BER of better than 10(-12) performance.

FAQ 2012-12-12

Can I remotely query the 86100D DCA-X to determine which user interface is running?
Yes. Issue the query :SYSTem:FCONfig? If the response is "Legacy" then the legacy UI is in use. If the response is "Compatible" or "Standard" then the FlexDCA interface is in use.

FAQ 2012-12-12

What is SCANSTA112 device?
The SCANSTA112 device is a 7-port multidrop IEEE 1149.1 (JTAG) multiplexer design to connect boundary scan chains into a single chain as well as the ability to remove a board from the system and retain test access to the remaining chains.

FAQ 2012-12-01

What are the failures that boundary scan test can detect?
Boundary Scan test will be able to diagnose the following failures:

FAQ 2012-12-01

Why are some of the features shown in the Framescope user manual not available in software version 7.0.5?
Users might encounter different features when using Framescope software version 7.0.5 versus what is stated in the documentation.

FAQ 2012-11-28

What you need to know about Advanced DGN Reporting?
Frequently Asked Questions about Advanced DGN Reporting.

FAQ 2012-11-28

How to debug the 3 differences that are encountered on the new hybrid pin cards (P/N: E4000-66562 and E4000-66563)?
Follow the guideline to debug your test when you start using the new bybrid pin cards: • E4000-66562 for 6MPs (standard hybrid pin card) • E4000-66563 for 12MPs (advanced hybrid pin card)

FAQ 2012-11-12

Why must my N4010A instrument firmware be A.05.06.02 (or newer)?
This is the minimum firmware revision for a hardware change that was introduced during October 2012

FAQ 2012-10-30

외부 믹서 연결 옵션 EXM은 11974 시리즈 Preselected Mixer를 지원할 예정입니까?
아니요.

FAQ 2012-10-25

Waveguide 플랜지용 교체 보호 캡은 어떻게 주문할 수 있습니까?

FAQ 2012-10-23

Sample DLL for i3070 External DLL Feature
External DLL (dynamic- link library) call feature expands i3070 platform capability for additional functional test / application in a flexible way. Here is a DLL example of data management, updating the test status to a database.

FAQ 2012-10-18

What external mixers will work with my PXA/mmW EXA and how do I order them?
Currently, the N9030A PXA/mmW EXA with Option EXM will work with either the 11970 Series (with the exception of the 11970K) or ) or external mixers from other vendors such a OML Inc. mixers.

FAQ 2012-10-17

How to report a VEE bug, serious error or submit an enhancement request effectively?
1. Go to the VEE Help menu and select Customer Feedback option...

FAQ 2012-10-16

FrameScope Pro Download

FAQ 2012-10-16

IO Libraries Suite: Can I use VXI on a 64-bit OS?
IO Libraries Suite 16.1 (or later) supports VXI (E8491A/B and E1406A) on 64-bit Vista, 7, Server 2008 R2...

FAQ 2012-10-10

IO Libraries Suite: IO Monitor란 무엇인가요?
IO Monitor는 키사이트 VISA, VISA COM 및 SICL I/O 라이브러리의 I/O 호출을 추적하는 유틸리티입니다.

FAQ 2012-10-09

IO Libraries Suite: 고객이 제공한 Suite 14 이상에서 이전 버전을 사용할 수 있습니까?
키사이트 계측기를 한 대 갖고 있는 고객이라면 버전과는 상관 없이 IO Libraries Suite 라이센스 한 개를 사용할 수 있는 법적 권리가 있습니다.

FAQ 2012-10-08

IO Libraries Suite 15 라이센스는 어떻게 구할 수 있나요?
키사이트는 약 150가지 키사이트 계측기 모델, GPIB 및 I/O 컨버터 제품, T&M Toolkit 및 VEE Pro 소프트웨어 개발 복사본과 함께 IO Libraries Suite를 무료로 제공해 드리고 있습니다.

FAQ 2012-10-08

Why do I need to hold the state of certain pins/nodes?
Non-boundary scan devices such as DDR or flash memories need to hold one or more nodes (chip select/enable) to fixed states during boundary scan testing, so that the device is disabled during boundary scan testing and its output pins (i.e. data) are not activated, as otherwise, it will cause unstable tests or damage to the circuitry. Boundary scan “hold states” are node/device pins on a board that are held to a logic of 1 or 0 by a boundary scan driver on the node, when the boundary scan device driver/output pin is in EXTEST.

FAQ 2012-10-01

What is the CAPTURE State?
During the CAPTURE state, data or instruction bits are loaded in parallel into data or instruction registers. The CAPTURE-DR (Data Register) loads data bits into the specified data register. CAPTURE-IR (Instruction Register) loads instruction bits into the Instruction Register.

FAQ 2012-10-01

All IntuiLink Tools for Keysight Oscilloscopes
Supported Models: Infiniium Series, 1000 Series, 2000 X-Series, 3000 X-Series, 5000 Series, 6000 Series, 7000 Series, and 54600 Series Oscilloscopes

FAQ 2012-09-26

How can I de-embed a test fixture using the 86100C/D Digital Communications Analyzer?
N1010A software with InfiniiSIM-DCA option provides the capability to de-embed and embed fixtures, cables, probes, and other circuit elements.

FAQ 2012-09-25

XVision fails to install on some laptops
Before installing XVision /ICT software, please follow the steps below:

FAQ 2012-09-25

What is the typical power consumption of the 86100C and 86100D Digital Communications Analyzer?
Typical measurements of 86100C and 86100D power consumption

FAQ 2012-09-25

What is the Boundary Scan device Normal Operation mode?
When the device is operating under the normal mode, the boundary register is transparent. Signals can pass through the boundary scan cells freely and the device operates as it would without test cells. In this mode, test data is captured in the boundary register cells, then shifted through the boundary register out to TDO.

FAQ 2012-09-01

이전 1 2 3 4 5 6 7 8 9 10 ... 다음