By Topic

By Type of Content

By Product Category

1-11 of 11

Sort:
Where can I find information or example programs using the API for Signal Studio?
The Signal Studio for pulse building help file has information and example programs under the API control chapter.

FAQ 2013-05-16

What happens to nested patterns and off-time packets in pulse mode?
Nested patterns are flattened. This means that a single trigger will not play the entire pattern. It merely steps into the pattern and plays the first pulse. The next trigger plays the next pulse, etc. Off-time packets are ignored in pulse mode.

FAQ 2012-12-28

Do corrections work with frequency and amplitude offsets?
Yes, however, the amplitude flatness accuracy is set by the spectrum analyzer flatness accuracy across the signal bandwidth...

FAQ 2012-12-28

Why can’t I view a help file downloaded from the Keysight website?
After downloading the file to your PC, open it from the location it was saved and a security warning appears. To view the help system, clear the checkmark from the "Always ask before opening this file" check box.

FAQ 2012-12-28

What is the best configuration for wideband I/Q modulation?
An E8267D Option 016 or an N8212A Option 016 signal generator with an M8190A arbitrary waveform generator

FAQ 2012-12-28

How many measurements do I need to make and how long is the predistortion data good?
The number of measurements needed depends on the number of parameters that are changed. The calibration (measurement data) could be valid for two days or longer.

FAQ 2012-12-28

How much time/frequency error is introduced by the Custom Profile or Custom I/Q resampling?
After using the formula to calculate the number of resampled data points, work backwards to determine the error.

FAQ 2012-12-28

Why is the FSK modulation index of the ESG limited to about 4 or less on the E4438C and 1 or less on the E443XB?
The interpolation in the DSP algorithms for the baseband generator limits the modulation index.

FAQ 2012-06-07

Can I control a Keysight 4284A/E4980A using my B1500A to make CV measurements and display the results in the EasyEXPERT data display window?
Yes.

FAQ 2011-02-15

Does the ESG or MXG with N7625B Signal Studio support the UE receiver tests?
Yes, the E4438C (ESG) or N5182A (MXG) with the N7625B LTE TDD signal studio can generate both LTE TDD downlink and uplink signals. So it can be used for receiver components (such as power amplifiers and transmitter, receiver, or transceiver RFICs)...

FAQ 2009-11-13

Why are you offering 3 instruments in 1? What if my customer needs only one of these instruments?
In addition to precise pulses and trigger customers need to stress the device to its limits. In the past they used either a second channel or an additional instrument to distort the signal. With the new build-in capabilities real-world signals can...

FAQ 2008-01-29