Discuter avec un expert

Support technique

Spectrum Analyzers (Signal Analyzers)

Recherche par numéro de modèle du produit: Exemples : 34401A, E4440A

1-25 sur 32

Tri:
Why do I continue to get the "Align 20 Hz to 3.6 GHz Required" message even though I ran the Align Now, All routine on my MXE?
You also need to run the System, Alignments, More, RF Preselector, Align Now alignments...

FAQ 2014-03-03

Why Do I Get an Install Error Message When I Try to Upgrade my Firmware?
The likely cause is a conflicting file name.

FAQ 2012-08-17

Why Do I Get a "Meas UNCAL" Message During Zero Span Measurement in Signal Analyzer Mode?
The “Meas UNCAL” message during zero span measurements indicates that the capacity of the capture memory has been exceeded for the current combination of RBW and sweep time.

FAQ 2012-08-17

Why Does FieldFox Sometimes Revert to a Zero Serial Number at Power On?
The firmware needs to be upgraded to ≥ A.03.02.

FAQ 2012-08-15

What is preventing the 89600A software running on a PC from connecting to an X-Series analyzer?
These requirements MUST be observed when using the 89600A VSA software with an X-Series Signal Analyzer.

FAQ 2012-06-12

Why do I get a Meas Uncal message when I select either the Quasi-Peak or EMI Average detector for taking a full band sweep with the MXE EMI Receiver?
Sweeptime has reached its maximum. See complete FAQ for further details...

FAQ 2012-05-10

Why do I get the "Align 20 Hz to 3.6 GHz Required" message every time I turn my MXE on?
You don't. Wait for it to warm back up...

FAQ 2012-05-09

What causes the "Final IF Overload" message and how do I correct for the message?
This message occurs when the Final IF is overloaded. This occurs at a mixer level > -8 dBm.

FAQ 2012-02-27

My PSA Series Spectrum Analyzer Shows error +605 Data Corrupt or Stale, NRAM copy of !....
The non-volatile RAM battery has expired. The replacement battery P/N is 1420-0314C. Click here for additional information.

FAQ 2012-02-26

What is the frequency range of the N5532A Sensor Module?
100 kHz to 4.2 GHz, 10 MHz to 18 GHz, 30 MHz to 26.5 GHz, and 30 MHz to 50 GHz.

FAQ 2012-02-26

For the E4406A VSA with the latest firmware and the X-Series Analyzers, why are the displayed results for W-CDMA Modulation Accuracy (Rho) different?
Previously with PSA A.06 firmware (E4406A A.07 firmware), mod accuracy only supported 1 slot capture. The current firmware now supports capturing a full frame, and this is the new default setting.

FAQ 2012-02-26

Can I make Noise Figure Measurements below 10 MHz with the ESA-E Series Spectrum Analyzer?
Yes, you can make useful noise figure measurements with the ESA-E Series Spectrum Analyzer down to 200 kHZ, however, no instrument specifications are provided.

FAQ 2012-02-25

Must I return my 89441A Vector Signal Analyzer (VSA) for repair if it displays an "RF LO Unlock" error?
If the error message occurs and persists, a failure has occurred in the RF section of the VSA.

FAQ 2012-02-25

Does the user interface of the handheld spectrum analyzer support multiple languages?
Yes, the user interface for each of the HSA models supports eleven languages.

FAQ 2012-02-20

Why Do I Get a "VCO Unlock Error" on my N9923A?
The solution is to upgrade firmware to A.05.04 or later.

FAQ 2011-11-14

How Do I Avoid a "Buffer Overflow" Error Message When Performing with TME Software Adjustment?
Use a direct crossover cable between your FieldFox and your PC.

FAQ 2011-08-29

What causes the error "Failed to load TraceCtrl from AgtTrace2.ocx" when 89601A VSA software is starting?
This FAQ provides instructions for removing an invalid registry key that causes 89601A VSA to display the error "Failed to load TraceCtrl from AgtTrace2.ocx" .

FAQ 2010-11-22

How do I correct VSA license errors?
Troubleshooting procedure inside.

FAQ 2010-11-22

What to do when, "Unwise.exe file missing," error message is given?
Save the file into C:\glacier_cd directory. (library # 1340106)

FAQ 2010-05-03

Is it possible to get an error log of incorrectly sent remote commands to my PSA, E4406A, EMC, or ESA Series Spectrum Analyzer?
Yes. PSA, E4406A and the ESA Series (with firmware A.08.00 and later) support this. You may turn Verbose error logging on through the front panel or remotely, SYST:ERR:VERBOSE ON

FAQ 2008-11-21

Why do I get a message telling me that I need Option B72 when I try to load the latest version of firmware into my ESA Spectrum Analyzer?
Due to the increased number of features included, firmware versions A.08.02 or later require a larger amount of memory.

FAQ 2008-10-27

How do I correct the "Could not start ngn" license error that occurs when the 89600 VSA software starts?
Copying a file from one directory to another will correct this error.

FAQ 2008-08-11

My Infiniium scope application is not running properly. Is there a way to reset it?

FAQ 2007-01-05

My Infiniium oscilloscope with the removable hard drive will no longer boot up, why?
Make sure the removable drive key lock is in the locked position.

FAQ 2006-10-20

Why can't my ESA-E Series Spectrum Analyzer demodulate a low level FM signal?
You may have encountered a firmware issue if the instrument is using firmware <=A.01.02. Upgrade the instrument firmware to resolve this issue.

FAQ 2004-09-18

1 2 Page suivante