Here’s the page we think you wanted. See search results instead:


Hable con un experto

The Importance and Value of PXI Multi-Vendor Interoperability

1   Hour | Webcast - grabado | Where & When

What is the Webcast About?
The strength of PXI lies in its widespread adoption as an open, multi-vendor technology platform for test and measurement. PXI now boasts over 70 technology manufacturers supplying over 1500 modules which allows for a very comprehensive ecosystem and limitless system development opportunities. In this seminar you will learn more about how the requirements of the PXI Standard create the framework of interoperability between modules/controllers/chassis designs from the variety of vendors building PXI (and PXI Express) instruments. You will also see examples of interoperability between leading PXI instrument providers.

Who Should View this Webcast?
This seminar will be valuable to engineers designing, specifying or creating automated test systems.

Where & When

Price Location For more information
Free At Your PC Enroll to view the March 28, 2012 recorded broadcast 

Prices shown are list prices and are subject to change without notice.

Training & Event Materials

The Importance and Value of PXI Multi-Vendor Interoperability Webcast Slides 
Slides from March 28, 2012 Webcast

Seminar Materials 2012-03-28