Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Mastering Signal Integrity and Power Integrity Design Seminar

WHY THIS SEMINAR IS IMPORTANT

At every turn, a newer, faster, better interconnect standard is proposed. Standard Working Groups are hard at work on next-generation protocols, trying to squeeze out more speed in the face of ever increasing constraints. When it comes to digital standards, every generational change introduces new challenges and risks, in particular, issues with Signal Integrity (SI) and Power Integrity (PI). Design success demands that today’s engineer have the skills needed to overcome these challenges and face down any risks. In this seminar, Keysight experts will share their industry expertise and present design, analysis and simulation solutions for effectively addressing signal integrity and power integrity challenges.

WHAT TO EXPECT

Attendees will receive detailed information on SI and PI design, analysis and simulation. Additionally, they will learn new simulation techniques for DDR4/DDR5, electromagnetic extraction, PCIe Gen4, power integrity, and more.

WHO SHOULD ATTEND

High-speed digital design engineers, SI and PI engineers, design team managers, application managers, and application engineers.

COST

Free

DRAWING

Come and enter the drawing for Steven Sandler’s “Power Integrity” text book, a perfect resource for high speed-digital engineers.

WHEN/WHERE

Wednesday, June 28

Embassy Suites by Hilton - Irvine
Orange County Airport
2120 Main Street
Irvine, CA 92614
Ambassador Room

Tuesday, July 18

Sheraton Detroit Novi Hotel
21111 Haggerty Road
Novi, MI 48375

Wednesday, July 19

Park Plaza
4460 West 78th Street Circle
Bloomington, MN 55435
Superior Room

Thursday, July 20

Woodfield Preserve
10 N. Martingale Road LL10
Schaumburg, IL 60173
Conference Room: A & B
(Lower Level)

Wednesday, August 16

Boulder Marriott
2660 Canyon Blvd
Boulder, CO 80302

Thursday, August 17

Keysight Technologies
9780 South Meridian Blvd.
Englewood, CO 80112

Tuesday, September 26

Sheraton Harrisburg Hershey Hotel
4650 Lindle Rd
Harrisburg, PA 17111

 

Tuesday, September 26

Holiday Inn & Suites Ottawa
101 Kanata Avenue
Kanata, ON K2T 1E7
Kanata

Wednesday, September 27

Keysight Technologies
8825 Stanford Boulevard
Suite 300
Columbia MD 21045
Annapolis Room

Wednesday, September 27

Hilton Garden Inn Toronto/Markham
300 Commerce Valley Drive East
Thornhill, ON L3T 7X3

Thursday, September 28

Hilton Vancouver Metrotown
6083 McKay Avenue
Burnaby, BC V5H 2W7  

AGENDA

9:30am Registration / Refreshments
10:00am Welcome & Introductions
10:10am DDR5 is Coming, Are You Ready?
Accurate Statistical-Based DDR Margin Estimation

JEDEC plans to release the new DDR5 standard in 2018. DDR5 will provide double the bandwidth and density over DDR4, pushing the speed grade from 3.2 to 6.4 Gbps. Without a doubt, Rx equalization will be necessary to handle the closed eye in the DDR5 system. Random and deterministic jitter will play a more important role as well. This presentation will introduce a breakthrough simulation technology designed to help you with your DDR5 and DDR4 design challenges. You will learn how to predict the noise and jitter distribution at ultra-low BER and account for Rx equalization in the parallel bus simulation.
11:00am

Demystifying VIAs in High-Speed PCB Design
A high-speed signal traveling vertically through the board layer is several times more complex and difficult to analyze than a signal traveling horizontally along the same layer. This presentation covers the basics of VIA construction and its impact to high-speed signals. We will also highlight tips for better VIA design and introduce different simulation techniques for generating more transparent interconnects and allow you to make various tradeoffs.

11:50am How Much Bandwidth Do I Need for My Channel Model?
Are You Killing Your Schedule and Increasing Uncertainty with Unnecessary 100GHz Full 3D EM Simulations?

How much bandwidth do you need for your channel model? The traditional answer has often been “As wide and as accurate as I can get!” to give you as much margin as possible against unknowns. However, this approach comes with the penalty of increased time and cost associated with simulation and equipment. Even then, you still don’t really know if what you have is good enough. How many system variables could you explore when each channel model run takes several days? The good news is that there are some simple approaches you can use to help you find that sweet spot between time, accuracy and cost using both frequency and time domain simulation techniques, so you can be confident about your model!
12:30pm Lunch
1:20pm Chronicles of a High-Speed PCB
Take a journey through a high speed PC board. We will start where the Layout engineer finishes. We will import the completed board into our board extraction tool, explore traces, select traces and extract their model. We will then take the extracted model in to our circuit simulation tool and run post layout circuit simulation to be able to better predict the system’s behavior. We will do this for a Serial channel, and a parallel channel as each design has its own challenges. By the end of this journey we can send the board to the fab house with confidence!
2:10pm

Power Integrity is More Than Decoupling Capacitors
Understanding The Power Integrity Ecosystem

Power Integrity is more than loop inductances and decoupling capacitors. Along with the power plane target impedances, the Power Integrity engineer also needs to consider the VRM model, and have some level of power electronics knowledge and understanding of how to bring all of these pieces together. This presentation details a Power Integrity ecosystem that covers all of these topics in an effort to help you design a better board.

3:00pm PCI Gen-4: How Far Can a Bit Travel Before it Needs to Refuel?
End-to-End System-Level Simulation with Repeaters for PCIe Gen4
The design solution space is becoming increasingly complex for the PCIe Gen-4 system, especially when a repeater is needed to extend the reach between a Root Complex (RC) and End Point (EP) device. Since the repeater’s settings must be co-optimized with those of the Transmitter (Tx) and Receiver (Rx) to maximize overall link performance, the parameter tuning of active components becomes a daunting problem to tackle. This presentation details a “how-to” guide for defining, executing, and analyzing system-level simulations involving all three components.
 
3:50pm Wrap-up & Announcements