您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

Fundamentals of Transient Low-Current Measurement Webcast

1   小時 | 網路廣播 -- 存檔 | 地點與時間

WHAT IS THE WEBCAST ABOUT

The measurement of fast transient voltages is a relatively well-understood and documented procedure. However, the measurement of fast transient currents presents a number of measurement challenges that make them much more difficult than measuring voltage transients. Digital multi-meters (DMMs) and oscilloscopes using either shunt resistors or a current probe are the most common methods for measuring AC current, but they all have drawbacks:

1. DMMs have limited bandwidth and cannot reveal any details about dynamic current behavior

2. Oscilloscope shunt resistor techniques often introduce unacceptable voltage drops and noise, besides having limited dynamic range.

3. Oscilloscope current probes require degaussing and adjustment, and they cannot typically measure below a few microamps of current.

This webcast will review the above solutions and then explain new techniques and equipment that can support the measurement of transient currents into the nanoamp and picoamp range at 1 Ghz sampling rates and up to 200 MHz of bandwidth. While the primary focus of this webcast is on the characterization of devices and materials, many of the techniques to be discussed are general and can also be applied to other situations (such as component and module testing).

WHO SHOULD ATTEND

Engineers, scientists and researchers that need to make low-level transient current measurements would benefit from attending this webcast.

PRESENTER

Alan Wadsworth, Application Engineer, Keysight Technologies

Alan Wadsworth has over 30 years of experience in the semiconductor industry in both design and test. He is also the author of Keysight’s Parametric Measurement Handbook, which contains over 200 pages of information on semiconductor parametric test and measurement techniques. Alan holds Bachelors and Masters degrees in electrical engineering from the Massachusetts Institute of Technology and an MBA from Santa Clara University.

地點與時間

費用 地點 詳細資訊
免費 At Your PC Enroll to view the October 25, 2016 recorded broadcast 

上表所列為參考訂價,如有任何變更,恕不另行通知。