이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

Precision Validation, Maintenance and Repair of Satellite Earth Stations Webcast

1   시간 | 웹캐스트 - recorded | 시간 및 장소

WHAT IS THE WEBCAST ABOUT

Satellite communication systems have been used for decades to provide fixed point and mobile services to the commercial and military markets worldwide. Services include two-way telecommunications, navigation, and television and radio broadcasting . As in most modern wireless systems, satellite communications bandwidths have evolved over time with digital data rates starting from kilobits per second (Kbps) to current system-wide capacity of over 100 gigabits per second (Gbps).

There is now unprecedented development in the provision of new high throughput satellite broadband solutions capable of delivering internet, voice, video and other unique communications services. Major operators and broadcasters either have launched or are making plans for a wide range of applications, including not only consumer but also gas and oil, disaster recovery, aeronautical, maritime, military and other mission critical requirements. For each satellite deployment, there is a much larger set of terrestrial-based systems, or ground stations, ranging from satellite control facilities to end-user devices. The validation, maintenance and troubleshooting of these ground stations often requires a combination of indoor and outdoor testing of numerous RF and IF subsystems and components. This webcast will discuss modern solutions for ground station testing that are rugged, portable, battery operated and achieve measurement accuracy comparable to benchtop equipment. Measurement examples of ground station parameters such as uplink power level and frequency accuracy, downlink interference, converter (up/down) performance, group delay and transmission line fault location for coaxial and waveguide feeds will be discussed.

Co-sponsor:

WHO SHOULD ATTEND

Engineers, technicians and their managers involved in the performance verification, installation and maintenance of ground stations which are part of broadband military and commercial satellite communications systems.

PRESENTER

Tom Hoppin, Application Specialist, Keysight Technologies

Tom started his working career as an electronic aviation technician in the US Marine Corps. After his service in 1973, he joined Hewlett-Packard as a manufacturing technician. During his career at HP/Agilent, he moved from manufacturing to production engineering and was promoted to engineer in 1989. Since then, he has held a number of engineering and management roles at Agilent/Keysight, focused on test system design and spectrum analysis. Tom retired in 2009 and has returned to Keysight as an application specialist for our RF and Microwave Handheld Analyzers. Tom enjoys woodworking, cycling and sailing.

시간 및 장소

강의료 위치 자세한 정보
무료 At Your PC Enroll to view the Sept 18, 2014 recorded broadcast 

가격은 정가이며 예고없이 변경될 수 있습니다.

교육 및 이벤트 자료

Precision Validation, Maintenance and Repair of Satellite Earth Stations Webcast Slides 
Slides from the September 18, 2014 webcast

세미나 프리젠테이션 2014-09-18

PDF PDF 896 KB