키사이트테크놀로지스는 뉴욕증권거래소(NYSE)에서 거래가 가능한 독립된 회사입니다. | 자세한 내용 보기

 

전문가 상담

Fast Characterization of Power Amplifier Performance with Modulated Signals

1   시간 | 웹캐스트 - recorded | 시간 및 장소

RF Power Amplifier Design Series: Part 3

Why this webcast is important

Characterizing amplifier performance using sinusoids is reasonable during the early stages of the design process. However, gain compression from a one-tone sweep or intermodulation distortion from a two-tone sweep may not accurately predict ACLR or EVM, the real specifications. Designers need to know ACLR and EVM while an amplifier is delivering a specified output power, and they need to know how much statistical variation to expect. Also, they want to know what design parameters could be adjusted to improve performance. This paper shows techniques for carrying out these types of simulations. ADS examples will be provided.

Who should attend

Power Amplifier Designers
 

시간 및 장소

강의료 위치 자세한 정보
무료 At Your PC Enroll to view the Apr 5, 2012 recorded broadcast 

가격은 정가이며 예고없이 변경될 수 있습니다.