Here’s the page we think you wanted. See search results instead:

 

Parla con un Esperto

RF and Microwave Measurement Insights

 See more at HOTSPOTS Homepage

RF and Microwave Measurement Insights - Full Day Agenda
Register - At the bottom of the page
Welcome & Overview – Keysight
Topic 1: Spectrum Analysis Fundamentals
Networking and Refreshment Break
Topic 2: Vector Signal Analysis Fundamentals
Networking and Refreshment Break
Topic 3: RF Power Measurement Basics
Lunch Break
Topic 4: Network Analysis Fundamentals
Networking and Refreshment Break
Topic 5: RF Design & Simulation fundamentals
Hands-on & Demonstrations

Papers & Abstracts

Welcome & Opening: Keysight RF and Microwave Fundamentals Seminar

From the company that has been a leading innovator in Spectrum and Network measurements for 70 years, please join us for a FREE RF and Microwave Fundamentals Seminar to help improve your understanding of basic RF measurements, including real applications, thus improving your efficiency and effectiveness whether you are in R&D or design & test.

You can see our latest solutions, and expand on the practical knowledge you need to have to perform your day-to-day-measurements. Application and product experts from Keysight will be on-hand to give demonstrations and technical presentations around the latest innovations, features and capabilities that enhance the fundamental measurements.

Topic 1: Spectrum Analysis Fundamentals

“Insight into the fundamentals of Spectrum Analysis with Keysight experts”

This presentation is intended to be a beginning tutorial on signal analysis. Vector signal analysis includes but is not restricted to spectrum analysis. It is written for those who are unfamiliar with spectrum analyzers and vector signal analyzers, and would like a basic understanding of how they work, what you need to know to use them to their fullest potential, and how to make them more effective for particular applications. It is written for new engineers and technicians, therefore a basic understanding of electrical concepts is recommended.

We will begin with an overview of spectrum analysis. In this section, we will define spectrum analysis as well as present a brief introduction to the types of tests that are made with a spectrum and signal analyzer. From there, we will learn about spectrum and signal analyzers in terms of the hardware inside, what the importance of each component is, and how it all works together. In order to make measurements on a signal analyzer and to interpret the results correctly, it is important to understand the characteristics of the analyzer. Spectrum and signal analyzer specifications will help you determine if a particular instrument will make the measurements you need to make, and how accurate the results will be.

Topic 2: Vector Signal Analysis Fundamentals

“Insight into signal complexity with the 89600 VSA Software”

This presentation continues from previous to delve into Vector Signal Analysis. The 89600 VSA software supports over 75 signal types. We have a track record of being first-to-market for new technologies. Recent examples include both LTE-Advanced and 802.11ac and we continue to lead the market with features and enhancements. For A/D customers, now we offer pulse and FMCW radar analysis along with flexible custom demodulators to enable analysis of non-standard or proprietary signals with industry-standard tools.

Topic 3: RF Power Measurement Basics

“Insight into RF Power Measurements with Keysight Experts”

This presentation is a tutorial on RF power measurement which covers the importance, types, and methods of power measurements. It also describes the different types of power sensor technologies – thermistor, thermocouple and diode detector. Last but not least, we describe the advanced measurements used for the latest RF and microwave applications and power measurement uncertainty calculation.

Topic 4: Network Analysis Fundamentals

“Insight into the fundamentals of Network Analysis with Keysight Experts”

This presentation provides a review on RF basics, understanding of S-parameter measurements and the examination of the architectures and calibrations of VNAs.

A vector network analyzer (VNA) is a precision measuring tool that tests the electrical performance of high frequency components, in the radio frequency (RF), microwave, and millimeter-wave frequency bands (we will use the generic term RF to apply to all of these frequencies). A VNA is a stimulus-response test system, composed of an RF source and multiple measurement receivers. It is specifically designed to measure the forward and reverse reflection and transmission responses, or S-parameters, of RF components. S-parameters have both a magnitude and a phase component, and they characterize the linear performance of the DUT. While VNAs can also be used for characterizing some non-linear behavior like amplifier gain compression or intermodulation distortion, S-parameters are the primary measurement. The network analyzer hardware is optimized for speed, yielding swept measurements that are faster than those obtained from the use of an individual source and an individual receiver like a spectrum analyzer. Through calibration, VNAs provide the highest level of accuracy for measuring RF components.

Topic 5: RF Design & Simulation fundamentals

“Insight into RF/MW designs with Keysight Experts”

This session is a tutorial on Design Simulation technology and tools from Keysight EDA EEsof.
We will demonstrate S-parameter simulation, impedance matching, tuning, optimization and device modelling. X-parameters are introduced and the integration of S-parameters into test/design is explained. Both ADS & Genesys software will be used for demonstration purpose


Register for one of the events by clicking on the appropriate link in the table below.

Alternatively, receive notifications of future RF and Microwave Measurement Insights HOTSPOTS Seminars as they become available by clicking ‘Notify me’.

 

Where & When
 

Date(s) Location Seminar's Language For more information
2017-09-26 Edinburgh, UK English Register Here
2017-10-03 Padova, Italy Italian Register Here
2017-10-04 Ekaterinburg, Russia Russian Register Here
2017-10-10 EUMW 2017, (Nuremberg) English Register Here
2017-10-10 Guwahati, India English Register Here
2017-10-12 Arkhangelsk, Russia Russian Register Here
2017-10-17 Alcalá de Henares (Madrid), Spain Spanish Register Here
2017-10-18 Izhevsk, Russia Russian Register Here
2017-10-19 Almería, Spain Spanish Register Here
2017-10-25 Dublin, Ireland English Register Here
2017-11-28 Rosenheim, Germany German Register Here
2018-01-25 Leuven, Belgium English Register Here
2018-01-23 Eindhoven, HTC, Netherlands English Register Here