Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:


Discuter avec un expert

Spurious Measurements: Optimizing for Speed and Accuracy

1   Hour | Webcast - enregistré | Où et quand

What is the Webcast About?
Finding and measuring spurious signals is a common task and frequently a frustrating one. Measurements can take too much time, and accuracy for signals near an analyzer’s noise floor is a particular challenge. This webcast describes how to structure measurements for efficient spur search, plus how to take maximum advantage of internal signal processing (such as fast averaging and noise floor subtraction) and other capabilities of modern signal analyzers. The paper also discusses optimizing the measurement tradeoffs between speed, dynamic range, and accuracy.

Who Should View this Webcast?
Engineers making spurious measurements, primarily in communications (both terrestrial and satellite) and aerospace/defense applications. Some will be making measurements on complete systems while others will be measuring components or subassemblies. This webcast applies both to front panel and ATE users.

Où et quand

Price Lieu Pour de plus amples renseignements
Free At Your PC Enroll to view the recording of the Feb 15, 2012 broadcast 

Les prix montrés sont les prix courants et peuvent être modifiés sans préavis.

Matériel pour la formation/l'événement

Spurious Measurements: Optimizing for Speed and Accuracy Webcast Slides 
Feb 15, 2012 Webcast Slides

Présentation de séminaire 2012-02-15