Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Addressing Challenging New Test Requirements for DOCSIS 3.1 Upstream Signals Webcast

1   Hour | Webcast - recorded | Where & When

WHAT IS THE WEBCAST ABOUT

RF test procedures for next-generation cable modems require measurements ranging from those that are very familiar (transmit power, modulation quality, noise and spurious, etc.) to those that are totally new and unique to DOCSIS 3.1 OFDMA signals. This 1 hour webcast will describe new measurement challenges such as synchronized ACP, partially-equalized MER, relative symbol clock error and inter-burst noise and will present innovative new techniques for measuring them with accuracy and repeatability. Additional topics will include complex triggering techniques, as needed for upstream MER testing and out-of-band spurious analysis.

WHO SHOULD ATTEND

• R&D engineers involved with designing DOCSIS 3.1-based transmitters, receivers and components
• Signal integrity engineers
• DOCSIS 3.1 system integrators
• Cable network operators

PRESENTER

Ken Voelker, DOCSIS Specialist

Ken’s involvement with RF comms began during high school, as he designed and built equipment for his ham radio station. Following college, he worked 4 years developing production ATE systems for TRW Inc., buying so much HP RF test equipment that the company eventually hired him as a factory applications engineer. The 33 year career that followed focused on helping customers apply modern signal analysis tools to the emerging test problems of digital RF comms, through training seminars, applications development, hands-on assistance and product enhancements. He helped launch the industry’s first Vector Signal Analyzer in 1992, and served as lead planner for the follow-on 89600 VSA for the first 15 years of its remarkable lifetime.

Following retirement in 2013, Ken has now returned to Keysight as DOCSIS specialist, and serves as their representative on the DOCSIS 3.1 Working Group for PHY Layer Acceptance Test.

Where & When

Price Location For more information
Free At Your PC Enroll to view the August 12, 2015 recorded broadcast 

Prices shown are list prices and are subject to change without notice.

Training & Event Materials

Addressing Challenging New RF Test Requirements for DOCSIS 3.1 Upstream Signals Webcast Slides 
Slides from the August 12, 2015 webcast

Seminar Materials 2015-08-12

PDF PDF 758 KB