Keysight Technologies is now an independent company trading on the NYSE | Learn more

 

Contact an Expert

Fast Characterization of Power Amplifier Performance with Modulated Signals

1   Hour | Webcast - recorded | Where & When

RF Power Amplifier Design Series: Part 3

Why this webcast is important

Characterizing amplifier performance using sinusoids is reasonable during the early stages of the design process. However, gain compression from a one-tone sweep or intermodulation distortion from a two-tone sweep may not accurately predict ACLR or EVM, the real specifications. Designers need to know ACLR and EVM while an amplifier is delivering a specified output power, and they need to know how much statistical variation to expect. Also, they want to know what design parameters could be adjusted to improve performance. This paper shows techniques for carrying out these types of simulations. ADS examples will be provided.

Who should attend

Power Amplifier Designers
 

Where & When

Price Location For more information
Free At Your PC Enroll to view the Apr 5, 2012 recorded broadcast 

Prices shown are list prices and are subject to change without notice.