Labview Start-up Program
To start programming in Labview, it is necessary to install the PnP driver within Labview.
The installations procedure for Labview rev. 5 is explained in the C:\VXIPNP\WINNT\hp81200.hlp file.
For Labview rev. 6 please do see following instructions:
a) remove PnP for 81200 at following if they are available from former installations at folowing location:
/../labview6/instr.lib/hp81200/ all files.
b) go to:
TOOLS/INSTRUMENTATION/IMPORT CVI INSTRUMENT DRIVER
select at
VXIPNP/WINNT/HP81200/hp81200.fp
next step is, that this file will be converted to the correct VXIPNP driver.
c) Run the Labview program,
-by clicking on the right mousebutton, you need to perform RELINK TO SUBVI Than will the icon be highlighted
-At the second icon you need to double click it and change the PC name and save it
-At the System name you need to write in the correct clocksystem name
e.g. DSRA, or DEMO_A
-When you already had done a small programm, you can load with this Labview program the setting for the 81250.
-the file hp81200.dll can be found at the VXIPNP/WINNT - direcorty