Here’s the page we think you wanted. See search results instead:


Contact an Expert

What are the differences between Keysight IO Libraries Suite versions 14.0 and 14.1?

IO Libraries Revisions: 14.0 and 14.1

The differences are explained in the following diagram. Before version 14.1, a user would need to be concerned with what programming API or I/O Library they were using. This can cause confusion because not all of the APIs allowed for control of all available GPIB cards and converters.

An application written with National Instruments NI-488.2 API can now be implemented with an Agilent GPIB card or converter.

Last Updated: 19July, 2005